This is the reference manual for the EDDemo Application The Lightweight Mesh EDDemo application demonstrates the energy detection(ED) feature of Atmel Transceivers and helps analysing the energy on all channels . This application requires only one node for demonstration. No Data communication is performed in this application and no networking API's are used. A terminal needs to be connected to the node . The node measures the energy values on all channels periodically and prints the results on the connected terminal.