Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
SIO2HOST - USB

This module performs serial input/output functionalities via USB.

Functions

void dtr_cb (bool)
 This function is callled with the value set as true whenever a device is connected to the terminal. More...
 
uint8_t sio2host_getchar (void)
 This function performs a blocking character receive functionality. More...
 
int sio2host_getchar_nowait (void)
 This function performs a non-blocking character receive functionality. More...
 
void sio2host_init (void)
 Initializes the Serial IO Module of the Host Device. More...
 
void sio2host_putchar (uint8_t)
 
uint8_t sio2host_rx (uint8_t *data, uint8_t max_length)
 Receives data from USB. More...
 
uint8_t sio2host_tx (uint8_t *data, uint8_t length)
 Transmits data via USB. More...
 
void usb_rx_notify (void)
 This function is called by the USB data receive Interrupt The Receive buffer is filled in this function. More...
 

void dtr_cb ( bool  )

This function is callled with the value set as true whenever a device is connected to the terminal.

References stdio_usb_disable(), and stdio_usb_enable().

uint8_t sio2host_getchar ( void  )

This function performs a blocking character receive functionality.

Returns
returns the data which is received

References sio2host_rx().

int sio2host_getchar_nowait ( void  )

This function performs a non-blocking character receive functionality.

Returns
'-1' if no data is recieved or returns the data if a character is received

References sio2host_rx().

void sio2host_init ( void  )

Initializes the Serial IO Module of the Host Device.

Returns
STATUS_OK for successful initialization and FAILURE incase the IO is not initialized

References stdio_usb_init().

Referenced by wsndemo_init().

void sio2host_putchar ( uint8_t  )

References sio2host_tx().

Referenced by appUartSendMessage().

uint8_t sio2host_rx ( uint8_t *  data,
uint8_t  max_length 
)

Receives data from USB.

Parameters
datapointer to the buffer where the received data is to be stored
max_lengthmaximum length of data to be received
Returns
actual number of bytes received

References serial_rx_buf, serial_rx_buf_head, SERIAL_RX_BUF_SIZE_HOST, serial_rx_buf_tail, and serial_rx_count.

Referenced by APP_TaskHandler(), sio2host_getchar(), and sio2host_getchar_nowait().

uint8_t sio2host_tx ( uint8_t *  data,
uint8_t  length 
)

Transmits data via USB.

Parameters
dataPointer to the buffer where the data to be transmitted is present
lengthNumber of bytes to be transmitted
Returns
Number of bytes actually transmitted

References udi_cdc_putc().

Referenced by sio2host_putchar().

void usb_rx_notify ( void  )

This function is called by the USB data receive Interrupt The Receive buffer is filled in this function.

References cpu_irq_disable, cpu_irq_enable, main_b_cdc_enable, serial_rx_buf, SERIAL_RX_BUF_SIZE_HOST, serial_rx_buf_tail, serial_rx_count, udi_cdc_getc(), and udi_cdc_is_rx_ready().