#include "board.h"
Macros | |
#define | LED_BLINK LED1_GPIO |
#define | LED_DATA LED1_GPIO |
#define | LED_IDENTIFY LED0_GPIO |
#define | LED_NETWORK LED0_GPIO |
Functions | |
void | wsndemo_init (void) |
Init function of the WSNDemo application. More... | |
void | wsndemo_task (void) |
Task of the WSNDemo application This task should be called in a while(1) More... | |
#define LED_BLINK LED1_GPIO |
#define LED_DATA LED1_GPIO |
Referenced by appDataInd(), and appSendData().
#define LED_IDENTIFY LED0_GPIO |
Referenced by appCmdHandle(), appCmdIdentifyDurationTimerHandler(), and appCmdIdentifyPeriodTimerHandler().
void wsndemo_init | ( | void | ) |
Init function of the WSNDemo application.
References sio2host_init(), sm_init(), and SYS_Init().
Referenced by main().
void wsndemo_task | ( | void | ) |
Task of the WSNDemo application This task should be called in a while(1)
References APP_TaskHandler(), and SYS_TaskHandler().
Referenced by main().