Supply Controller (SUPC) driver for SAM.
Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.
#include "compiler.h"
Macros | |
#define | SUPC_CR_KEY_PASSWD SUPC_CR_KEY(0xA5U) |
Key used to write SUPC registers. More... | |
#define | SUPC_MR_KEY_PASSWD SUPC_MR_KEY(0xA5U) |
Enumerations | |
enum | slcdc_power_mode { SLCDC_POWER_MODE_LCDOFF = SUPC_MR_LCDMODE_LCDOFF, SLCDC_POWER_MODE_LCDON_EXTVR = SUPC_MR_LCDMODE_LCDON_EXTVR, SLCDC_POWER_MODE_LCDON_INVR = SUPC_MR_LCDMODE_LCDON_INVR } |
Power Mode. More... | |
Functions | |
void | supc_backup_sram_off (Supc *p_supc) |
void | supc_backup_sram_on (Supc *p_supc) |
void | supc_disable_backup_power_on_reset (Supc *p_supc) |
void | supc_disable_brownout_detector (Supc *p_supc) |
Disable the core brownout detector. More... | |
void | supc_disable_brownout_reset (Supc *p_supc) |
Disable the assertion of core reset signal when a brownout detection occurs. More... | |
void | supc_disable_monitor_interrupt (Supc *p_supc) |
Disable the assertion of SUPC interrupt signal when a supply monitor detection occurs. More... | |
void | supc_disable_monitor_reset (Supc *p_supc) |
Disable the assertion of core reset signal when a supply monitor detection occurs. More... | |
void | supc_disable_voltage_regulator (Supc *p_supc) |
void | supc_enable_backup_mode (Supc *p_supc) |
void | supc_enable_backup_power_on_reset (Supc *p_supc) |
void | supc_enable_brownout_detector (Supc *p_supc) |
Enable the core brownout detector. More... | |
void | supc_enable_brownout_reset (Supc *p_supc) |
Enable the assertion of core reset signal when a brownout detection occurs. More... | |
void | supc_enable_monitor_interrupt (Supc *p_supc) |
Enable the assertion of SUPC interrupt signal when a supply monitor detection occurs. More... | |
void | supc_enable_monitor_reset (Supc *p_supc) |
Enable the assertion of the core reset signal when a supply monitor detection occurs. More... | |
void | supc_enable_voltage_regulator (Supc *p_supc) |
enum slcdc_power_mode | supc_get_slcd_power_mode (Supc *p_supc) |
uint32_t | supc_get_status (Supc *p_supc) |
Get supply controller status. More... | |
void | supc_set_monitor_sampling_period (Supc *p_supc, uint32_t ul_period) |
Set Supply monitor sampling period. More... | |
void | supc_set_monitor_threshold (Supc *p_supc, uint32_t ul_threshold) |
Set Supply monitor threshold. More... | |
void | supc_set_regulator_trim_factory (Supc *p_supc) |
void | supc_set_regulator_trim_user (Supc *p_supc, uint32_t value) |
void | supc_set_slcd_power_mode (Supc *p_supc, enum slcdc_power_mode mode) |
void | supc_set_slcd_vol (Supc *p_supc, uint32_t vol) |
void | supc_set_wakeup_inputs (Supc *p_supc, uint32_t ul_inputs, uint32_t ul_transition) |
void | supc_set_wakeup_mode (Supc *p_supc, uint32_t ul_mode) |
void | supc_switch_sclk_to_32kxtal (Supc *p_supc, uint32_t ul_bypass) |
Switch slow clock source selection to external 32k (Xtal or Bypass) oscillator. More... | |
#define SUPC_CR_KEY_PASSWD SUPC_CR_KEY(0xA5U) |
Key used to write SUPC registers.
#define SUPC_MR_KEY_PASSWD SUPC_MR_KEY(0xA5U) |
enum slcdc_power_mode |
void supc_backup_sram_off | ( | Supc * | p_supc | ) |
void supc_backup_sram_on | ( | Supc * | p_supc | ) |
void supc_disable_backup_power_on_reset | ( | Supc * | p_supc | ) |
void supc_disable_voltage_regulator | ( | Supc * | p_supc | ) |
void supc_enable_backup_mode | ( | Supc * | p_supc | ) |
void supc_enable_backup_power_on_reset | ( | Supc * | p_supc | ) |
void supc_enable_voltage_regulator | ( | Supc * | p_supc | ) |
enum slcdc_power_mode supc_get_slcd_power_mode | ( | Supc * | p_supc | ) |
void supc_set_regulator_trim_factory | ( | Supc * | p_supc | ) |
void supc_set_regulator_trim_user | ( | Supc * | p_supc, |
uint32_t | value | ||
) |
void supc_set_slcd_power_mode | ( | Supc * | p_supc, |
enum slcdc_power_mode | mode | ||
) |
void supc_set_slcd_vol | ( | Supc * | p_supc, |
uint32_t | vol | ||
) |
void supc_set_wakeup_inputs | ( | Supc * | p_supc, |
uint32_t | ul_inputs, | ||
uint32_t | ul_transition | ||
) |
void supc_set_wakeup_mode | ( | Supc * | p_supc, |
uint32_t | ul_mode | ||
) |
Referenced by sm_init().