Alert Notification Profile declarations.
Copyright (c) 2017-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | ADV_TYPE_LEN (0x01) |
#define | ALERT_NOTI_CONTROL_CHAR_UUID (0x2A44) |
#define | ANP_ADV_DATA_APPEARANCE_DATA ("\x00\x40") |
#define | ANP_ADV_DATA_APPEARANCE_LEN (2) |
Appearance type & Length. More... | |
#define | ANP_ADV_DATA_APPEARANCE_TYPE (0x19) |
#define | ANP_ADV_DATA_NAME_DATA ("ATMEL-ANS") |
#define | ANP_ADV_DATA_NAME_LEN (9) |
Advertisement Name Type Length & data. More... | |
#define | ANP_ADV_DATA_NAME_TYPE (0x09) |
#define | ANP_ADV_DATA_UUID_LEN (2) |
ANCS Service Solicitation Info. More... | |
#define | ANP_ADV_DATA_UUID_TYPE (0x03) |
#define | APP_ANP_ADV_TIMEOUT (655) |
APP_ANP_ADV_TIMEOUT Advertising time-out between 0x0001 and 0x028F in seconds, 0x0000 disables time-out. More... | |
#define | APP_ANP_FAST_ADV (1600) |
Advertisement Interval. More... | |
#define | AT_BLE_DISCOVERY_SUCCESS (10) |
#define | CLIENT_CHAR_CONF_DESC_UUID (0x2902) |
#define | NEW_ALERT_CHAR_UUID (0x2A46) |
#define | SCAN_RESP_LEN (10) |
Scan Response length. More... | |
#define | SUPPORT_NEW_ALERT_CHAR_UUID (0x2A47) |
#define | SUPPORT_UNREAD_ALERT_CHAR_UUID (0x2A48) |
#define | UNREAD_ALERT_STATUS_CHAR_UUID (0x2A45) |
Typedefs | |
typedef void(* | connected_callback_t )(bool) |
Functions | |
at_ble_status_t | alert_service_discovery (void) |
Discovering the services of Alert Notification. More... | |
void | anp_client_adv (void) |
does all the profile initialization and starts the advertisement More... | |
void | anp_client_char_changed_handler (at_ble_characteristic_changed_t *params) |
Handler for char changed handler. More... | |
at_ble_status_t | anp_client_characteristic_found_handler (void *params) |
Handler for characteristic found event. More... | |
at_ble_status_t | anp_client_descriptor_found_handler (void *params) |
Handler for descriptor found event. More... | |
void | anp_client_disable_notification (void) |
invoked by app for disabling the notifications in gatt server More... | |
at_ble_status_t | anp_client_disconnected_event_handler (void *params) |
Handler for disconnection event. More... | |
at_ble_status_t | anp_client_discovery_complete_handler (void *params) |
Handler for discovery complete event. More... | |
void | anp_client_init (void *params) |
Function used for profile initialization and also enable the advertisement. More... | |
at_ble_status_t | anp_client_notification_handler (void *params) |
Handler for notification event. More... | |
at_ble_status_t | anp_client_read_response_handler (void *params) |
Handler for read response handle. More... | |
at_ble_status_t | anp_client_security_done_handler (void *param) |
invoked by ble manager for setting the notification More... | |
at_ble_status_t | anp_client_service_found_handler (void *params) |
Handler for service found event. More... | |
void | anp_client_write_notification_handler (void) |
Handler for enabling the notification. More... | |
at_ble_status_t | anp_client_write_response_handler (void *params) |
Handler for write response. More... | |
at_ble_status_t | anp_info_connect_handler (void *params) |
Connection handler callback. More... | |
void | anp_info_init (void) |
Initialize the profile specific information. More... | |
at_ble_status_t | anp_info_service_discover (void *params) |
Discovering the services of Alert Notification. More... | |
at_ble_status_t | anp_write_to_ncp (uint8_t *value) |
char changed handler invoked by application More... | |
void | register_connected_callback (connected_callback_t app_connected_cb) |
register the call back for application state More... | |
#define ADV_TYPE_LEN (0x01) |
#define ALERT_NOTI_CONTROL_CHAR_UUID (0x2A44) |
Referenced by anp_client_characteristic_found_handler().
#define ANP_ADV_DATA_APPEARANCE_DATA ("\x00\x40") |
#define ANP_ADV_DATA_APPEARANCE_LEN (2) |
Appearance type & Length.
#define ANP_ADV_DATA_APPEARANCE_TYPE (0x19) |
#define ANP_ADV_DATA_NAME_DATA ("ATMEL-ANS") |
#define ANP_ADV_DATA_NAME_LEN (9) |
Advertisement Name Type Length & data.
#define ANP_ADV_DATA_NAME_TYPE (0x09) |
#define ANP_ADV_DATA_UUID_LEN (2) |
ANCS Service Solicitation Info.
#define ANP_ADV_DATA_UUID_TYPE (0x03) |
#define APP_ANP_ADV_TIMEOUT (655) |
APP_ANP_ADV_TIMEOUT Advertising time-out between 0x0001 and 0x028F in seconds, 0x0000 disables time-out.
Referenced by anp_client_adv().
#define APP_ANP_FAST_ADV (1600) |
Advertisement Interval.
This is the reference manual for the Time Information Profile
Referenced by anp_client_adv().
#define AT_BLE_DISCOVERY_SUCCESS (10) |
Referenced by anp_client_discovery_complete_handler().
#define CLIENT_CHAR_CONF_DESC_UUID (0x2902) |
Referenced by anp_client_descriptor_found_handler().
#define NEW_ALERT_CHAR_UUID (0x2A46) |
Referenced by anp_client_characteristic_found_handler().
#define SCAN_RESP_LEN (10) |
Scan Response length.
#define SUPPORT_NEW_ALERT_CHAR_UUID (0x2A47) |
Referenced by anp_client_characteristic_found_handler().
#define SUPPORT_UNREAD_ALERT_CHAR_UUID (0x2A48) |
Referenced by anp_client_characteristic_found_handler().
#define UNREAD_ALERT_STATUS_CHAR_UUID (0x2A45) |
Referenced by anp_client_characteristic_found_handler().
typedef void(* connected_callback_t)(bool) |
at_ble_status_t alert_service_discovery | ( | void | ) |
Discovering the services of Alert Notification.
References anp_conn_handle, AT_BLE_FAILURE, at_ble_primary_service_discover_all(), AT_BLE_SUCCESS, DBG_LOG, DBG_LOG_DEV, GATT_DISCOVERY_ENDING_HANDLE, and GATT_DISCOVERY_STARTING_HANDLE.
Referenced by anp_custom_event(), anp_info_connect_handler(), and anp_info_service_discover().
void anp_client_adv | ( | void | ) |
does all the profile initialization and starts the advertisement
does all the profile initialization and starts the advertisement
References APP_ANP_ADV_TIMEOUT, APP_ANP_FAST_ADV, AT_BLE_ADV_FP_ANY, AT_BLE_ADV_GEN_DISCOVERABLE, at_ble_adv_start(), AT_BLE_ADV_TYPE_UNDIRECTED, AT_BLE_SUCCESS, and DBG_LOG.
Referenced by app_connected_state(), and main().
void anp_client_char_changed_handler | ( | at_ble_characteristic_changed_t * | params | ) |
Handler for char changed handler.
[in] | characteristic | changed event parameter containing details like characteristic handle,value |
at_ble_status_t anp_client_characteristic_found_handler | ( | void * | params | ) |
Handler for characteristic found event.
[in] | characteristic | found event parameter containing details like characteristic handle,uuid |
Handler for characteristic found event.
[in] | at_ble_characteristic_found_t | consists the characteristic handle,value handle |
References ALERT_NOTI_CONTROL_CHAR_UUID, gatt_anp_handler::alert_np_char_handle, AT_BLE_SUCCESS, at_ble_characteristic_found_t::char_handle, at_ble_characteristic_found_t::char_uuid, at_ble_characteristic_found_t::conn_handle, DBG_LOG, DBG_LOG_DEV, DBG_LOG_PTS, gatt_anp_handler::desc_discovery, gatt_anp_handler::new_alert_char_handle, NEW_ALERT_CHAR_UUID, at_ble_characteristic_found_t::properties, gatt_anp_handler::supp_new_char_handle, gatt_anp_handler::supp_unread_char_handle, SUPPORT_NEW_ALERT_CHAR_UUID, SUPPORT_UNREAD_ALERT_CHAR_UUID, at_ble_uuid_t::type, gatt_anp_handler::unread_alert_char_handle, UNREAD_ALERT_STATUS_CHAR_UUID, at_ble_uuid_t::uuid, and at_ble_characteristic_found_t::value_handle.
at_ble_status_t anp_client_descriptor_found_handler | ( | void * | params | ) |
Handler for descriptor found event.
[in] | descriptor | found event parameter containing details like descriptor handle,uuid |
Handler for descriptor found event.
[in] | at_ble_descriptor_found_t | consists the descriptor handle |
References AT_BLE_SUCCESS, AT_BLE_UUID_16, CLIENT_CHAR_CONF_DESC_UUID, DBG_LOG, DBG_LOG_PTS, at_ble_descriptor_found_t::desc_handle, at_ble_descriptor_found_t::desc_uuid, gatt_anp_handler::new_alert_char_handle, gatt_anp_handler::new_alert_desc_handle, at_ble_uuid_t::type, gatt_anp_handler::unread_alert_char_handle, gatt_anp_handler::unread_alert_desc_handle, and at_ble_uuid_t::uuid.
void anp_client_disable_notification | ( | void | ) |
invoked by app for disabling the notifications in gatt server
[in] | none |
References anp_alert_noti(), AT_BLE_SUCCESS, DBG_LOG, DBG_LOG_DEV, gatt_anp_handler::new_alert_desc_handle, and gatt_anp_handler::unread_alert_desc_handle.
Referenced by anp_custom_event().
at_ble_status_t anp_client_disconnected_event_handler | ( | void * | params | ) |
Handler for disconnection event.
[in] | disconnected | event parameter containing details like handle |
Handler for disconnection event.
[in] | at_ble_disconnected_t | consists connection handle and reason return none |
References ALL_UNUSED, AT_BLE_SUCCESS, and connected_cb.
at_ble_status_t anp_client_discovery_complete_handler | ( | void * | params | ) |
Handler for discovery complete event.
[in] | discovery | complete event which contains result of discovery event |
Handler for discovery complete event.
[in] | at_ble_discovery_complete_t | which consists of discovery status handle and params |
References anp_client_security_done_handler(), AT_BLE_ATT_INSUFF_RESOURCE, at_ble_characteristic_discover_all(), at_ble_descriptor_discover_all(), at_ble_disconnect(), AT_BLE_DISCOVERY_SUCCESS, AT_BLE_FAILURE, AT_BLE_INVALID_PARAM, AT_BLE_SUCCESS, AT_BLE_TERMINATED_BY_USER, gatt_anp_handler::char_discovery, DBG_LOG, DBG_LOG_DEV, gatt_anp_handler::desc_discovery, gatt_anp_handler::end_handle, gatt_anp_handler::start_handle, and at_ble_cmd_complete_event_t::status.
void anp_client_init | ( | void * | params | ) |
Function used for profile initialization and also enable the advertisement.
Function used for profile initialization and also enable the advertisement.
[in] | void | params passed by the blemanager,app may use it or may not |
References anp_info_init(), AT_BLE_SUCCESS, ble_advertisement_data_set(), BLE_GAP_EVENT_TYPE, BLE_GATT_CLIENT_EVENT_TYPE, ble_mgr_events_callback_handler(), DBG_LOG, REGISTER_CALL_BACK, and UNUSED.
Referenced by main().
at_ble_status_t anp_client_notification_handler | ( | void * | params | ) |
Handler for notification event.
[in] | notification | received parameter containing the notification value |
Handler for notification event.
[in] | at_ble_notification_recieved_t | consists the char handle |
References anp_alert_notify_response(), and AT_BLE_SUCCESS.
at_ble_status_t anp_client_read_response_handler | ( | void * | params | ) |
Handler for read response handle.
Handler for read response handle.
[in] | at_ble_characteristic_read_response_t | consists of characteristic handle value handle |
References anp_alert_read_response(), anp_client_write_notification_handler(), AT_BLE_SUCCESS, start_notification, SUPPORTED_NEW_ALERT_READ, and SUPPORTED_UNREAD_ALERT_READ.
at_ble_status_t anp_client_security_done_handler | ( | void * | param | ) |
invoked by ble manager for setting the notification
[in] | param's | passed by the ble manager which may or may not be used |
References anp_alert_read(), AT_BLE_SUCCESS, DBG_LOG_DEV, LED0, LED_Toggle, start_notification, gatt_anp_handler::supp_new_char_handle, gatt_anp_handler::supp_unread_char_handle, and UNUSED.
Referenced by anp_client_discovery_complete_handler().
at_ble_status_t anp_client_service_found_handler | ( | void * | params | ) |
Handler for service found event.
[in] | service | found event parameter containing details like service handle,uuid |
Handler for service found event.
[in] | at_ble_primary_service_found_t | which consists of starting and ending handle of service |
References ANP_SERVICE_UUID, AT_BLE_SUCCESS, AT_BLE_UUID_16, gatt_anp_handler::char_discovery, DBG_LOG, DBG_LOG_PTS, gatt_anp_handler::end_handle, at_ble_primary_service_found_t::end_handle, at_ble_primary_service_found_t::service_uuid, gatt_anp_handler::start_handle, at_ble_primary_service_found_t::start_handle, at_ble_uuid_t::type, and at_ble_uuid_t::uuid.
void anp_client_write_notification_handler | ( | void | ) |
Handler for enabling the notification.
[in] | none |
References anp_alert_noti(), AT_BLE_SUCCESS, DBG_LOG, DBG_LOG_DEV, gatt_anp_handler::new_alert_desc_handle, and gatt_anp_handler::unread_alert_desc_handle.
Referenced by anp_client_read_response_handler(), and anp_custom_event().
at_ble_status_t anp_client_write_response_handler | ( | void * | params | ) |
Handler for write response.
[in] | write | response parameter contacting the result of write request |
Handler for write response.
[in] | at_ble_characteristic_write_response_t | consists the char |
References AT_BLE_SUCCESS, at_ble_characteristic_write_response_t::char_handle, DBG_LOG_DEV, gatt_anp_handler::new_alert_desc_handle, and gatt_anp_handler::unread_alert_desc_handle.
at_ble_status_t anp_info_connect_handler | ( | void * | params | ) |
Connection handler callback.
[in] | at_ble_connected_t | which consists of connection handle |
References alert_service_discovery(), anp_conn_handle, AT_BLE_SUCCESS, at_ble_connected_t::conn_status, connected_cb, DBG_LOG, and at_ble_connected_t::handle.
void anp_info_init | ( | void | ) |
Initialize the profile specific information.
Initialize the profile specific information.
[in] | none |
References alert_np_char_data, gatt_anp_handler::alert_np_data, new_alert_char_data, gatt_anp_handler::new_alert_char_data, supp_new_char_data, gatt_anp_handler::supp_new_char_data, supp_unread_char_data, gatt_anp_handler::supp_unread_char_data, unread_alert_char_data, and gatt_anp_handler::unread_alert_char_data.
Referenced by anp_client_init().
at_ble_status_t anp_info_service_discover | ( | void * | params | ) |
Discovering the services of Alert Notification.
[in] | at_ble_connected_t | which consists of connection handle |
References alert_service_discovery(), and ALL_UNUSED.
at_ble_status_t anp_write_to_ncp | ( | uint8_t * | value | ) |
char changed handler invoked by application
[in] | uint8_t | array consists of value to be written to alert notification control point |
[in] | uint8_t | consists of value to be written to alert notification control point |
References gatt_anp_handler::alert_np_char_handle, and at_ble_characteristic_write().
Referenced by anp_custom_event().
void register_connected_callback | ( | connected_callback_t | app_connected_cb | ) |
register the call back for application state
[in] | @return | none |
register the call back for application state
[in] | app_connected_cb | application callback function |
References connected_cb.
Referenced by main().