Microchip® Advanced Software Framework

at_ble_htpt_disable_ind_t Struct Reference

Parameters of the AT_BLE_HTPT_DISABLE_IND message.

#include <at_ble_api.h>

Data Fields

uint16_t conhdl
 Connection handle. More...
 
uint16_t interm_temp_ntf_en
 Intermediate temperature notification configuration. More...
 
uint16_t meas_intv
 Measurement interval. More...
 
uint16_t meas_intv_ind_en
 Measurement interval indication configuration. More...
 
uint16_t temp_meas_ind_en
 Temperature measurement indication configuration. More...
 

uint16_t at_ble_htpt_disable_ind_t::conhdl

Connection handle.

uint16_t at_ble_htpt_disable_ind_t::interm_temp_ntf_en

Intermediate temperature notification configuration.

uint16_t at_ble_htpt_disable_ind_t::meas_intv

Measurement interval.

uint16_t at_ble_htpt_disable_ind_t::meas_intv_ind_en

Measurement interval indication configuration.

uint16_t at_ble_htpt_disable_ind_t::temp_meas_ind_en

Temperature measurement indication configuration.