Microchip® Advanced Software Framework

•All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Misc APIs

This group includes APIs which are not belong to any task.

Functions

at_ble_status_t at_ble_enable_sleep (bool en_sleep)
 Enable/disable deep sleep. More...
 
at_ble_status_t at_ble_event_get (at_ble_events_t *event, void *params, uint32_t timeout)
 extracts the next event form the event queue More...
 
at_ble_status_t at_ble_event_user_defined_post (void *params)
 Posts a user defined custom event into the event queue, allowing the user code to process other events in the same event handling loop. More...
 

at_ble_status_t at_ble_enable_sleep ( bool  en_sleep)

Enable/disable deep sleep.

Sleep is enabled by default.

Parameters
[in]en_sleeptrue to enable deep sleep or false to disable it
Returns
Upon successful completion the function shall return AT_BLE_SUCCESS, Otherwise the function shall return at_ble_status_t
at_ble_status_t at_ble_event_get ( at_ble_events_t event,
void *  params,
uint32_t  timeout 
)

extracts the next event form the event queue

Parameters
[out]eventThe received event
[out]paramsReceived event data
[in]timeoutTime in millisecond this function will block waiting of an event (0xFFFFFFFF to block indefinitely) in this case, if the user wishes to unblock the function at_ble_event_user_defined_post can be used
Returns
Upon successful completion the function shall return AT_BLE_SUCCESS, Otherwise the function shall return at_ble_status_t
at_ble_status_t at_ble_event_user_defined_post ( void *  params)

Posts a user defined custom event into the event queue, allowing the user code to process other events in the same event handling loop.

Events will be received with the as AT_BLE_CUSTOM_EVENT

Parameters
[in]paramsParameters sent to the custom event
Returns
AT_BLE_SUCCESS operation completed successfully
AT_BLE_FAILURE Generic error.