#include <at_ble_api.h>
Data Fields | |
uint16_t | desc_val_length |
descriptor value initial length More... | |
uint16_t | desc_val_max_length |
maximum possible length of the descriptor value More... | |
at_ble_handle_t | handle |
Here the stack will store the handle for future use. More... | |
at_ble_attr_permissions_t | perm |
descriptor permissions More... | |
at_ble_uuid_t | uuid |
descriptor uuid More... | |
uint16_t at_ble_generic_att_desc_t::desc_val_length |
descriptor value initial length
uint16_t at_ble_generic_att_desc_t::desc_val_max_length |
maximum possible length of the descriptor value
at_ble_handle_t at_ble_generic_att_desc_t::handle |
Here the stack will store the handle for future use.
at_ble_attr_permissions_t at_ble_generic_att_desc_t::perm |
descriptor permissions
at_ble_uuid_t at_ble_generic_att_desc_t::uuid |
descriptor uuid