HID Service.
Copyright (c) 2017-2018 Microchip Technology Inc. and its subsidiaries.
#include "stddef.h"
#include "stdio.h"
#include "string.h"
#include "at_ble_api.h"
#include "ble_manager.h"
#include "hid.h"
#include "hid_device.h"
Functions | |
void | hid_boot_keyboardreport_update (at_ble_handle_t conn_handle, uint8_t serv_inst, uint8_t *bootreport, uint16_t len) |
to update the boot keyboard report. More... | |
void | hid_boot_mousereport_update (at_ble_handle_t conn_handle, uint8_t serv_inst, uint8_t *bootreport, uint16_t len) |
to update the boot mouse report. More... | |
uint8_t | hid_get_reportchar (uint16_t handle, uint8_t serv, uint8_t reportid) |
to get the report characteristic id. More... | |
uint8_t | hid_get_reportid (uint8_t serv, uint16_t handle, uint8_t reportnum) |
to get the report ID. More... | |
uint8_t | hid_ntf_instance (uint8_t serv_num, uint16_t char_handle) |
to get the notification instance. More... | |
void | hid_serv_def_init (uint8_t servnum) |
service definition initialization function More... | |
uint8_t | hid_serv_get_instance (uint16_t handle) |
to get service instance. More... | |
void | hid_serv_init (uint8_t servinst, uint8_t device, uint8_t *mode, uint8_t report_num, uint8_t *report_type, uint8_t **report_val, uint8_t *report_len, hid_info_t *info) |
service Configuration function More... | |
void | hid_serv_report_map (uint8_t servinst, uint8_t *report_info, uint16_t len) |
update the report descriptor for HID device More... | |
void | hid_serv_report_update (uint16_t conn_handle, uint8_t serv_inst, uint8_t reportid, uint8_t *report, uint16_t len) |
to update the report. More... | |
uint16_t | hid_service_dbreg (uint8_t inst, uint8_t *report_type, uint8_t *report_id, uint8_t report_num) |
register the HID service. More... | |
Variables | |
uint8_t | ctrl_point [1] |
hid_gatt_serv_handler_t | hid_inst [HID_MAX_SERV_INST] |
hid_serv_t | hid_serv_inst [HID_MAX_SERV_INST] |
uint8_t | keyb_in_report [8] |
uint8_t | Keyb_out_report [1] |
at_ble_generic_att_desc_t | report_desc [HID_NUM_OF_REPORT] |
void hid_boot_keyboardreport_update | ( | at_ble_handle_t | conn_handle, |
uint8_t | serv_inst, | ||
uint8_t * | bootreport, | ||
uint16_t | len | ||
) |
to update the boot keyboard report.
Function to update the boot keyboard report.
References ALL_UNUSED, at_ble_characteristic_value_get(), at_ble_characteristic_value_set(), at_ble_notification_send(), AT_BLE_SUCCESS, and DBG_LOG_DEV.
Referenced by hid_prf_boot_keyboardreport_update().
void hid_boot_mousereport_update | ( | at_ble_handle_t | conn_handle, |
uint8_t | serv_inst, | ||
uint8_t * | bootreport, | ||
uint16_t | len | ||
) |
to update the boot mouse report.
Function to update the boot mouse report.
References ALL_UNUSED, at_ble_characteristic_value_get(), at_ble_characteristic_value_set(), at_ble_notification_send(), AT_BLE_SUCCESS, and DBG_LOG_DEV.
Referenced by hid_prf_boot_mousereport_update().
uint8_t hid_get_reportchar | ( | uint16_t | handle, |
uint8_t | serv, | ||
uint8_t | reportid | ||
) |
to get the report characteristic id.
Function to get report characteristic id.
References at_ble_descriptor_value_get(), AT_BLE_SUCCESS, DBG_LOG_DEV, HID_INVALID_INST, and HID_NUM_OF_REPORT.
Referenced by hid_serv_report_update().
uint8_t hid_get_reportid | ( | uint8_t | serv, |
uint16_t | handle, | ||
uint8_t | reportnum | ||
) |
to get the report ID.
Function to get the report ID.
References at_ble_descriptor_value_get(), AT_BLE_SUCCESS, DBG_LOG_DEV, and HID_INVALID_INST.
Referenced by hid_prf_char_changed_handler().
uint8_t hid_ntf_instance | ( | uint8_t | serv_num, |
uint16_t | char_handle | ||
) |
to get the notification instance.
Function to get the notification instance.
References BOOT_KEY_INPUT_REPORT, BOOT_MOUSE_INPUT_REPORT, CHAR_REPORT, CHAR_REPORT_CCD, CONTROL_POINT, DBG_LOG_DEV, HID_NUM_OF_REPORT, and PROTOCOL_MODE.
Referenced by hid_prf_char_changed_handler().
void hid_serv_def_init | ( | uint8_t | servnum | ) |
service definition initialization function
service definition initialization function
References hid_serv::hid_control_point, hid_serv::hid_dev_boot_keyboard_in_report, hid_serv::hid_dev_boot_keyboard_out_report, hid_serv::hid_dev_info, hid_serv::hid_dev_proto_mode_char, hid_serv::hid_dev_report_map_char, hid_serv::hid_dev_report_val_char, hid_serv::hid_dev_serv_handle, hid_serv::hid_dev_serv_uuid, and HID_NUM_OF_REPORT.
Referenced by hid_prf_init().
uint8_t hid_serv_get_instance | ( | uint16_t | handle | ) |
to get service instance.
Function to get service instance.
References DBG_LOG_DEV, and HID_MAX_SERV_INST.
Referenced by hid_prf_char_changed_handler().
void hid_serv_init | ( | uint8_t | servinst, |
uint8_t | device, | ||
uint8_t * | mode, | ||
uint8_t | report_num, | ||
uint8_t * | report_type, | ||
uint8_t ** | report_val, | ||
uint8_t * | report_len, | ||
hid_info_t * | info | ||
) |
service Configuration function
Initialize the hid profile based on user input.
References at_ble_chr_t::additional_desc_count, at_ble_chr_t::additional_desc_list, AT_BLE_ATTR_NO_PERMISSIONS, AT_BLE_ATTR_READABLE_NO_AUTHN_NO_AUTHR, AT_BLE_ATTR_READABLE_REQ_AUTHN_NO_AUTHR, AT_BLE_ATTR_WRITABLE_NO_AUTHN_NO_AUTHR, AT_BLE_ATTR_WRITABLE_REQ_AUTHN_NO_AUTHR, AT_BLE_CHAR_NOTIFY, AT_BLE_CHAR_READ, AT_BLE_CHAR_WRITE, AT_BLE_CHAR_WRITE_WITHOUT_RESPONSE, AT_BLE_UUID_16, BLE_PAIR_ENABLE, at_ble_service_t::char_count, at_ble_service_t::char_list, at_ble_chr_t::char_val, at_ble_chr_t::client_config_desc, ctrl_point, DBG_LOG, DBG_LOG_PTS, at_ble_generic_att_desc_t::desc_val_length, at_ble_generic_att_desc_t::desc_val_max_length, FEATURE_REPORT, at_ble_generic_att_desc_t::handle, at_ble_server_config_desc_t::handle, at_ble_user_desc_t::handle, at_ble_char_val_t::handle, at_ble_service_t::handle, HID_CHARACTERISTIC_NUM, hid_serv::hid_control_point, hid_serv::hid_dev_boot_keyboard_in_report, hid_serv::hid_dev_boot_keyboard_out_report, hid_serv::hid_dev_info, hid_serv::hid_dev_proto_mode_char, hid_serv::hid_dev_report_map_char, hid_serv::hid_dev_report_val_char, hid_serv::hid_dev_serv_handle, hid_serv::hid_dev_serv_uuid, HID_KEYBOARD_MODE, HID_MOUSE_MODE, HID_REPORT_REF_DESC, HID_SERV_UUID, HID_UUID_CHAR_BOOT_KEY_INPUT_REPORT, HID_UUID_CHAR_BOOT_KEY_OUTPUT_REPORT, HID_UUID_CHAR_BOOT_MOUSE_INPUT_REPORT, HID_UUID_CHAR_HID_CONTROL_POINT, HID_UUID_CHAR_HID_INFORMATION, HID_UUID_CHAR_PROTOCOL_MODE, HID_UUID_CHAR_REPORT, HID_UUID_CHAR_REPORT_MAP, at_ble_service_t::inc_list, at_ble_service_t::included_count, at_ble_char_val_t::init_value, INPUT_REPORT, keyb_in_report, Keyb_out_report, at_ble_user_desc_t::len, at_ble_char_val_t::len, at_ble_char_val_t::max_len, OUTPUT_REPORT, at_ble_generic_att_desc_t::perm, at_ble_server_config_desc_t::perm, at_ble_service_t::perm, at_ble_user_desc_t::permissions, at_ble_char_val_t::permissions, at_ble_chr_t::presentation_format, PRIMARY_SERVICE, at_ble_char_val_t::properties, hid_gatt_serv_handler::serv, hid_gatt_serv_handler::serv_chars, hid_gatt_serv_handler::serv_desc, at_ble_chr_t::server_config_desc, at_ble_uuid_t::type, at_ble_service_t::type, at_ble_chr_t::user_desc, at_ble_user_desc_t::user_description, at_ble_uuid_t::uuid, at_ble_generic_att_desc_t::uuid, at_ble_char_val_t::uuid, and at_ble_service_t::uuid.
Referenced by hid_prf_init().
void hid_serv_report_map | ( | uint8_t | servinst, |
uint8_t * | report_info, | ||
uint16_t | len | ||
) |
update the report descriptor for HID device
Function update the report descriptor for HID device.
References at_ble_chr_t::char_val, hid_serv::hid_dev_report_map_char, at_ble_char_val_t::init_value, at_ble_char_val_t::len, at_ble_char_val_t::max_len, and hid_gatt_serv_handler::serv_chars.
Referenced by hid_prf_init().
void hid_serv_report_update | ( | uint16_t | conn_handle, |
uint8_t | serv_inst, | ||
uint8_t | reportid, | ||
uint8_t * | report, | ||
uint16_t | len | ||
) |
to update the report.
Function to update the report.
References at_ble_characteristic_value_set(), at_ble_notification_send(), AT_BLE_SUCCESS, DBG_LOG, DBG_LOG_DEV, hid_get_reportchar(), and HID_INVALID_INST.
Referenced by hid_prf_report_update().
uint16_t hid_service_dbreg | ( | uint8_t | inst, |
uint8_t * | report_type, | ||
uint8_t * | report_id, | ||
uint8_t | report_num | ||
) |
register the HID service.
Register the service into database.
References at_ble_descriptor_value_set(), at_ble_service_define(), AT_BLE_SUCCESS, DBG_LOG, DBG_LOG_DEV, delay_ms, at_ble_service_t::handle, HID_SERV_FAILED, and hid_gatt_serv_handler::serv.
Referenced by hid_prf_init().
uint8_t ctrl_point[1] |
Referenced by hid_serv_init().
hid_gatt_serv_handler_t hid_inst[HID_MAX_SERV_INST] |
hid_serv_t hid_serv_inst[HID_MAX_SERV_INST] |
uint8_t keyb_in_report[8] |
Referenced by hid_serv_init().
uint8_t Keyb_out_report[1] |
Referenced by hid_serv_init().
at_ble_generic_att_desc_t report_desc[HID_NUM_OF_REPORT] |