Introduction
******************************Introduction ***********************************
The HID Mouse example application bring-up the HID over GATT (HOGP) profile defined by the Bluetooth SIG. The HID over GATT (HOGP) profile defined by the Bluetooth SIG enables support of HID services over a Bluetooth Low Energy (BLE) protocol stack using Generic Attribute profile (GATT). This allows devices like keyboard or mouse implementing HOGP to connect to a compatible HOGP/BLE host device (e.g.: Mobile Phone, Tablet, TV, etc.).
- Supported Evolution Kit -
- ATSAML21-XPRO-B + ATBTLC1000 XPRO
- ATSAMD21-XPRO + ATBTLC1000 XPRO
- ATSAMG55-XPRO + ATBTLC1000 XPRO
- ATSAM4S-XPRO + ATBTLC1000 XPRO
- Running the demo -
- 1. Build and flash the binary into supported evaluation board.
- 2. Open the console using TeraTerm or any serial port monitor.
- 3. Press the Reset button.
- 4. Wait for around 10 seconds for the patches to be downloaded device will initialize and start-up.
- 5. The device is now in advertising mode.
- 6. The demo requires use of an Android mobile phone supporting HOGP. The HOGP profile is natively supported in Android from version 4.4 (Android KitKat) and higher versions. The phone must include support a Bluetooth chipset supporting BT 4.0 or higher version on the mobile phone, In Bluetooth settings scan for the devices, device with “ATMEL-HID” will be found as shown below. Click on “ATMEL-HID” to get connected.
- 7. Once connected, the client side will request for the pairing procedure . The console log provides a guidance for the user to enter the pass-key.
- 8. Once the device connected to host (Phone). User can click on SW0 button on supported platform for simulating mouse movement.
- 9. For every press on button, the user can see corresponding cursor movement on HID host as described below:
- First 5 Button Press: Cursor moves right
- Next 5 Button Press: Cursor moved down
- Next 5 Button Press: Cursor moves left
- Next 5 Button Press: Cursor moved up.
Modules
***************************** MODULES *****************************************
- BLE Manager -
- The Event Manager is responsible for handling the following:
- Generic BLE Event Handling:-
- BLE Event Manager handles the events triggered by BLE stack and also responsible for invoking all registered callbacks for respective events. BLE Manager handles all GAP related functionality. In addition to that handles multiple connection instances, Pairing, Encryption, Scanning.
- Handling Multi-role/multi-connection:-
- BLE Event Manager is responsible for handling multiple connection instances and stores bonding information and Keys to retain the bonded device. BLE Manager is able to identify and remove the device information when pairing/encryption gets failed. In case of multi-role, it handles the state/event handling of both central and peripheral in multiple contexts.
- Controlling the Advertisement data:-
- BLE Event Manager is responsible for generating the advertisement and scan response data for BLE profiles/services that are attached with BLE Manager.
- BLE Profile-
- This profile defines how a device with Bluetooth low energy wireless communications can support HID services over the Bluetooth low energy protocol stack using the Generic Attribute Profile. HID Over GATT Profile supports two services:
- Human Interface Device -
- The HID Service exposes characteristics required for a HID Device to transfer HID report descriptors and reports to a HID Host. This also exposes the characteristics for a HID Host to write to a Device. The Human Interface Device Service is instantiated as a Primary Service.
- Device Information service -
- The Device Information Service exposes manufacturer and/or vendor information about a device.
- BLE Platform Services -
- Interface Settings -
- Connect ATBTLC1000 XPRO to SAML21-XPRO-B -> EXT1
- Connect ATBTLC1000 XPRO to SAMD21-XPRO -> EXT1
- Connect ATBTLC1000 XPRO to SAMG55-XPRO -> EXT1
- Connect ATBTLC1000 XPRO to SAM4S-XPRO -> EXT1
- Serial Console COM port settings -
- Baudrate 115200
- Parity None, Stop Bit 1, Start Bit 1
- No Hardware Handshake
- 6-Wire Mode Connection Setup -
- Pins are 1:1 match with SAML21/D21 Xpro EXT1 Header to BTLC1000 XPro Header
- UART(No Flow Control)-SAM L21/D21 XPro Pins (Rx-Pin13, Tx-Pin14)
- UART(With Flow Control)-SAM G55 Xpro Pins (Rx-Pin13, Tx-Pin14, RTS-Pin5, CTS-Pin6, Rx-Pin16, Tx-Pin17)
- BTLC1000 Wakeup Pin-SAM G55 XPro Pins(Pin4)
- BTLC1000 Chip Enable Pin-SAM G55 XPro Pins(Pin10)
- BTLC1000 Vcc Pin-SAM L21/D21/G55 Xpro Pins(Pin20)
- BTLC1000 GND Pin-SAM L21/D21/G55 Xpro Pins(Pin19)
- 4-Wire Mode Connection setup -
- UART(With Flow Control)-SAM L21/D21 XPro Pins (Rx-Pin15, Tx-Pin17, RTS-Pin16, CTS-Pin18)
- BTLC1000 Wakeup Pin-SAM L21/D21 XPro Pins (Rx-Pin6)
- BTLC1000 Chip Enable Pin-SAM L21/D21 XPro Pins (Rx-Pin4)
- UART(With Flow Control)-SAM G55/4S Xpro Pins (Rx-Pin13, Tx-Pin14, RTS-Pin5, CTS-Pin6)
- BTLC1000 Wakeup Pin-SAM G55/4S XPro Pins(Pin4)
- BTLC1000 Chip Enable Pin-SAM G55/4S XPro Pins(Pin10)
- BTLC1000 Vcc Pin-SAM L21/D21/G55/4S Xpro Pins(Pin20)
- BTLC1000 GND Pin-SAM L21/D21/G55/4S Xpro Pins(Pin19)
Package
***************************** BluSDK Package *****************************************
- BluSDK -
- ATBTLC1000 -
- Developement kit -
- Applications -
- Support and FAQ visit -