Parameters of the AT_BLE_LECB_ADD_CREDIT_IND message.
#include <at_ble_api.h>
Data Fields | |
uint16_t | dest_credit |
Destination Credit for the LE Credit Based Connection. More... | |
uint16_t | le_psm |
LE Protocol/Service Multiplexer. More... | |
uint16_t | src_credit |
Source Credit for the LE Credit Based Connection. More... | |
uint16_t at_ble_lecb_add_credit_ind_t::dest_credit |
Destination Credit for the LE Credit Based Connection.
uint16_t at_ble_lecb_add_credit_ind_t::le_psm |
LE Protocol/Service Multiplexer.
uint16_t at_ble_lecb_add_credit_ind_t::src_credit |
Source Credit for the LE Credit Based Connection.