Microchip® Advanced Software Framework

at_ble_bus_info_t Struct Reference

#include <at_ble_api.h>

Data Fields

uint8_t btlc1000_uart_pinout_switch
 In case of using AT_BLE_UART as interface this is used to switch UART pin-out, true or false. More...
 
uint32_t bus_baudrate
 UART baudrate value one of at_ble_uart_baudrate_tag values. More...
 
uint8_t bus_type
 Either AT_BLE_UART or AT_BLE_SPI. More...
 
uint8_t host_external_wakeup_gpio
 Select BTLC1000 GPIO for host wakeup, for Wing board select BTLC1000_EXT_PIN9 only, for SoC use the enum values. More...
 

uint8_t at_ble_bus_info_t::btlc1000_uart_pinout_switch

In case of using AT_BLE_UART as interface this is used to switch UART pin-out, true or false.

Referenced by ble_device_init().

uint32_t at_ble_bus_info_t::bus_baudrate

UART baudrate value one of at_ble_uart_baudrate_tag values.

Referenced by ble_device_init().

uint8_t at_ble_bus_info_t::bus_type

Either AT_BLE_UART or AT_BLE_SPI.

Referenced by ble_device_init().

uint8_t at_ble_bus_info_t::host_external_wakeup_gpio

Select BTLC1000 GPIO for host wakeup, for Wing board select BTLC1000_EXT_PIN9 only, for SoC use the enum values.

Referenced by ble_device_init().