Standard I/O (stdio) | Common standard I/O driver that implements the stdio read and write functions on AVR and SAM devices |
 Standard serial I/O (stdio) | Common standard serial I/O management driver that implements a stdio serial interface on AVR and SAM devices |
BLE Manager | BLE Manager provides Common Framework for Application, BLE Profiles, BLE Services, Library and Platform This group includes functionality of GAP, GATT, HTPT, DTM Events and handling the GAP activities |
 BLE GAP Events | This group includes functionality of GAP Events and handling the GAP activities |
 BLE Event Subscription | This group includes functionality of registering the BLE Events from profile/service/application |
 BLE Event Un-Subscribe | This group includes functionality of un-subscribe the BLE Events from BLE Manager |
 BLE Pairing | This group includes functionality of pair request from/to peer device based on the device role |
 Dynamic Advertisement/Scan Data | This group includes functionality of creating the advertisement data and scan data |
 BLE Services Add/Remove | This group includes functionality of adding or removing the components, service, BLE services from ASF Wizard |
 Platform Initialization | This group includes functionality of initializing the BTLC1000 and initializing the Host interface |
GAP APIs | This group includes all GAP APIs; Device Configuration, Address Management, Connections, .. |
 Device Configuration APIs | This group includes GAP device configurations APIs |
 Address Management APIs | This group includes GAP address APIs |
 Advertising Procedure APIs | This group includes advertising APIs |
 Scanning Procedure APIs | This group includes scanning APIs |
 Connecting Procedure APIs | This group includes connections APIs |
 Security APIs | This group includes security APIs |
 Misc APIs | This group includes other GAP related APIs |
 White-List APIs | This group includes GAP White-List related APIs |
GATT Client APIs | This group includes all GATT Client APIs; Discover, Read, Write, .. |
GATT Server APIs | This group includes all GATT Server APIs; Set value, Get value, Notify, Indicate, .. |
L2CAP APIs | This group includes all L2CAP layer APIs |
HTPT APIs | This group includes all HTPT APIs; Database Creation, Send Temperature, .. |
Misc APIs | This group includes APIs which are not belong to any task |
Error codes | This group includes all error codes which was handled by Atmel APIs through different levels |
Direct test Mode APIs (DTM) | This group includes all Direct test mode APIs |
Calibration APIs | This group includes all the Calibration related APIs |
MACROs | This group includes Macros defined to be used of at_ble_trace.h |
Functions | This group includes all function prototypes required to be used |
Examples | |
SAM Serial USART (SERCOM USART) Driver | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the SERCOM module in its USART mode to transfer or receive USART data frames |
Compiler abstraction layer and code utilities | Compiler abstraction layer and code utilities for Cortex-M0+ based Atmel SAM devices |
 Status Codes | |
 Preprocessor - Macro Recursion | |
 Preprocessor - Macro Repeat | |
 Preprocessor - Stringize | |
 Preprocessor - Token Paste | |
Global interrupt management | This is a driver for global enabling and disabling of interrupts |
 Deprecated interrupt definitions | |
Atmel part identification macros | This collection of macros identify which series and families that the various Atmel parts belong to |
 AVR UC3 parts | |
 AVR XMEGA parts | |
 megaAVR parts | |
 SAM parts | |
SAM System (SYSTEM) Driver | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's system relation functionality, necessary for the basic device operation |
SAM System Clock Management (SYSTEM CLOCK) Driver | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's clocking related functions |
SAM System Interrupt (SYSTEM INTERRUPT) Driver | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of internal software and hardware interrupts/exceptions |
SAM System Pin Multiplexer (SYSTEM PINMUX) Driver | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's physical I/O Pins, to alter the direction and input/drive characteristics as well as to configure the pin peripheral multiplexer selection |
Busy-Wait Delay Routines | This module provides simple loop-based delay routines for those applications requiring a brief wait during execution |
SAM External Interrupt (EXTINT) Driver | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of external interrupts generated by the physical device pins, including edge detection |
serial First-In-First-Out Buffer (FIFO) | See fifo_quickstart |
Serial Interface (Serial) | See Quick start guide for Serial Interface service |
SAM Timer/Counter (TC) Driver | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the timer modules within the device, for waveform generation and timing operations |
SAM Port (PORT) Driver | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's General Purpose Input/Output (GPIO) pin functionality, for manual pin state reading and writing |
Generic board support | The generic board support module includes board-specific definitions and function prototypes, such as the board initialization function |
 SAM D21 Xplained Pro board | |
  Features | Symbols that describe features and capabilities of the board |