Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
PXP reporter application

Introduction

******************************Introduction ***********************************

The PXP-Reporter example application bring-up the Proximity profile defined by the Bluetooth SIG which would send the proximity information to Proximity Monitor enbled BLE device. The Proximity Reporter example application supports the following features:

  • Advertisement.
  • Pairing / Bonding.
  • Services: Link Loss Service, Immediate Alert Service and TX Power Service.

The Proximity Reporter example application supports the following characteristics:

  • Immediate Alert Level.
  • Link Loss Alert Level.
  • Transmit Power Level.

Supported Evolution Kit -

  • ATSAML21-XPRO-B + ATBTLC1000 XPRO
  • ATSAMD21-XPRO + ATBTLC1000 XPRO
  • ATSAMG55-XPRO + ATBTLC1000 XPRO
  • ATSAM4S-XPRO + ATBTLC1000 XPRO

Running the demo -

  • 1. Build and flash the binary into supported evaluation board.
  • 2. Open the console using TeraTerm or any serial port monitor.
  • 3. Press the Reset button.
  • 4. Wait for around 10 seconds for the patches to be downloaded device will initialize and start-up.
  • 5. The device is now in advertising mode.
  • 6. On a BLE compatible iPhone®/Android phone, enable Bluetooth in the Settings page. Start the Atmel Smart Connect App and scan for devices. ATMEL-PXP will be appear among the devices scanned. Click on "ATMEL-PXP" to connect to supported platform.
  • 7. Once connected, the client side will request for the pairing procedure . The console log provides a guidance for the user to enter the pass-key.
  • 8. Once paired, the application displays the PXP reporter service.
  • 9. Click on the desired service for configuretion of alert level characteristics
  • 10. After configuration of the desired alert levels, click on desired service and then move the mobile away from reporter. Based on the distance of seperation path loss is reported .

Modules

***************************** MODULES *****************************************

  • BLE Manager -
    • The Event Manager is responsible for handling the following:
      • Generic BLE Event Handling:-
        • BLE Event Manager handles the events triggered by BLE stack and also responsible for invoking all registered callbacks for respective events. BLE Manager handles all GAP related functionality. In addition to that handles multiple connection instances, Pairing, Encryption, Scanning.
      • Handling Multi-role/multi-connection:-
        • BLE Event Manager is responsible for handling multiple connection instances and stores bonding information and Keys to retain the bonded device. BLE Manager is able to identify and remove the device information when pairing/encryption gets failed. In case of multi-role, it handles the state/event handling of both central and peripheral in multiple contexts.
      • Controlling the Advertisement data:-
        • BLE Event Manager is responsible for generating the advertisement and scan response data for BLE profiles/services that are attached with BLE Manager.
  • BLE Profile-
    • The Proximity profile defines the behavior when a device moves away from a peer device so that the connection is dropped or the path loss increases above a preset level, causing an immediate alert. This alert can be used to notify the user about disconnection of the devices from each other. As a consequence of this alert, a device may take further action, for example to lock one of the devices so that it is no longer usable.
    • The Proximity Reporter - shall be a GATT server.

      The Proximity Reporter Profile supports three services:

      • Link Loss service -
        • The Link Loss service defines behavior when a link is lost between two devices.
      • Immediate Alert service -
        • The Immediate Alert service defines behavior when a link is lost between two devices.
      • Tx Power service -
        • The Tx Power service exposes a device’s current transmit power level when in a connection.
  • BLE Platform Services -
    • Interface Settings -
      • Connect ATBTLC1000 XPRO to SAML21-XPRO-B -> EXT1
      • Connect ATBTLC1000 XPRO to SAMD21-XPRO -> EXT1
      • Connect ATBTLC1000 XPRO to SAMG55-XPRO -> EXT1
      • Connect ATBTLC1000 XPRO to SAM4S-XPRO -> EXT1
    • Serial Console COM port settings -
      • Baudrate 115200
      • Parity None, Stop Bit 1, Start Bit 1
      • No Hardware Handshake
    • 6-Wire Mode Connection Setup -
      • Pins are 1:1 match with SAML21/D21 Xpro EXT1 Header to BTLC1000 XPro Header
      • UART(No Flow Control)-SAM L21/D21 XPro Pins (Rx-Pin13, Tx-Pin14)
      • UART(With Flow Control)-SAM G55 Xpro Pins (Rx-Pin13, Tx-Pin14, RTS-Pin5, CTS-Pin6, Rx-Pin16, Tx-Pin17)
      • BTLC1000 Wakeup Pin-SAM G55 XPro Pins(Pin4)
      • BTLC1000 Chip Enable Pin-SAM G55 XPro Pins(Pin10)
      • BTLC1000 Vcc Pin-SAM L21/D21/G55 Xpro Pins(Pin20)
      • BTLC1000 GND Pin-SAM L21/D21/G55 Xpro Pins(Pin19)
    • 4-Wire Mode Connection setup -
      • UART(With Flow Control)-SAM L21/D21 XPro Pins (Rx-Pin15, Tx-Pin17, RTS-Pin16, CTS-Pin18)
      • BTLC1000 Wakeup Pin-SAM L21/D21 XPro Pins (Rx-Pin6)
      • BTLC1000 Chip Enable Pin-SAM L21/D21 XPro Pins (Rx-Pin4)
      • UART(With Flow Control)-SAM G55/4S Xpro Pins (Rx-Pin13, Tx-Pin14, RTS-Pin5, CTS-Pin6)
      • BTLC1000 Wakeup Pin-SAM G55/4S XPro Pins(Pin4)
      • BTLC1000 Chip Enable Pin-SAM G55/4S XPro Pins(Pin10)
      • BTLC1000 Vcc Pin-SAM L21/D21/G55/4S Xpro Pins(Pin20)
      • BTLC1000 GND Pin-SAM L21/D21/G55/4S Xpro Pins(Pin19)

Package

***************************** BluSDK Package *****************************************