Microchip® Advanced Software Framework

•All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
White-List APIs

This group includes GAP White-List related APIs.

Functions

at_ble_status_t at_ble_get_whitelist_size (uint8_t *size)
 Get total number of white list entries that can be stored in the Controller. More...
 
at_ble_status_t at_ble_whitelist_add (at_ble_addr_t *address)
 Adds a peer device address to the white-list. More...
 
at_ble_status_t at_ble_whitelist_clear (void)
 Clear the white-list. More...
 
at_ble_status_t at_ble_whitelist_remove (at_ble_addr_t *address)
 Removes a peer device address from the white-list. More...
 

at_ble_status_t at_ble_get_whitelist_size ( uint8_t *  size)

Get total number of white list entries that can be stored in the Controller.

Parameters
[out]sizeThe white-list size
Note
the returned size is the maximum size of Public address white list only, Randome static address white list has the same size too
Returns
Upon successful completion the function shall return AT_BLE_SUCCESS, Otherwise the function shall return at_ble_status_t
at_ble_status_t at_ble_whitelist_add ( at_ble_addr_t address)

Adds a peer device address to the white-list.

Parameters
[in]addresspeer device address
Note
This command can be used at any time except when:
  • the advertising filter policy uses the white list and advertising is enabled.
  • the scanning filter policy uses the white list and scanning is enabled.
  • the initiator filter policy uses the white list and a create connection command is outstanding.
The only addresses that should be added to the white-list is Public device address or random static device address
In case of connection mode is AUTO, the white-list will be cleared
To get scan results from only peers added to white list, make sure that "filter_whitelist" argument of at_ble_scan_start is true.
Returns
Upon successful completion the function shall return AT_BLE_SUCCESS, Otherwise the function shall return at_ble_status_t
at_ble_status_t at_ble_whitelist_clear ( void  )

Clear the white-list.

Returns
Upon successful completion the function shall return AT_BLE_SUCCESS, Otherwise the function shall return at_ble_status_t
at_ble_status_t at_ble_whitelist_remove ( at_ble_addr_t address)

Removes a peer device address from the white-list.

Parameters
[in]addresspeer device address
Note
This command can be used at any time except when:
  • the advertising filter policy uses the white list and advertising is enabled.
  • the scanning filter policy uses the white list and scanning is enabled.
  • the initiator filter policy uses the white list and a create connection command is outstanding.
Returns
Upon successful completion the function shall return AT_BLE_SUCCESS, Otherwise the function shall return at_ble_status_t