adv_element | |
 adv_element_container | |
 adv_element_t | Advertisement data element |
 at_ble_addr_t | Blue-tooth Low Energy address Type |
 at_ble_adv_cmp_evt_t | Advertising complete event |
 at_ble_adv_data_update_on_the_fly_t | Use this structure when calling the api at_ble_adv_data_update_on_the_fly to set the advertising data on the fly |
 at_ble_adv_report_t | Advertising report status |
 at_ble_att_cfg_t | |
 at_ble_att_info_req_t | |
 at_ble_bus_info_t | |
 at_ble_channel_map_t | Channel Map Structure |
 at_ble_char_list | Encapsulation for a characteristic and its length |
 at_ble_char_presentation_t | Characteristic presentation format |
 at_ble_char_val_t | |
 at_ble_characteristic_changed_t | |
 at_ble_characteristic_configuration_changed_t | |
 at_ble_characteristic_found_t | |
 at_ble_characteristic_read_req_t | |
 at_ble_characteristic_read_response_t | |
 at_ble_characteristic_t | Characteristic structure |
 at_ble_characteristic_write_request_t | Structure received when write to a characteristic is required |
 at_ble_characteristic_write_response_t | |
 at_ble_chr_t | |
 at_ble_cmd_complete_event_t | |
 at_ble_conn_param_update_done_t | |
 at_ble_conn_param_update_request_t | |
 at_ble_connected_t | AT_BLE_CONNECTED message format |
 at_ble_connection_params_t | Connection parameters |
 at_ble_CSRK_t | Connection Signature Resolution Key |
 at_ble_descriptor_found_t | |
 at_ble_dev_config_t | Device configuration |
 at_ble_dev_info | Peer device request to modify local device info such as name or appearance |
  dev_info | Device information data |
   device_name | Device name |
 at_ble_disconnected_t | Handle and Status of disconnected peer |
 at_ble_dtm_t | Data type of DMT status and report, "number_of_packets" will be used only in case of receiving the event AT_BLE_LE_PACKET_REPORT after calling the API |
 at_ble_encryption_request_t | |
 at_ble_encryption_status_changed_t | |
 at_ble_gap_dev_name_t | Device name |
 at_ble_gap_deviceinfo_t | Device info DB at_ble_set_gap_deviceinfo |
 at_ble_gap_irk_t | Identity Resolving Key |
 at_ble_gap_whitelist_t | White-list structure |
 at_ble_gapc_cmp_evt_t | |
 at_ble_gapc_dev_info_val_t | Retrieve information Structure |
 at_ble_gapc_get_info_cmd_t | Retrieve information command Structure |
 at_ble_generic_att_desc_t | |
 at_ble_htpt_cfg_indntf_ind_t | Parameters of the AT_BLE_HTPT_CFG_INDNTF_IND message |
 at_ble_htpt_create_db_cfm_t | Parameters of the AT_BLE_HTPT_CREATE_DB_CFM message |
 at_ble_htpt_db_cfg | Parameters of the Health thermometer service database |
 at_ble_htpt_disable_ind_t | Parameters of the AT_BLE_HTPT_DISABLE_IND message |
 at_ble_htpt_enable_rsp_t | Parameters of the AT_BLE_HTPT_ENABLE_RSP message |
 at_ble_htpt_meas_intv_chg_ind_t | Parameters of the AT_BLE_HTPT_MEAS_INTV_CHG_IND message |
 at_ble_htpt_meas_intv_chg_req_t | Parameters of the AT_BLE_HTPT_MEAS_INTV_CHG_REQ message |
 at_ble_htpt_meas_intv_upd_rsp_t | Parameters of the AT_BLE_HTPT_MEAS_INTV_UPD_RSP message |
 at_ble_htpt_temp_send_cfm_t | Parameters of the AT_BLE_HTPT_TEMP_SEND_CFM message |
 at_ble_inc_srv_t | |
 at_ble_included_service_found_t | |
 at_ble_included_service_t | Service Definition |
 at_ble_indication_confirmed_t | |
 at_ble_indication_recieved_t | |
 at_ble_init_config_t | |
 at_ble_IRK_t | IRKey |
 at_ble_lecb_add_credit_ind_t | Parameters of the AT_BLE_LECB_ADD_CREDIT_IND message |
 at_ble_lecb_conn_req_t | Parameters of the AT_BLE_LECB_CONN_REQ message |
 at_ble_lecb_connected_t | Parameters of the AT_BLE_LECB_CONNECTED message |
 at_ble_lecb_data_recv_t | Parameters of the AT_BLE_LECB_DATA_RECIEVED message |
 at_ble_lecb_disconnected_t | Parameters of the AT_BLE_LECB_DISCONNECTED message |
 at_ble_lecb_send_rsp_t | Parameters of the AT_BLE_LECB_SEND_RESP message |
 at_ble_LTK_t | Long Term Key |
 at_ble_mempool_t | |
 at_ble_mtu_changed_ind_t | MTU changed value |
 at_ble_notification_recieved_t | |
 at_ble_pair_done_t | Pairing done message |
 at_ble_pair_features_t | Pairing Features |
 at_ble_pair_key_request_t | |
 at_ble_pair_request_t | |
 at_ble_peer_att_info_ind_t | Peer attribute info structure GAPC_GET_DEV_INFO_REQ_IND |
 at_ble_prf_date_time_t | Time profile information |
 at_ble_prf_server_error_ind_t | Message structure used to inform APP that an error has occurred in the profile server role task |
 at_ble_primary_service_found_t | |
 at_ble_read_authorize_request_t | |
 at_ble_resolv_rand_addr_status_t | |
 at_ble_rx_power_value_t | |
 at_ble_scan_info_t | Scan Information |
 at_ble_scan_report_t | Scan report status |
 at_ble_server_config_desc_t | |
 at_ble_service_t | |
 at_ble_sign_counter_t | Signature counter |
 at_ble_signature_info_t | Connection Signature information |
 at_ble_slave_sec_request_t | |
 at_ble_spcp_t | Slave preferred connection parameters |
 at_ble_user_desc_t | |
 at_ble_uuid_t | UUID type |
 ble_connected_dev_info | |
 ble_connected_dev_info_t | BLE manager maintains the device connection information, device role, bonding information, device connection state and Long Term Key |
 ble_custom_event_cb | |
 ble_custom_event_cb_t | All BLE Custom event callback types |
 ble_dtm_event_cb | |
 ble_dtm_event_cb_t | All BLE DTM event callback types |
 ble_gap_event_cb | |
 ble_gap_event_cb_t | BLE GAP Event callback types |
 ble_gatt_client_event_cb | |
 ble_gatt_client_event_cb_t | All BLE GATT Client callback types |
 ble_gatt_server_event_cb | |
 ble_gatt_server_event_cb_t | All BLE GATT Server callback types |
 ble_htpt_event_cb | |
 ble_htpt_event_cb_t | All BLE HTPT event callback types |
 ble_l2cap_event_cb | |
 ble_l2cap_event_cb_t | All BLE L2CAP callback types |
 gatt_cts_handler | |
 gatt_dst_handler | |
 gatt_rtu_handler | |
 gatt_service_handler | |
 gatt_service_handler_t | GATT services handles |
 genclk_config | Hardware representation of a set of generic clock parameters |
 hw_timer_tag | |
 os_signal | |
 pdc_packet | PDC data packet for transfer |
 platform_api_list_tag | |
 pll_config | Hardware-specific representation of PLL configuration |
 prf_date_time | Time profile information |
 prf_server_error_ind | Message structure used to inform APP that an error has occurred in the profile server role task |
 s_interrupt_source | Describes a PIO interrupt source, including the PIO instance triggering the interrupt and the associated interrupt handler |
 sam_uart_opt | Option list for UART peripheral initialization |
 sam_usart_opt_t | |
 scan_resp_element | |
 ser_fifo_desc | FIFO descriptor used by FIFO driver |
 StructCPtr | Structure of pointers to constant 64-, 32-, 16- and 8-bit unsigned integers |
 StructCVPtr | Structure of pointers to constant volatile 64-, 32-, 16- and 8-bit unsigned integers |
 StructPtr | Structure of pointers to 64-, 32-, 16- and 8-bit unsigned integers |
 StructVPtr | Structure of pointers to volatile 64-, 32-, 16- and 8-bit unsigned integers |
 uart_config_optical | |
 uart_rs232_options | Input parameters when initializing RS232 and similar modes |
 Union16 | 16-bit union |
 Union32 | 32-bit union |
 Union64 | 64-bit union |
 UnionCPtr | Union of pointers to constant 64-, 32-, 16- and 8-bit unsigned integers |
 UnionCVPtr | Union of pointers to constant volatile 64-, 32-, 16- and 8-bit unsigned integers |
 UnionPtr | Union of pointers to 64-, 32-, 16- and 8-bit unsigned integers |
 UnionVPtr | Union of pointers to volatile 64-, 32-, 16- and 8-bit unsigned integers |
 usart_iso7816_opt_t | |
 usart_spi_opt_t | |
 user_custom_event | |