NV component header.
The segment D_NV_MEMORY must be defined and reserved in the linker script (.xcl file), for example like this:
-D_D_NV_MEMORY_START=400 -D_D_NV_MEMORY_SIZE=4000
-Z(CODE)D_NV_MEMORY+_D_NV_MEMORY_SIZE=[_D_NV_MEMORY_START:+_D_NV_MEMORY_SIZE]
Note that nothing should actually be placed in the segment. These linker script commands will ensure that the entire range is reserved and not programmed (left as 0xff).
The segment should start on a flash page boundary, and the size should correspond to the define D_NV_MEMORY_SIZE.
Further, since the device can only erase a whole page and not arbitrary locations in flash, the sector size must be an integer multiple of the flash page size. Otherwise, erasing the first or last page of a sector will also erase content in flash locations neighbouring the sector.
Copyright (c) 2018 Microchip Technology Inc. and its subsidiaries.
#include <compiler.h>
Macros | |
#define | ADD_COMMA(value, n) value, |
#define | ARRAY_SIZE(a) (sizeof(a)/sizeof(a[0])) |
#define | CEIL(a, b) (((a) - 1U)/(b) + 1U) |
#define | COMPARE_WITH_THRESHOLD(a, b, threshold) (abs((a) - (b)) < (threshold) ? ((a) > (b) ? 1 : 0) : ((a) > (b) ? 0 : 1)) |
#define | D_NV_FIRST_SECTOR 0 |
#define | D_NV_MEMORY_SIZE (D_NV_SECTOR_COUNT * D_NV_SECTOR_SIZE) |
#define | D_NV_SECTOR_COUNT 2 |
#define | D_NV_SECTOR_SIZE (8192U) |
#define | FIELD_OFFSET(struct_type, field_name) (((uint8_t*) &((struct_type *)(NULL))->field_name) - (uint8_t*)NULL) |
#define | FIRST_BIT_CLEARED(bitmask) (~(bitmask) & ((bitmask) + 1)) |
#define | FIRST_BIT_SET(bitmask) ((bitmask) & (~(bitmask) + 1)) |
#define | FLASH_PTR |
#define | GET_CONST_PARENT_BY_FIELD(TYPE, FIELD, FIELD_POINTER) ((const TYPE *)(((const uint8_t *)FIELD_POINTER) - offsetof(TYPE, FIELD))) |
#define | GET_FIELD_PTR(structPtr, typeName, fieldName) ((uint8_t *)(structPtr) + offsetof(typeName, fieldName)) |
#define | GET_INDEX_FROM_OFFSET(PTR1, PTR2) (PTR1 - PTR2) |
#define | GET_PARENT_BY_FIELD(TYPE, FIELD, FIELD_POINTER) ((TYPE *)(((uint8_t *)FIELD_POINTER) - offsetof(TYPE, FIELD))) |
#define | GET_STRUCT_BY_FIELD_POINTER(struct_type, field_name, field_pointer) ((struct_type *) (((uint8_t *) field_pointer) - FIELD_OFFSET(struct_type, field_name))) |
#define | INIT_ARRAY(initValue, size) {REPEAT_MACRO(ADD_COMMA, initValue, size)} |
#define | MAX(x, y) ((x)<(y)?(y):(x)) |
#define | MIN(x, y) ((x)<(y)?(x):(y)) |
#define | SLICE_SIZE(type, firstField, lastField) (offsetof(type, lastField) - offsetof(type, firstField) + sizeof(((type *)0)->lastField)) |
Typedefs | |
typedef uint16_t | D_Nv_Size_t |
Functions | |
void | D_Nv_EraseSector (uint8_t sector) |
Erases a sector of the internal NV. More... | |
bool | D_Nv_IsEmpty (uint8_t sector, uint16_t offset, D_Nv_Size_t numberOfBytes) |
Checks if the requested range is empty (containing all 0xFF). More... | |
bool | D_Nv_IsEqual (uint8_t sector, uint16_t offset, uint8_t *pBuffer, D_Nv_Size_t numberOfBytes) |
Compare bytes with contents of the internal NV. More... | |
void | D_Nv_Read (uint8_t sector, uint16_t offset, uint8_t *pBuffer, D_Nv_Size_t numberOfBytes) |
Read bytes from the internal NV. More... | |
void | D_Nv_SetSystemIntegrityCheckFunction (void(*pf)(void)) |
The function to set system integrity check callback function. More... | |
void | D_Nv_Write (uint8_t sector, uint16_t offset, uint8_t *pBuffer, D_Nv_Size_t numberOfBytes) |
Write bytes to the internal NV. More... | |
#define ADD_COMMA | ( | value, | |
n | |||
) | value, |
#define ARRAY_SIZE | ( | a | ) | (sizeof(a)/sizeof(a[0])) |
#define CEIL | ( | a, | |
b | |||
) | (((a) - 1U)/(b) + 1U) |
#define COMPARE_WITH_THRESHOLD | ( | a, | |
b, | |||
threshold | |||
) | (abs((a) - (b)) < (threshold) ? ((a) > (b) ? 1 : 0) : ((a) > (b) ? 0 : 1)) |
#define D_NV_FIRST_SECTOR 0 |
Referenced by CompareData(), D_Nv_EraseSector(), D_Nv_Read(), and D_Nv_Write().
#define D_NV_MEMORY_SIZE (D_NV_SECTOR_COUNT * D_NV_SECTOR_SIZE) |
Referenced by D_Nv_Init().
#define D_NV_SECTOR_COUNT 2 |
#define D_NV_SECTOR_SIZE (8192U) |
Referenced by CompareData(), D_Nv_EraseSector(), D_Nv_Init(), D_Nv_Read(), and D_Nv_Write().
#define FIELD_OFFSET | ( | struct_type, | |
field_name | |||
) | (((uint8_t*) &((struct_type *)(NULL))->field_name) - (uint8_t*)NULL) |
#define FIRST_BIT_CLEARED | ( | bitmask | ) | (~(bitmask) & ((bitmask) + 1)) |
#define FIRST_BIT_SET | ( | bitmask | ) | ((bitmask) & (~(bitmask) + 1)) |
#define FLASH_PTR |
Referenced by CompareData(), D_Nv_Read(), and pdsInitItemMask().
#define GET_CONST_PARENT_BY_FIELD | ( | TYPE, | |
FIELD, | |||
FIELD_POINTER | |||
) | ((const TYPE *)(((const uint8_t *)FIELD_POINTER) - offsetof(TYPE, FIELD))) |
#define GET_FIELD_PTR | ( | structPtr, | |
typeName, | |||
fieldName | |||
) | ((uint8_t *)(structPtr) + offsetof(typeName, fieldName)) |
#define GET_INDEX_FROM_OFFSET | ( | PTR1, | |
PTR2 | |||
) | (PTR1 - PTR2) |
#define GET_PARENT_BY_FIELD | ( | TYPE, | |
FIELD, | |||
FIELD_POINTER | |||
) | ((TYPE *)(((uint8_t *)FIELD_POINTER) - offsetof(TYPE, FIELD))) |
#define GET_STRUCT_BY_FIELD_POINTER | ( | struct_type, | |
field_name, | |||
field_pointer | |||
) | ((struct_type *) (((uint8_t *) field_pointer) - FIELD_OFFSET(struct_type, field_name))) |
#define INIT_ARRAY | ( | initValue, | |
size | |||
) | {REPEAT_MACRO(ADD_COMMA, initValue, size)} |
#define MAX | ( | x, | |
y | |||
) | ((x)<(y)?(y):(x)) |
#define MIN | ( | x, | |
y | |||
) | ((x)<(y)?(x):(y)) |
#define SLICE_SIZE | ( | type, | |
firstField, | |||
lastField | |||
) | (offsetof(type, lastField) - offsetof(type, firstField) + sizeof(((type *)0)->lastField)) |
typedef uint16_t D_Nv_Size_t |
void D_Nv_EraseSector | ( | uint8_t | sector | ) |
Erases a sector of the internal NV.
sector | The sector to erase (0..D_NV_SECTOR_COUNT) |
References D_NV_FIRST_SECTOR, D_NV_MEMORY_END, D_NV_MEMORY_START, D_NV_SECTOR_SIZE, and nvm_erase_row().
bool D_Nv_IsEmpty | ( | uint8_t | sector, |
uint16_t | offset, | ||
D_Nv_Size_t | numberOfBytes | ||
) |
Checks if the requested range is empty (containing all 0xFF).
sector | The sector to use (0..D_NV_SECTOR_COUNT) |
offset | The start offset to check |
numberOfBytes | The number of bytes to check |
References CompareData().
bool D_Nv_IsEqual | ( | uint8_t | sector, |
uint16_t | offset, | ||
uint8_t * | pBuffer, | ||
D_Nv_Size_t | numberOfBytes | ||
) |
Compare bytes with contents of the internal NV.
sector | The sector to use (0..D_NV_SECTOR_COUNT) | |
offset | The offset to start comparing with | |
[in] | pBuffer | The start address of the buffer that contains the data to compare with |
numberOfBytes | The number of bytes to compare |
References CompareData().
void D_Nv_Read | ( | uint8_t | sector, |
uint16_t | offset, | ||
uint8_t * | pBuffer, | ||
D_Nv_Size_t | numberOfBytes | ||
) |
Read bytes from the internal NV.
sector | The sector to use (0..D_NV_SECTOR_COUNT) | |
offset | The offset to start reading at | |
[out] | pBuffer | The start address of the buffer to store the read data to |
numberOfBytes | The number of bytes to read |
References D_NV_FIRST_SECTOR, D_NV_MEMORY_END, D_NV_MEMORY_START, D_NV_SECTOR_SIZE, and FLASH_PTR.
void D_Nv_SetSystemIntegrityCheckFunction | ( | void(*)(void) | pf | ) |
The function to set system integrity check callback function.
References s_pfSystemCheckCallback.
void D_Nv_Write | ( | uint8_t | sector, |
uint16_t | offset, | ||
uint8_t * | pBuffer, | ||
D_Nv_Size_t | numberOfBytes | ||
) |
Write bytes to the internal NV.
sector | The sector to use (0..D_NV_SECTOR_COUNT) | |
offset | The offset to start writing to | |
[in] | pBuffer | The start address of the buffer that contains the data to write |
numberOfBytes | The number of bytes to write |
References D_NV_FIRST_SECTOR, D_NV_MEMORY_END, D_NV_MEMORY_START, D_NV_SECTOR_SIZE, MIN, nvm_write_buffer(), s_pfSystemCheckCallback, STATUS_BUSY, STATUS_OK, system_interrupt_enter_critical_section(), and system_interrupt_leave_critical_section().