Data Structures | |
struct | i2c_master_config |
Configuration structure for the I2C Master device. More... | |
struct | i2c_master_module |
SERCOM I2C Master driver software device instance structure. More... | |
struct | i2c_master_packet |
I2C master packet for read/write. More... | |
Enumerations | |
enum | i2c_master_baud_rate { I2C_MASTER_BAUD_RATE_100KHZ = 100, I2C_MASTER_BAUD_RATE_400KHZ = 400 } |
I2C frequencies. More... | |
enum | i2c_master_inactive_timeout { I2C_MASTER_INACTIVE_TIMEOUT_DISABLED = SERCOM_I2CM_CTRLA_INACTOUT(0), I2C_MASTER_INACTIVE_TIMEOUT_55US = SERCOM_I2CM_CTRLA_INACTOUT(1), I2C_MASTER_INACTIVE_TIMEOUT_105US = SERCOM_I2CM_CTRLA_INACTOUT(2), I2C_MASTER_INACTIVE_TIMEOUT_205US = SERCOM_I2CM_CTRLA_INACTOUT(3) } |
Values for inactive bus time-out. More... | |
enum | i2c_master_interrupt_flag { I2C_MASTER_INTERRUPT_WRITE = 0, I2C_MASTER_INTERRUPT_READ = 1 } |
Interrupt flags. More... | |
enum | i2c_master_start_hold_time { I2C_MASTER_START_HOLD_TIME_DISABLED = SERCOM_I2CM_CTRLA_SDAHOLD(0), I2C_MASTER_START_HOLD_TIME_50NS_100NS = SERCOM_I2CM_CTRLA_SDAHOLD(1), I2C_MASTER_START_HOLD_TIME_300NS_600NS = SERCOM_I2CM_CTRLA_SDAHOLD(2), I2C_MASTER_START_HOLD_TIME_400NS_800NS = SERCOM_I2CM_CTRLA_SDAHOLD(3) } |
Values for hold time after start bit. More... | |
Lock/Unlock | |
static enum status_code | i2c_master_lock (struct i2c_master_module *const module) |
Attempt to get lock on driver instance. More... | |
static void | i2c_master_unlock (struct i2c_master_module *const module) |
Unlock driver instance. More... | |
Configuration and Initialization | |
static bool | i2c_master_is_syncing (const struct i2c_master_module *const module) |
Returns the synchronization status of the module. More... | |
static void | i2c_master_get_config_defaults (struct i2c_master_config *const config) |
Gets the I2C master default configurations. More... | |
enum status_code | i2c_master_init (struct i2c_master_module *const module, Sercom *const hw, const struct i2c_master_config *const config) |
Initializes the requested I2C hardware module. More... | |
static void | i2c_master_enable (const struct i2c_master_module *const module) |
Enables the I2C module. More... | |
static void | i2c_master_disable (const struct i2c_master_module *const module) |
Disable the I2C module. More... | |
void | i2c_master_reset (struct i2c_master_module *const module) |
Resets the hardware module. More... | |
Read and Write | |
enum status_code | i2c_master_read_packet_wait (struct i2c_master_module *const module, struct i2c_master_packet *const packet) |
Reads data packet from slave. More... | |
enum status_code | i2c_master_read_packet_wait_no_stop (struct i2c_master_module *const module, struct i2c_master_packet *const packet) |
Reads data packet from slave without sending a stop condition when done. More... | |
enum status_code | i2c_master_write_packet_wait (struct i2c_master_module *const module, struct i2c_master_packet *const packet) |
Writes data packet to slave. More... | |
enum status_code | i2c_master_write_packet_wait_no_stop (struct i2c_master_module *const module, struct i2c_master_packet *const packet) |
Writes data packet to slave without sending a stop condition when done. More... | |
void | i2c_master_send_stop (struct i2c_master_module *const module) |
Sends stop condition on bus. More... | |
void | i2c_master_send_nack (struct i2c_master_module *const module) |
Sends nack signal on bus. More... | |
enum status_code | i2c_master_read_byte (struct i2c_master_module *const module, uint8_t *byte) |
Reads one byte data from slave. More... | |
enum status_code | i2c_master_write_byte (struct i2c_master_module *const module, uint8_t byte) |
Write one byte data to slave. More... | |
enum status_code | i2c_master_read_packet_wait_no_nack (struct i2c_master_module *const module, struct i2c_master_packet *const packet) |
Reads data packet from slave without sending a nack signal and a stop condition when done. More... | |
enum i2c_master_baud_rate |
I2C frequencies.
Values for I2C speeds supported by the module. The driver will also support setting any other value, in which case set the value in the i2c_master_config at desired value divided by 1000.
Example: If 10KHz operation is required, give baud_rate in the configuration structure the value 10.
Enumerator | |
---|---|
I2C_MASTER_BAUD_RATE_100KHZ |
Baud rate at 100KHz (Standard-mode) |
I2C_MASTER_BAUD_RATE_400KHZ |
Baud rate at 400KHz (Fast-mode) |
Values for inactive bus time-out.
If the inactive bus time-out is enabled and the bus is inactive for longer than the time-out setting, the bus state logic will be set to idle.
Values for hold time after start bit.
Values for the possible I2C master mode SDA internal hold times after start bit has been sent.
|
inlinestatic |
Disable the I2C module.
Disables the requested I2C module.
[in] | module | Pointer to the software module struct |
References _sercom_get_interrupt_vector(), Assert, and system_interrupt_disable().
Referenced by i2c_master_reset().
|
inlinestatic |
Enables the I2C module.
Enables the requested I2C module and set the bus state to IDLE after the specified timeout period if no stop bit is detected.
[in] | module | Pointer to the software module struct |
References _sercom_get_interrupt_vector(), Assert, and system_interrupt_enable().
Referenced by edbg_eui_read_eui64().
|
inlinestatic |
Gets the I2C master default configurations.
Use to initialize the configuration structure to known default values.
The default configuration is as follows:
Those default configuration only available if the device supports it:
[out] | config | Pointer to configuration structure to be initiated |
References Assert, i2c_master_config::baud_rate, i2c_master_config::buffer_timeout, GCLK_GENERATOR_0, i2c_master_config::generator_source, I2C_MASTER_BAUD_RATE_100KHZ, I2C_MASTER_INACTIVE_TIMEOUT_DISABLED, I2C_MASTER_START_HOLD_TIME_300NS_600NS, i2c_master_config::inactive_timeout, PINMUX_DEFAULT, i2c_master_config::pinmux_pad0, i2c_master_config::pinmux_pad1, i2c_master_config::run_in_standby, i2c_master_config::scl_low_timeout, i2c_master_config::sda_scl_rise_time_ns, i2c_master_config::start_hold_time, and i2c_master_config::unknown_bus_state_timeout.
Referenced by edbg_eui_read_eui64().
enum status_code i2c_master_init | ( | struct i2c_master_module *const | module, |
Sercom *const | hw, | ||
const struct i2c_master_config *const | config | ||
) |
Initializes the requested I2C hardware module.
Initializes the SERCOM I2C master device requested and sets the provided software module struct. Run this function before any further use of the driver.
[out] | module | Pointer to software module struct |
[in] | hw | Pointer to the hardware instance |
[in] | config | Pointer to the configuration struct |
STATUS_OK | Module initiated correctly |
STATUS_ERR_DENIED | If module is enabled |
STATUS_BUSY | If module is busy resetting |
STATUS_ERR_ALREADY_INITIALIZED | If setting other GCLK generator than previously set |
STATUS_ERR_BAUDRATE_UNAVAILABLE | If given baudrate is not compatible with set GCLK frequency |
References _sercom_get_sercom_inst_index(), _sercom_instances, _sercom_set_handler(), Assert, i2c_master_config::generator_source, sercom_set_gclk_generator(), system_gclk_chan_config::source_generator, STATUS_BUSY, STATUS_ERR_DENIED, STATUS_OK, system_apb_clock_set_mask(), SYSTEM_CLOCK_APB_APBC, SYSTEM_CLOCK_APB_APBD, system_gclk_chan_enable(), system_gclk_chan_get_config_defaults(), and system_gclk_chan_set_config().
Referenced by edbg_eui_read_eui64().
|
inlinestatic |
Returns the synchronization status of the module.
Returns the synchronization status of the module.
[in] | module | Pointer to software module structure |
true | Module is busy synchronizing |
false | Module is not synchronizing |
References Assert.
|
inlinestatic |
Attempt to get lock on driver instance.
This function checks the instance's lock, which indicates whether or not it is currently in use, and sets the lock if it was not already set.
The purpose of this is to enable exclusive access to driver instances, so that, e.g., transactions by different services will not interfere with each other.
[in,out] | module | Pointer to the driver instance to lock |
STATUS_OK | If the module was locked |
STATUS_BUSY | If the module was already locked |
References STATUS_BUSY, STATUS_OK, system_interrupt_enter_critical_section(), and system_interrupt_leave_critical_section().
enum status_code i2c_master_read_byte | ( | struct i2c_master_module *const | module, |
uint8_t * | byte | ||
) |
Reads one byte data from slave.
[in,out] | module | Pointer to software module struct |
[out] | byte | Read one byte data to slave |
STATUS_OK | One byte was read successfully |
STATUS_ERR_TIMEOUT | If no response was given within specified timeout period |
STATUS_ERR_DENIED | If error on bus |
STATUS_ERR_PACKET_COLLISION | If arbitration is lost |
STATUS_ERR_BAD_ADDRESS | If slave is busy, or no slave acknowledged the address |
References _i2c_master_wait_for_bus().
enum status_code i2c_master_read_packet_wait | ( | struct i2c_master_module *const | module, |
struct i2c_master_packet *const | packet | ||
) |
Reads data packet from slave.
Reads a data packet from the specified slave address on the I2C bus and sends a stop condition when finished.
[in,out] | module | Pointer to software module struct |
[in,out] | packet | Pointer to I2C packet to transfer |
STATUS_OK | The packet was read successfully |
STATUS_ERR_TIMEOUT | If no response was given within specified timeout period |
STATUS_ERR_DENIED | If error on bus |
STATUS_ERR_PACKET_COLLISION | If arbitration is lost |
STATUS_ERR_BAD_ADDRESS | If slave is busy, or no slave acknowledged the address |
References _i2c_master_read_packet(), Assert, and STATUS_BUSY.
Referenced by edbg_eui_read_eui64().
enum status_code i2c_master_read_packet_wait_no_nack | ( | struct i2c_master_module *const | module, |
struct i2c_master_packet *const | packet | ||
) |
Reads data packet from slave without sending a nack signal and a stop condition when done.
Starts blocking read operation. Reads a data packet from the specified slave address on the I2C bus without sending a nack signal and a stop condition when done, thus retaining ownership of the bus when done. To end the transaction, a read or write with stop condition must be performed.
[in,out] | module | Pointer to software module struct |
[in,out] | packet | Pointer to I2C packet to transfer |
STATUS_OK | The packet was read successfully |
STATUS_ERR_TIMEOUT | If no response was given within specified timeout period |
STATUS_ERR_DENIED | If error on bus |
STATUS_ERR_PACKET_COLLISION | If arbitration is lost |
STATUS_ERR_BAD_ADDRESS | If slave is busy, or no slave acknowledged the address |
References _i2c_master_read_packet(), Assert, and STATUS_BUSY.
enum status_code i2c_master_read_packet_wait_no_stop | ( | struct i2c_master_module *const | module, |
struct i2c_master_packet *const | packet | ||
) |
Reads data packet from slave without sending a stop condition when done.
Reads a data packet from the specified slave address on the I2C bus without sending a stop condition when done, thus retaining ownership of the bus when done. To end the transaction, a read or write with stop condition must be performed.
[in,out] | module | Pointer to software module struct |
[in,out] | packet | Pointer to I2C packet to transfer |
STATUS_OK | The packet was read successfully |
STATUS_ERR_TIMEOUT | If no response was given within specified timeout period |
STATUS_ERR_DENIED | If error on bus |
STATUS_ERR_PACKET_COLLISION | If arbitration is lost |
STATUS_ERR_BAD_ADDRESS | If slave is busy, or no slave acknowledged the address |
References _i2c_master_read_packet(), Assert, and STATUS_BUSY.
void i2c_master_reset | ( | struct i2c_master_module *const | module | ) |
Resets the hardware module.
Reset the module to hardware defaults.
[in,out] | module | Pointer to software module structure |
References _sercom_get_interrupt_vector(), Assert, i2c_master_disable(), system_interrupt_clear_pending(), system_interrupt_enter_critical_section(), and system_interrupt_leave_critical_section().
Referenced by edbg_eui_read_eui64().
void i2c_master_send_nack | ( | struct i2c_master_module *const | module | ) |
Sends nack signal on bus.
Sends a nack signal on bus.
[in,out] | module | Pointer to the software instance struct |
References Assert.
void i2c_master_send_stop | ( | struct i2c_master_module *const | module | ) |
Sends stop condition on bus.
Sends a stop condition on bus.
[in,out] | module | Pointer to the software instance struct |
References Assert.
|
inlinestatic |
Unlock driver instance.
This function clears the instance lock, indicating that it is available for use.
[in,out] | module | Pointer to the driver instance to lock |
STATUS_OK | If the module was locked |
STATUS_BUSY | If the module was already locked |
enum status_code i2c_master_write_byte | ( | struct i2c_master_module *const | module, |
uint8_t | byte | ||
) |
Write one byte data to slave.
[in,out] | module | Pointer to software module struct |
[in] | byte | Send one byte data to slave |
STATUS_OK | One byte was write successfully |
STATUS_ERR_TIMEOUT | If no response was given within specified timeout period |
STATUS_ERR_DENIED | If error on bus |
STATUS_ERR_PACKET_COLLISION | If arbitration is lost |
STATUS_ERR_BAD_ADDRESS | If slave is busy, or no slave acknowledged the address |
References _i2c_master_wait_for_bus().
enum status_code i2c_master_write_packet_wait | ( | struct i2c_master_module *const | module, |
struct i2c_master_packet *const | packet | ||
) |
Writes data packet to slave.
Writes a data packet to the specified slave address on the I2C bus and sends a stop condition when finished.
[in,out] | module | Pointer to software module struct |
[in,out] | packet | Pointer to I2C packet to transfer |
STATUS_OK | If packet was write successfully |
STATUS_BUSY | If master module is busy with a job |
STATUS_ERR_DENIED | If error on bus |
STATUS_ERR_PACKET_COLLISION | If arbitration is lost |
STATUS_ERR_BAD_ADDRESS | If slave is busy, or no slave acknowledged the address |
STATUS_ERR_TIMEOUT | If timeout occurred |
STATUS_ERR_OVERFLOW | If slave did not acknowledge last sent data, indicating that slave does not want more data and was not able to read last data sent |
References _i2c_master_write_packet(), Assert, and STATUS_BUSY.
enum status_code i2c_master_write_packet_wait_no_stop | ( | struct i2c_master_module *const | module, |
struct i2c_master_packet *const | packet | ||
) |
Writes data packet to slave without sending a stop condition when done.
Writes a data packet to the specified slave address on the I2C bus without sending a stop condition, thus retaining ownership of the bus when done. To end the transaction, a read or write with stop condition or sending a stop with the i2c_master_send_stop function must be performed.
[in,out] | module | Pointer to software module struct |
[in,out] | packet | Pointer to I2C packet to transfer |
STATUS_OK | If packet was write successfully |
STATUS_BUSY | If master module is busy |
STATUS_ERR_DENIED | If error on bus |
STATUS_ERR_PACKET_COLLISION | If arbitration is lost |
STATUS_ERR_BAD_ADDRESS | If slave is busy, or no slave acknowledged the address |
STATUS_ERR_TIMEOUT | If timeout occurred |
STATUS_ERR_OVERFLOW | If slave did not acknowledge last sent data, indicating that slave do not want more data |
References _i2c_master_write_packet(), Assert, and STATUS_BUSY.
Referenced by edbg_eui_read_eui64().