The linkaddr module is an abstract representation of addresses in Rime.
Data Structures | |
union | linkaddr_t |
Files | |
file | linkaddr.c |
Functions for manipulating Rime addresses | |
file | linkaddr.h |
Header file for the Rime address representation | |
Macros | |
#define | LINKADDR_SIZE LINKADDR_CONF_SIZE |
Functions | |
int | linkaddr_cmp (const linkaddr_t *addr1, const linkaddr_t *addr2) |
Compare two Rime addresses. More... | |
void | linkaddr_copy (linkaddr_t *dest, const linkaddr_t *from) |
Copy a Rime address. More... | |
void | linkaddr_set_node_addr (linkaddr_t *addr) |
Set the address of the current node. More... | |
Variables | |
linkaddr_t | linkaddr_node_addr |
The Rime address of the node. More... | |
linkaddr_t | linkaddr_node_addr |
The Rime address of the node. More... | |
const linkaddr_t | linkaddr_null = { { 0, 0, 0, 0, 0, 0, 0, 0 } } |
The null Rime address. More... | |
const linkaddr_t | linkaddr_null |
The null Rime address. More... | |
#define LINKADDR_SIZE LINKADDR_CONF_SIZE |
Referenced by input(), linkaddr_cmp(), and linkaddr_copy().
int linkaddr_cmp | ( | const linkaddr_t * | addr1, |
const linkaddr_t * | addr2 | ||
) |
Compare two Rime addresses.
addr1 | The first address |
addr2 | The second address |
This function compares two Rime addresses and returns the result of the comparison. The function acts like the '==' operator and returns non-zero if the addresses are the same, and zero if the addresses are different.
References LINKADDR_SIZE.
Referenced by create(), index_from_lladdr(), input_packet(), mac_sequence_is_duplicate(), mac_sequence_register_seqno(), neighbor_queue_from_addr(), packet_input(), send_one_packet(), send_packet(), uip_ds6_link_neighbor_callback(), and uip_over_mesh_send().
void linkaddr_copy | ( | linkaddr_t * | dest, |
const linkaddr_t * | from | ||
) |
Copy a Rime address.
dest | The destination |
from | The source This function copies a Rime address from one location to another. |
References LINKADDR_SIZE.
Referenced by create(), frame802154_parse(), input(), linkaddr_set_node_addr(), mac_sequence_register_seqno(), nbr_table_add_lladdr(), output(), packetbuf_attr_clear(), packetbuf_set_addr(), send_packet(), uip_over_mesh_make_announced_gateway(), uip_over_mesh_send(), and uip_over_mesh_set_gateway().
void linkaddr_set_node_addr | ( | linkaddr_t * | addr | ) |
Set the address of the current node.
addr | The address This function sets the Rime address of the node. |
References linkaddr_copy().
Referenced by set_link_addr().
linkaddr_t linkaddr_node_addr |
The Rime address of the node.
This variable contains the Rime address of the node. This variable should not be changed directly; rather, the linkaddr_set_node_addr() function should be used.
Referenced by create(), gateway_announce_recv(), init(), input_packet(), packet_input(), print_stats(), recv_data(), send_data(), send_one_packet(), send_packet(), uip_over_mesh_init(), uip_over_mesh_make_announced_gateway(), and uip_over_mesh_send().
linkaddr_t linkaddr_node_addr |
The Rime address of the node.
This variable contains the Rime address of the node. This variable should not be changed directly; rather, the linkaddr_set_node_addr() function should be used.
Referenced by create(), gateway_announce_recv(), init(), input_packet(), packet_input(), print_stats(), recv_data(), send_data(), send_one_packet(), send_packet(), uip_over_mesh_init(), uip_over_mesh_make_announced_gateway(), and uip_over_mesh_send().
const linkaddr_t linkaddr_null = { { 0, 0, 0, 0, 0, 0, 0, 0 } } |
The null Rime address.
This variable contains the null Rime address. The null address is used in route tables to indicate that the table entry is unused. Nodes with no configured address has the null address. Nodes with their node address set to the null address will have problems communicating with other nodes.
Referenced by create(), frame802154_parse(), index_from_lladdr(), input_packet(), nbr_table_add_lladdr(), output(), packet_input(), packetbuf_attr_clear(), send_one_packet(), send_packet(), uip_ds6_link_neighbor_callback(), and uip_over_mesh_send().
const linkaddr_t linkaddr_null |
The null Rime address.
This variable contains the null Rime address. The null address is used in route tables to indicate that the table entry is unused. Nodes with no configured address has the null address. Nodes with their node address set to the null address will have problems communicating with other nodes.
Referenced by create(), frame802154_parse(), index_from_lladdr(), input_packet(), nbr_table_add_lladdr(), output(), packet_input(), packetbuf_attr_clear(), send_one_packet(), send_packet(), uip_ds6_link_neighbor_callback(), and uip_over_mesh_send().