Microchip® Advanced Software Framework

slip.h File Reference
#include "contiki.h"

Functions

 PROCESS_NAME (slip_process)
 
void slip_arch_init (unsigned long ubr)
 
void slip_arch_writeb (unsigned char c)
 
int slip_input_byte (unsigned char c)
 Input a SLIP byte. More...
 
uint8_t slip_send (void)
 Send an IP packet from the uIP buffer with SLIP. More...
 
void slip_set_input_callback (void(*callback)(void))
 Set a function to be called when there is activity on the SLIP interface; used for detecting if a node is a gateway node. More...
 
uint8_t slip_write (const void *ptr, int len)
 

Variables

uint8_t slip_active
 
uint16_t slip_ip_drop
 
uint16_t slip_overflow
 
uint16_t slip_rubbish
 
uint16_t slip_twopackets
 

PROCESS_NAME ( slip_process  )
void slip_arch_init ( unsigned long  ubr)
void slip_arch_writeb ( unsigned char  c)
int slip_input_byte ( unsigned char  c)

Input a SLIP byte.

This function is called by the RS232/SIO device driver to pass incoming bytes to the SLIP driver. The function can be called from an interrupt context.

For systems using low-power CPU modes, the return value of the function can be used to determine if the CPU should be woken up or not. If the function returns non-zero, the CPU should be powered up. If the function returns zero, the CPU can continue to be powered down.

Parameters
cThe data that is to be passed to the SLIP driver
Returns
Non-zero if the CPU should be powered up, zero otherwise.

References begin, c, end, pkt_end, process_poll(), RX_BUFSIZE, rxbuf, SLIP_END, SLIP_ESC, SLIP_ESC_END, SLIP_ESC_ESC, slip_overflow, slip_rubbish, SLIP_STATISTICS, slip_twopackets, state, STATE_ESC, STATE_OK, STATE_RUBBISH, and STATE_TWOPACKETS.

uint8_t slip_send ( void  )

Send an IP packet from the uIP buffer with SLIP.

References c, i, slip_arch_writeb(), SLIP_END, SLIP_ESC, SLIP_ESC_END, SLIP_ESC_ESC, uip_appdata, uip_buf, UIP_FW_OK, uip_len, UIP_LLH_LEN, and UIP_TCPIP_HLEN.

Referenced by input_callback(), and output().

void slip_set_input_callback ( void(*)(void)  callback)

Set a function to be called when there is activity on the SLIP interface; used for detecting if a node is a gateway node.

References c, and input_callback.

Referenced by init().

uint8_t slip_write ( const void *  ptr,
int  len 
)

uint8_t slip_active

Referenced by PROCESS_THREAD().

uint16_t slip_ip_drop

Referenced by PROCESS_THREAD().

uint16_t slip_overflow

Referenced by slip_input_byte().

uint16_t slip_rubbish

Referenced by slip_input_byte().

uint16_t slip_twopackets

Referenced by slip_input_byte().