Microchip® Advanced Software Framework

uip_conn Struct Reference

Representation of a uIP TCP connection.

The uip_conn structure is used for identifying a connection. All but one field in the structure are to be considered read-only by an application. The only exception is the appstate field whose purpose is to let the application store application-specific state (e.g., file pointers) for the connection. The type of this field is configured in the "uipopt.h" header file.

#include <uip.h>

Data Fields

uip_tcp_appstate_t appstate
 The application state. More...
 
uint16_t initialmss
 
             Initial maximum segment size for the

connection. More...

 
uint16_t len
 Length of the data that was previously sent. More...
 
uint16_t lport
 The local TCP port, in network byte order. More...
 
uint16_t mss
 
             Current maximum segment size for the

connection. More...

 
uint8_t nrtx
 
             The number of retransmissions for the last

segment sent. More...

 
uint8_t rcv_nxt [4]
 
          The sequence number that we expect to

receive next. More...

 
uip_ipaddr_t ripaddr
 The IP address of the remote host. More...
 
uint16_t rport
 
             The local remote TCP port, in network byte

order. More...

 
uint8_t rto
 Retransmission time-out. More...
 
uint8_t sa
 
             Retransmission time-out calculation state

variable. More...

 
uint8_t snd_nxt [4]
 The sequence number that was last sent by us. More...
 
uint8_t sv
 
             Retransmission time-out calculation state

variable. More...

 
uint8_t tcpstateflags
 TCP state and flags. More...
 
uint8_t timer
 The retransmission timer. More...
 

uip_tcp_appstate_t uip_conn::appstate

The application state.

Referenced by eventhandler(), tcp_attach(), tcp_connect(), and tcpip_uipcall().

uint16_t uip_conn::initialmss

             Initial maximum segment size for the

connection.

Referenced by uip_connect(), and uip_process().

uint16_t uip_conn::len

Length of the data that was previously sent.

Referenced by uip_connect(), and uip_process().

uint16_t uip_conn::lport

The local TCP port, in network byte order.

Referenced by appcall(), make_tcp_stats(), tcpip_uipcall(), uip_connect(), and uip_process().

uint16_t uip_conn::mss

             Current maximum segment size for the

connection.

Referenced by uip_connect(), and uip_process().

uint8_t uip_conn::nrtx

             The number of retransmissions for the last

segment sent.

Referenced by make_tcp_stats(), uip_connect(), and uip_process().

uint8_t uip_conn::rcv_nxt[4]

          The sequence number that we expect to

receive next.

Referenced by uip_add_rcv_nxt(), uip_connect(), and uip_process().

uip_ipaddr_t uip_conn::ripaddr

The IP address of the remote host.

Referenced by make_tcp_stats(), uip_connect(), and uip_process().

uint16_t uip_conn::rport

             The local remote TCP port, in network byte

order.

Referenced by make_tcp_stats(), uip_connect(), and uip_process().

uint8_t uip_conn::rto

Retransmission time-out.

Referenced by uip_connect(), and uip_process().

uint8_t uip_conn::sa

             Retransmission time-out calculation state

variable.

Referenced by uip_connect(), and uip_process().

uint8_t uip_conn::snd_nxt[4]

The sequence number that was last sent by us.

Referenced by uip_connect(), and uip_process().

uint8_t uip_conn::sv

             Retransmission time-out calculation state

variable.

Referenced by uip_connect(), and uip_process().

uint8_t uip_conn::tcpstateflags

TCP state and flags.

Referenced by eventhandler(), for(), make_tcp_stats(), uip_connect(), uip_init(), and uip_process().

uint8_t uip_conn::timer

The retransmission timer.

Referenced by make_tcp_stats(), uip_connect(), and uip_process().