SAM Peripheral Analog-to-Digital Converter Driver.
Copyright (c) 2012-2018 Microchip Technology Inc. and its subsidiaries.
#include "adc.h"
Macros | |
#define | PIN_INVALID_ADC_AIN 0xFFFFUL |
Functions | |
static void | _adc_configure_ain_pin (uint32_t pin) |
static enum status_code | _adc_set_config (struct adc_module *const module_inst, struct adc_config *const config) |
void | adc_get_config_defaults (struct adc_config *const config) |
Initializes an ADC configuration structure to defaults. More... | |
enum status_code | adc_init (struct adc_module *const module_inst, Adc *hw, struct adc_config *config) |
Initializes the ADC. More... | |
void | adc_regular_ain_channel (uint32_t *pin_array, uint8_t size) |
Initializes the ADC channel sequence. More... | |
void | adc_set_window_mode (struct adc_module *const module_inst, const enum adc_window_mode window_mode, const int16_t window_lower_value, const int16_t window_upper_value) |
Sets the ADC window mode. More... | |
#define PIN_INVALID_ADC_AIN 0xFFFFUL |
Referenced by _adc_configure_ain_pin().
|
inlinestatic |
Configure MUX settings for the analog pins
This function will set the given ADC input pins to the analog function in the pinmux, giving the ADC access to the analog signal
[in] | pin | AINxx pin to configure |
References Assert, system_pinmux_config::input_pull, system_pinmux_config::mux_position, PIN_INVALID_ADC_AIN, system_pinmux_get_config_defaults(), SYSTEM_PINMUX_PIN_PULL_NONE, and system_pinmux_pin_set_config().
Referenced by _adc_set_config(), and adc_regular_ain_channel().
|
static |
Writes an ADC configuration to the hardware module
Writes out a given ADC module configuration to the hardware module.
[out] | module_inst | Pointer to the ADC software instance struct |
[in] | config | Pointer to configuration struct |
STATUS_OK | The configuration was successful |
STATUS_ERR_INVALID_ARG | Invalid argument(s) were provided |
References _adc_configure_ain_pin(), adc_config::accumulate_samples, ADC_ACCUMULATE_DISABLE, ADC_ACCUMULATE_SAMPLES_16, ADC_ACCUMULATE_SAMPLES_256, ADC_ACCUMULATE_SAMPLES_4, ADC_ACCUMULATE_SAMPLES_64, ADC_DIVIDE_RESULT_16, ADC_DIVIDE_RESULT_2, ADC_DIVIDE_RESULT_4, ADC_DIVIDE_RESULT_8, ADC_DIVIDE_RESULT_DISABLE, ADC_RESOLUTION_10BIT, ADC_RESOLUTION_12BIT, ADC_RESOLUTION_13BIT, ADC_RESOLUTION_14BIT, ADC_RESOLUTION_15BIT, ADC_RESOLUTION_16BIT, ADC_RESOLUTION_8BIT, ADC_RESOLUTION_CUSTOM, ADC_WINDOW_MODE_DISABLE, adc_config::clock_prescaler, adc_config::clock_source, adc_config::correction, adc_correction_config::correction_enable, adc_config::differential_mode, adc_config::divide_result, adc_config::event_action, adc_config::freerunning, adc_correction_config::gain_correction, adc_config::gain_factor, adc_pin_scan_config::inputs_to_scan, adc_config::left_adjust, adc_config::negative_input, adc_correction_config::offset_correction, adc_pin_scan_config::offset_start_scan, adc_config::pin_scan, adc_config::positive_input, adc_config::reference, adc_config::reference_compensation_enable, adc_config::resolution, adc_config::run_in_standby, adc_config::sample_length, system_gclk_chan_config::source_generator, STATUS_ERR_INVALID_ARG, STATUS_OK, system_gclk_chan_enable(), system_gclk_chan_get_config_defaults(), system_gclk_chan_set_config(), while(), adc_config::window, adc_window_config::window_lower_value, adc_window_config::window_mode, and adc_window_config::window_upper_value.
Referenced by adc_init().
void adc_regular_ain_channel | ( | uint32_t * | pin_array, |
uint8_t | size | ||
) |
Initializes the ADC channel sequence.
Like SAMD and SAMR21 the INPUTOFFSET register will be incremented one automatically after a conversion done, causing the next conversion to be done with the positive input equal to MUXPOS + INPUTOFFSET, it is scanning continuously one by one even ADC channels are not continuous.
Initializes the ADC channel sequence by the sequence of pin_array.
[in] | pin_array | The array of the Mux selection for the positive ADC input |
[in] | size | The size of pin_array |
References _adc_configure_ain_pin(), and i.