Microchip® Advanced Software Framework

cc.h File Reference

Default definitions of C compiler quirk work-arounds.

Author
Adam Dunkels adam@.nosp@m.dunk.nosp@m.els.c.nosp@m.om

This file is used for making use of extra functionality of some C compilers used for Contiki, and defining work-arounds for various quirks and problems with some other C compilers.

#include "contiki-conf.h"

Macros

#define CC_ASSIGN_AGGREGATE(dest, src)   *dest = *src
 Configure if the C compiler supports the assignment of struct value. More...
 
#define CC_CONCAT(s1, s2)   CC_CONCAT2(s1, s2)
 A C preprocessing macro for concatenating to strings. More...
 
#define CC_CONCAT2(s1, s2)   s1##s2
 
#define CC_CONST_FUNCTION   const
 Configure if the C compiler have problems with const function pointers. More...
 
#define CC_DOUBLE_HASH   0
 Configure if C compiler supports double hash marks in C macros. More...
 
#define CC_FASTCALL   CC_CONF_FASTCALL
 Configure if the C compiler supports fastcall function declarations. More...
 
#define CC_FUNCTION_POINTER_ARGS   1
 Configure if the C compiler supports the arguments for function pointers. More...
 
#define CC_INLINE   CC_CONF_INLINE
 
#define CC_REGISTER_ARG
 Configure if the C compiler supports the "register" keyword for function arguments. More...
 
#define CC_UNSIGNED_CHAR_BUGS   0
 Configure work-around for unsigned char bugs with sdcc. More...
 
#define NULL   0
 

#define CC_ASSIGN_AGGREGATE (   dest,
  src 
)    *dest = *src

Configure if the C compiler supports the assignment of struct value.

#define CC_CONCAT (   s1,
  s2 
)    CC_CONCAT2(s1, s2)

A C preprocessing macro for concatenating to strings.

We need use two macros (CC_CONCAT and CC_CONCAT2) in order to allow concatenation of two #defined macros.

#define CC_CONCAT2 (   s1,
  s2 
)    s1##s2
#define CC_CONST_FUNCTION   const

Configure if the C compiler have problems with const function pointers.

#define CC_DOUBLE_HASH   0

Configure if C compiler supports double hash marks in C macros.

#define CC_FASTCALL   CC_CONF_FASTCALL

Configure if the C compiler supports fastcall function declarations.

#define CC_FUNCTION_POINTER_ARGS   1

Configure if the C compiler supports the arguments for function pointers.

#define CC_INLINE   CC_CONF_INLINE
#define CC_REGISTER_ARG

Configure if the C compiler supports the "register" keyword for function arguments.

#define CC_UNSIGNED_CHAR_BUGS   0

Configure work-around for unsigned char bugs with sdcc.

#define NULL   0