Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Best-effort multihop forwarding

The multihop module implements a multihop forwarding mechanism.

Routes must have already been setup with the route_add() function. Setting up routes is done with another Rime module such as the route-discovery module.

The multihop sends a packet to an identified node in the network by using multi-hop forwarding at each node in the network. The application or protocol that uses the multihop primitive supplies a routing function for selecting the next-hop neighbor. If the multihop primitive is requested to send a packet for which no suitable next hop neighbor is found, the caller is immediately notified of this and may choose to initiate a route discovery process.

Channels

The multihop module uses 1 channel.

Data Structures

struct  multihop_callbacks
 
struct  multihop_conn
 

Files

file  multihop.h
 
    Multihop forwarding header file

 

Macros

#define MULTIHOP_ATTRIBUTES
 

Functions

void multihop_close (struct multihop_conn *c)
 
void multihop_open (struct multihop_conn *c, uint16_t channel, const struct multihop_callbacks *u)
 
void multihop_resend (struct multihop_conn *c, const linkaddr_t *nexthop)
 
int multihop_send (struct multihop_conn *c, const linkaddr_t *to)
 

#define MULTIHOP_ATTRIBUTES
Value:
#define PACKETBUF_ATTR_BIT
Definition: packetbuf.h:444
Definition: packetbuf.h:379
#define UNICAST_ATTRIBUTES
Definition: unicast.h:69
#define PACKETBUF_ADDRSIZE
Definition: packetbuf.h:446
Definition: packetbuf.h:370
Definition: packetbuf.h:380

void multihop_close ( struct multihop_conn c)
void multihop_open ( struct multihop_conn c,
uint16_t  channel,
const struct multihop_callbacks u 
)
void multihop_resend ( struct multihop_conn c,
const linkaddr_t nexthop 
)
int multihop_send ( struct multihop_conn c,
const linkaddr_t to 
)