Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Real-time task scheduling

The real-time module handles the scheduling and execution of real-time tasks (with predictable execution times).

Data Structures

struct  rtimer
 Representation of a real-time task. More...
 

Files

file  rtimer.c
 
    Implementation of the architecture-agnostic parts of the real-time timer module.

 
file  rtimer.h
 
    Header file for the real-time timer module.

 

Macros

#define _DEBUG_   0
 
#define PRINTF(...)
 
#define RTIMER_NOW()
 Get the current clock time. More...
 
#define RTIMER_SECOND   RTIMER_ARCH_SECOND
 
#define RTIMER_TIME(task)
 Get the time that a task last was executed. More...
 

Typedefs

typedef void(* rtimer_callback_t )(struct rtimer *t, void *ptr)
 

Enumerations

enum  {
  RTIMER_OK,
  RTIMER_ERR_FULL,
  RTIMER_ERR_TIME,
  RTIMER_ERR_ALREADY_SCHEDULED
}
 

Functions

void rtimer_arch_init (void)
 
void rtimer_arch_schedule (rtimer_clock_t t)
 
void rtimer_init (void)
 Initialize the real-time scheduler. More...
 
void rtimer_run_next (void)
 Execute the next real-time task and schedule the next task, if any. More...
 
int rtimer_set (struct rtimer *task, rtimer_clock_t time, rtimer_clock_t duration, rtimer_callback_t func, void *ptr)
 Post a real-time task. More...
 

Variables

static struct rtimernext_rtimer
 

#define _DEBUG_   0
#define PRINTF (   ...)

Referenced by rtimer_set().

#define RTIMER_NOW ( )

Get the current clock time.

Returns
The current time
        This function returns what the real-time module thinks
        is the current time. The current time is used to set
        the timeouts for real-time tasks.

Referenced by init(), phase_wait(), powercycle(), schedule_powercycle(), schedule_powercycle_fixed(), send_one_packet(), send_packet(), and turn_on().

#define RTIMER_SECOND   RTIMER_ARCH_SECOND
#define RTIMER_TIME (   task)

Get the time that a task last was executed.

Parameters
taskThe task
Returns
The time that a task last was executed
        This function returns the time that the task was last
        executed. This typically is used to get a periodic
        execution of a task without clock drift.

Referenced by schedule_powercycle().

typedef void(* rtimer_callback_t)(struct rtimer *t, void *ptr)

anonymous enum
Enumerator
RTIMER_OK 
RTIMER_ERR_FULL 
RTIMER_ERR_TIME 
RTIMER_ERR_ALREADY_SCHEDULED 

void rtimer_arch_schedule ( rtimer_clock_t  t)
void rtimer_init ( void  )

Initialize the real-time scheduler.

This function initializes the real-time scheduler and must be called at boot-up, before any other functions from the real-time scheduler is called.

References rtimer_arch_init().

Referenced by main().

void rtimer_run_next ( void  )

Execute the next real-time task and schedule the next task, if any.

This function is called by the architecture dependent code to execute and schedule the next real-time task.

References rtimer::func, next_rtimer, NULL, rtimer::ptr, rtimer_arch_schedule(), and rtimer::time.

Referenced by rtimer_adjust_ticks(), rtimer_arch_schedule(), and rtimer_irq_callback().

int rtimer_set ( struct rtimer task,
rtimer_clock_t  time,
rtimer_clock_t  duration,
rtimer_callback_t  func,
void *  ptr 
)

Post a real-time task.

Parameters
taskA pointer to the task variable previously declared with RTIMER_TASK().
timeThe time when the task is to be executed.
durationUnused argument.
funcA function to be called when the task is executed.
ptrAn opaque pointer that will be supplied as an argument to the callback function.
Returns
Non-zero (true) if the task could be scheduled, zero (false) if the task could not be scheduled.

This function schedules a real-time task at a specified time in the future.

References rtimer::func, NULL, PRINTF, rtimer::ptr, rtimer_arch_schedule(), RTIMER_OK, and rtimer::time.

Referenced by init(), schedule_powercycle(), schedule_powercycle_fixed(), and turn_on().

struct rtimer* next_rtimer
static

Referenced by rtimer_run_next().