SAM RTC Driver (Tamper)
Copyright (c) 2015-2018 Microchip Technology Inc. and its subsidiaries.
Data Structures | |
struct | rtc_tamper_config |
RTC Tamper configuration structure. More... | |
struct | rtc_tamper_input_config |
RTC tamper input configuration structure. More... | |
Functions | |
RTC Tamper Detection | |
static void | rtc_tamper_get_config_defaults (struct rtc_tamper_config *const config) |
Gets the RTC tamper default configurations. More... | |
enum status_code | rtc_tamper_set_config (struct rtc_module *const module, struct rtc_tamper_config *const tamper_cfg) |
static uint32_t | rtc_tamper_get_detect_flag (struct rtc_module *const module) |
Retrieves the RTC tamper detection status. More... | |
static void | rtc_tamper_clear_detect_flag (struct rtc_module *const module, const uint32_t detect_flags) |
Clears RTC tamper detection flag. More... | |
#define | RTC_TAMPER_DETECT_ID0 (1UL << 0) |
RTC tamper ID0 detection bitmask. More... | |
#define | RTC_TAMPER_DETECT_ID1 (1UL << 1) |
RTC tamper ID1 detection bitmask. More... | |
#define | RTC_TAMPER_DETECT_ID2 (1UL << 2) |
RTC tamper ID2 detection bitmask. More... | |
#define | RTC_TAMPER_DETECT_ID3 (1UL << 3) |
RTC tamper ID3 detection bitmask. More... | |
#define | RTC_TAMPER_DETECT_ID4 (1UL << 4) |
RTC tamper ID4 detection bitmask. More... | |
#define | RTC_TAMPER_DETECT_EVT (1UL << 5) |
RTC tamper input event detection bitmask. More... | |
enum | rtc_tamper_active_layer_freq_divider { RTC_TAMPER_ACTIVE_LAYER_FREQ_DIV_2 = RTC_MODE0_CTRLB_ACTF_DIV2, RTC_TAMPER_ACTIVE_LAYER_FREQ_DIV_4 = RTC_MODE0_CTRLB_ACTF_DIV4, RTC_TAMPER_ACTIVE_LAYER_FREQ_DIV_8 = RTC_MODE0_CTRLB_ACTF_DIV8, RTC_TAMPER_ACTIVE_LAYER_FREQ_DIV_16 = RTC_MODE0_CTRLB_ACTF_DIV16, RTC_TAMPER_ACTIVE_LAYER_FREQ_DIV_32 = RTC_MODE0_CTRLB_ACTF_DIV32, RTC_TAMPER_ACTIVE_LAYER_FREQ_DIV_64 = RTC_MODE0_CTRLB_ACTF_DIV64, RTC_TAMPER_ACTIVE_LAYER_FREQ_DIV_128 = RTC_MODE0_CTRLB_ACTF_DIV128, RTC_TAMPER_ACTIVE_LAYER_FREQ_DIV_256 = RTC_MODE0_CTRLB_ACTF_DIV256 } |
RTC tamper active layer frequency divider. More... | |
enum | rtc_tamper_debounce_freq_divider { RTC_TAMPER_DEBOUNCE_FREQ_DIV_2 = RTC_MODE0_CTRLB_DEBF_DIV2, RTC_TAMPER_DEBOUNCE_FREQ_DIV_4 = RTC_MODE0_CTRLB_DEBF_DIV4, RTC_TAMPER_DEBOUNCE_FREQ_DIV_8 = RTC_MODE0_CTRLB_DEBF_DIV8, RTC_TAMPER_DEBOUNCE_FREQ_DIV_16 = RTC_MODE0_CTRLB_DEBF_DIV16, RTC_TAMPER_DEBOUNCE_FREQ_DIV_32 = RTC_MODE0_CTRLB_DEBF_DIV32, RTC_TAMPER_DEBOUNCE_FREQ_DIV_64 = RTC_MODE0_CTRLB_DEBF_DIV64, RTC_TAMPER_DEBOUNCE_FREQ_DIV_128 = RTC_MODE0_CTRLB_DEBF_DIV128, RTC_TAMPER_DEBOUNCE_FREQ_DIV_256 = RTC_MODE0_CTRLB_DEBF_DIV256 } |
RTC tamper debounce frequency divider. More... | |
enum | rtc_tamper_input_action { RTC_TAMPER_INPUT_ACTION_OFF = RTC_TAMPCTRL_IN0ACT_OFF, RTC_TAMPER_INPUT_ACTION_WAKE = RTC_TAMPCTRL_IN0ACT_WAKE, RTC_TAMPER_INPUT_ACTION_CAPTURE = RTC_TAMPCTRL_IN0ACT_CAPTURE, RTC_TAMPER_INPUT_ACTION_ACTL = RTC_TAMPCTRL_IN0ACT_ACTL } |
RTC tamper input action. More... | |
enum | rtc_tamper_level_sel { RTC_TAMPER_LEVEL_FALLING = (0), RTC_TAMPER_LEVEL_RISING = (1) } |
RTC tamper input level select. More... | |
enum | rtc_tamper_debounce_seq { RTC_TAMPER_DEBOUNCE_SYNC, RTC_TAMPER_DEBOUNCE_ASYNC, RTC_TAMPER_DEBOUNCE_MAJORITY } |
RTC tamper debounce sequential. More... | |
#define RTC_TAMPER_DETECT_EVT (1UL << 5) |
RTC tamper input event detection bitmask.
Referenced by rtc_tamper_clear_detect_flag(), and rtc_tamper_get_detect_flag().
#define RTC_TAMPER_DETECT_ID0 (1UL << 0) |
RTC tamper ID0 detection bitmask.
The RTC provides several selectable polarity external inputs (INn) that can be used for tamper detection. When detect, tamper inputs support the four actions:
Separate debouncers are embedded for each external input. The detection time depends on whether the debouncer operates synchronously or asynchronously, and whether majority detection is enabled or not. For details, refer to the section "Tamper Detection" of datasheet.
Referenced by rtc_tamper_clear_detect_flag(), and rtc_tamper_get_detect_flag().
#define RTC_TAMPER_DETECT_ID1 (1UL << 1) |
RTC tamper ID1 detection bitmask.
Referenced by rtc_tamper_clear_detect_flag(), and rtc_tamper_get_detect_flag().
#define RTC_TAMPER_DETECT_ID2 (1UL << 2) |
RTC tamper ID2 detection bitmask.
Referenced by rtc_tamper_clear_detect_flag(), and rtc_tamper_get_detect_flag().
#define RTC_TAMPER_DETECT_ID3 (1UL << 3) |
RTC tamper ID3 detection bitmask.
Referenced by rtc_tamper_clear_detect_flag(), and rtc_tamper_get_detect_flag().
#define RTC_TAMPER_DETECT_ID4 (1UL << 4) |
RTC tamper ID4 detection bitmask.
Referenced by rtc_tamper_clear_detect_flag(), and rtc_tamper_get_detect_flag().
RTC tamper active layer frequency divider.
The available prescaler factor for the RTC clock output used during active layer protection.
RTC tamper debounce frequency divider.
The available prescaler factor for the input debouncers.
RTC tamper debounce sequential.
The available sequential for tamper debounce.
RTC tamper input action.
The available action taken by the tamper input.
enum rtc_tamper_level_sel |
|
inlinestatic |
Clears RTC tamper detection flag.
Clears the given detection flag of the module.
[in] | module | Pointer to the TC software instance struct |
[in] | detect_flags | Bitmask of detection flags |
References Assert, RTC_TAMPER_DETECT_EVT, RTC_TAMPER_DETECT_ID0, RTC_TAMPER_DETECT_ID1, RTC_TAMPER_DETECT_ID2, RTC_TAMPER_DETECT_ID3, and RTC_TAMPER_DETECT_ID4.
|
inlinestatic |
Gets the RTC tamper default configurations.
Initializes the configuration structure to default values.
The default configuration is as follows:
[out] | config | Configuration structure to be initialized to default values. |
References rtc_tamper_input_config::action, rtc_tamper_config::actl_freq_div, Assert, rtc_tamper_config::bkup_reset_on_tamper, rtc_tamper_config::deb_freq_div, rtc_tamper_config::deb_seq, rtc_tamper_input_config::debounce_enable, rtc_tamper_config::dma_tamper_enable, rtc_tamper_config::gp0_enable, rtc_tamper_config::gp_reset_on_tamper, id, rtc_tamper_config::in_cfg, rtc_tamper_input_config::level, RTC_TAMPER_ACTIVE_LAYER_FREQ_DIV_8, RTC_TAMPER_DEBOUNCE_FREQ_DIV_8, RTC_TAMPER_DEBOUNCE_SYNC, RTC_TAMPER_INPUT_ACTION_OFF, and RTC_TAMPER_LEVEL_FALLING.
|
inlinestatic |
Retrieves the RTC tamper detection status.
Retrieves the detection status of each input pin and the input event.
[in] | module | Pointer to the RTC software instance struct |
RTC_TAMPER_DETECT_ID0 | Tamper condition on IN0 has been detected |
RTC_TAMPER_DETECT_ID1 | Tamper condition on IN1 has been detected |
RTC_TAMPER_DETECT_ID2 | Tamper condition on IN2 has been detected |
RTC_TAMPER_DETECT_ID3 | Tamper condition on IN3 has been detected |
RTC_TAMPER_DETECT_ID4 | Tamper condition on IN4 has been detected |
RTC_TAMPER_DETECT_EVT | Tamper input event has been detected |
References Assert, RTC_TAMPER_DETECT_EVT, RTC_TAMPER_DETECT_ID0, RTC_TAMPER_DETECT_ID1, RTC_TAMPER_DETECT_ID2, RTC_TAMPER_DETECT_ID3, and RTC_TAMPER_DETECT_ID4.
enum status_code rtc_tamper_set_config | ( | struct rtc_module *const | module, |
struct rtc_tamper_config *const | tamper_cfg | ||
) |