Microchip® Advanced Software Framework

serial-line.c File Reference
#include "dev/serial-line.h"
#include <string.h>
#include "lib/ringbuf.h"

Macros

#define BUFSIZE   128
 
#define END   0x0a
 
#define IGNORE_CHAR(c)   (c == 0x0d)
 

Functions

 PROCESS (serial_line_process,"Serial driver")
 
 PROCESS_THREAD (serial_line_process, ev, data)
 
void serial_line_init (void)
 
int serial_line_input_byte (unsigned char c)
 Get one byte of input from the serial driver. More...
 

Variables

static struct ringbuf rxbuf
 
static uint8_t rxbuf_data [BUFSIZE]
 
process_event_t serial_line_event_message
 Event posted when a line of input has been received. More...
 

#define BUFSIZE   128

Referenced by PROCESS_THREAD().

#define END   0x0a
#define IGNORE_CHAR (   c)    (c == 0x0d)

Referenced by serial_line_input_byte().

PROCESS ( serial_line_process  ,
"Serial driver"   
)
void serial_line_init ( void  )
int serial_line_input_byte ( unsigned char  c)

Get one byte of input from the serial driver.

This function is to be called from the actual RS232 driver to get one byte of serial data input.

For systems using low-power CPU modes, the return value of the function can be used to determine if the CPU should be woken up or not. If the function returns non-zero, the CPU should be powered up. If the function returns zero, the CPU can continue to be powered down.

Parameters
cThe data that is received.
Returns
Non-zero if the CPU should be powered up, zero otherwise.

References END, IGNORE_CHAR, process_poll(), ringbuf_put(), and rxbuf.

struct ringbuf rxbuf
static
uint8_t rxbuf_data[BUFSIZE]
static

Referenced by serial_line_init().

process_event_t serial_line_event_message

Event posted when a line of input has been received.

This event is posted when an entire line of input has been received from the serial port. A data pointer to the incoming line of input is sent together with the event.

Referenced by PROCESS_THREAD().