Trickle timer library implementation.
#include "contiki-conf.h"
#include "lib/trickle-timer.h"
#include "sys/ctimer.h"
#include "sys/cc.h"
#include "lib/random.h"
Macros | |
#define | _DEBUG_ 0 |
#define | PRINTF(...) |
#define | tt_rand() wide_rand() |
Wide randoms for platforms using a 4-byte wide clock (see TRICKLE_TIMER_WIDE_RAND) More... | |
Functions | |
static void | double_interval (void *ptr) |
static void | fire (void *ptr) |
static clock_time_t | get_t (clock_time_t i_cur) |
static uint8_t | max_imax (clock_time_t value) |
static void | new_interval (struct trickle_timer *tt) |
static void | schedule_for_end (struct trickle_timer *tt) |
static uint32_t | wide_rand (void) |
Trickle Timer Library: Functions called by protocol implementations | |
void | trickle_timer_consistency (struct trickle_timer *tt) |
To be called by the protocol when it hears a consistent transmission. More... | |
void | trickle_timer_inconsistency (struct trickle_timer *tt) |
To be called by the protocol when it hears an inconsistent transmission. More... | |
uint8_t | trickle_timer_config (struct trickle_timer *tt, clock_time_t i_min, uint8_t i_max, uint8_t k) |
Configure a trickle timer. More... | |
uint8_t | trickle_timer_set (struct trickle_timer *tt, trickle_timer_cb_t proto_cb, void *ptr) |
Start a previously configured trickle timer. More... | |
Variables | |
static clock_time_t | loc_clock |
static struct trickle_timer * | loctt |