Microchip® Advanced Software Framework

uip-ds6-nbr.c File Reference

    IPv6 Neighbor cache (link-layer/IPv6 address mapping)
Author
Mathilde Durvy mdurv.nosp@m.y@ci.nosp@m.sco.c.nosp@m.om
Julien Abeille jabei.nosp@m.lle@.nosp@m.cisco.nosp@m..com
Simon Duquennoy simon.nosp@m.duq@.nosp@m.sics..nosp@m.se
#include <string.h>
#include <stdlib.h>
#include <stddef.h>
#include "lib/list.h"
#include "net/linkaddr.h"
#include "net/packetbuf.h"
#include "net/ipv6/uip-ds6-nbr.h"
#include "net/ip/uip-debug.h"

Macros

#define _DEBUG_   DEBUG_NONE
 
#define LINK_NEIGHBOR_CALLBACK(addr, status, numtx)   UIP_CONF_DS6_LINK_NEIGHBOR_CALLBACK(addr, status, numtx)
 
#define NEIGHBOR_STATE_CHANGED(n)   UIP_CONF_DS6_NEIGHBOR_STATE_CHANGED(n)
 

Functions

void LINK_NEIGHBOR_CALLBACK (const linkaddr_t *addr, int status, int numtx)
 
 NBR_TABLE_GLOBAL (uip_ds6_nbr_t, ds6_neighbors)
 
void NEIGHBOR_STATE_CHANGED (uip_ds6_nbr_t *n)
 
uip_ds6_nbr_tuip_ds6_get_least_lifetime_neighbor (void)
 
This searches inside the neighbor table for the neighbor that is about to
expire the next.
More...
 
void uip_ds6_link_neighbor_callback (int status, int numtx)
 
uip_ds6_nbr_tuip_ds6_nbr_add (const uip_ipaddr_t *ipaddr, const uip_lladdr_t *lladdr, uint8_t isrouter, uint8_t state)
 Neighbor Cache basic routines. More...
 
const uip_ipaddr_tuip_ds6_nbr_get_ipaddr (const uip_ds6_nbr_t *nbr)
 
const uip_lladdr_tuip_ds6_nbr_get_ll (const uip_ds6_nbr_t *nbr)
 
uip_ipaddr_tuip_ds6_nbr_ipaddr_from_lladdr (const uip_lladdr_t *lladdr)
 
uip_ds6_nbr_tuip_ds6_nbr_ll_lookup (const uip_lladdr_t *lladdr)
 
const uip_lladdr_tuip_ds6_nbr_lladdr_from_ipaddr (const uip_ipaddr_t *ipaddr)
 
uip_ds6_nbr_tuip_ds6_nbr_lookup (const uip_ipaddr_t *ipaddr)
 
int uip_ds6_nbr_num (void)
 
void uip_ds6_nbr_rm (uip_ds6_nbr_t *nbr)
 
void uip_ds6_neighbor_periodic (void)
 
void uip_ds6_neighbors_init (void)