Microchip® Advanced Software Framework

•All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Multi-threading library

The event driven Contiki kernel does not provide multi-threading by itself - instead, preemptive multi-threading is implemented as a library that optionally can be linked with applications.

This library consists of two parts: a platform independent part, which is the same for all platforms on which Contiki runs, and a platform specific part, which must be implemented specifically for the platform that the multi-threading library should run.

Modules

 Architecture support for multi-threading
 The Contiki multi-threading library requires some architecture specific support for setting up and switching stacks.
 

Data Structures

struct  mt_thread
 

Macros

#define MT_OK
 No error. More...
 

Functions

void mt_exec (struct mt_thread *thread)
 Execute parts of a thread. More...
 
void mt_exit (void)
 Exit a thread. More...
 
void mt_init (void)
 Initializes the multithreading library. More...
 
void mt_remove (void)
 Uninstalls library and cleans up. More...
 
void mt_start (struct mt_thread *thread, void(*function)(void *), void *data)
 Starts a multithreading thread. More...
 
void mt_stop (struct mt_thread *thread)
 Stop a thread. More...
 
void mt_yield (void)
 Voluntarily give up the processor. More...
 

#define MT_OK

No error.

void mt_exec ( struct mt_thread thread)

Execute parts of a thread.

This function is called by a Contiki process and runs a thread. The function does not return until the thread has yielded, or is preempted.

Note
The thread library must first be initialized with the mt_init() function.
Parameters
threadA pointer to a struct mt_thread block that must be allocated by the caller.

References MT_STATE_READY, MT_STATE_RUNNING, mtarch_exec(), mt_thread::state, and mt_thread::thread.

void mt_exit ( void  )

Exit a thread.

This function is called from within an executing thread in order to exit the thread. The function never returns.

References MT_STATE_EXITED, mtarch_yield(), NULL, and mt_thread::state.

void mt_init ( void  )

Initializes the multithreading library.

References mtarch_init().

void mt_remove ( void  )

Uninstalls library and cleans up.

References mtarch_remove().

void mt_start ( struct mt_thread thread,
void(*)(void *)  function,
void *  data 
)

Starts a multithreading thread.

Parameters
threadPointer to an mt_thread struct that must have been previously allocated by the caller.
functionA pointer to the entry function of the thread that is to be set up.
dataA pointer that will be passed to the entry function.

References MT_STATE_READY, mtarch_start(), mt_thread::state, and mt_thread::thread.

void mt_stop ( struct mt_thread thread)

Stop a thread.

This function is called by a Contiki process in order to clean up a thread. The struct mt_thread block may then be discarded by the caller.

Parameters
threadA pointer to a struct mt_thread block that must be allocated by the caller.

References mtarch_stop(), and mt_thread::thread.

void mt_yield ( void  )

Voluntarily give up the processor.

This function is called by a running thread in order to give up control of the CPU.

References MT_STATE_READY, mtarch_pstop(), mtarch_yield(), NULL, and mt_thread::state.