Microchip® Advanced Software Framework

•All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Mesh routing

The mesh module sends packets using multi-hop routing to a specified receiver somewhere in the network.

Channels

The mesh module uses 3 channel; one for the multi-hop forwarding (multihop) and two for the route disovery (route-discovery).

Data Structures

struct  mesh_callbacks
 Mesh callbacks. More...
 
struct  mesh_conn
 

Files

file  mesh.h
 
    Header file for the Rime mesh routing protocol

 

Functions

void mesh_close (struct mesh_conn *c)
 Close an mesh connection. More...
 
void mesh_open (struct mesh_conn *c, uint16_t channels, const struct mesh_callbacks *callbacks)
 Open a mesh connection. More...
 
int mesh_ready (struct mesh_conn *c)
 Test if mesh is ready to send a packet (or packet is queued) More...
 
int mesh_send (struct mesh_conn *c, const linkaddr_t *dest)
 Send a mesh packet. More...
 

void mesh_close ( struct mesh_conn c)

Close an mesh connection.

Parameters
cA pointer to a struct mesh_conn
        This function closes an mesh connection that has
        previously been opened with mesh_open().

        This function typically is called as an exit handler.
void mesh_open ( struct mesh_conn c,
uint16_t  channels,
const struct mesh_callbacks callbacks 
)

Open a mesh connection.

Parameters
cA pointer to a struct mesh_conn
channelsThe channels on which the connection will operate; mesh uses 3 channels
callbacksPointer to callback structure
        This function sets up a mesh connection on the
        specified channel. The caller must have allocated the
        memory for the struct mesh_conn, usually by declaring it
        as a static variable.

        The struct mesh_callbacks pointer must point to a structure
        containing function pointers to functions that will be called
        when a packet arrives on the channel.
int mesh_ready ( struct mesh_conn c)

Test if mesh is ready to send a packet (or packet is queued)

Parameters
cThe mesh connection on which is to be tested
Return values
0Packet queued
!0Ready
int mesh_send ( struct mesh_conn c,
const linkaddr_t dest 
)

Send a mesh packet.

Parameters
cThe mesh connection on which the packet should be sent
destThe address of the final destination of the packet
Return values
Non-zeroif the packet could be queued for sending, zero otherwise
        This function sends a mesh packet. The packet must be
        present in the packetbuf before this function is called.

        The parameter c must point to an abc connection that
        must have previously been set up with mesh_open().