Microchip® Advanced Software Framework

•All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Frame802154

Data Structures

struct  field_length_t
 Structure that contains the lengths of the various addressing and security fields in the 802.15.4 header. More...
 
struct  frame802154_aux_hdr_t
 802.15.4 Aux security header More...
 
struct  frame802154_fcf_t
 The IEEE 802.15.4 frame has a number of constant/fixed fields that can be counted to make frame construction and max payload calculations easier. More...
 
struct  frame802154_scf_t
 802.15.4 security control bitfield. More...
 
struct  frame802154_t
 Parameters used by the frame802154_create() function. More...
 

Files

file  frame802154.c
 802.15.4 frame creation and parsing functions
 
file  frame802154.h
 802.15.4 frame creation and parsing functions
 

Macros

#define IEEE802154_PANID   IEEE802154_CONF_PANID
 

Functions

static CC_INLINE uint8_t addr_len (uint8_t mode)
 
static void field_len (frame802154_t *p, field_length_t *flen)
 

Variables

uint8_t frame802154_fcf_t::ack_required
 1 bit. More...
 
frame802154_aux_hdr_t frame802154_t::aux_hdr
 Aux security header. More...
 
uint8_t frame802154_t::dest_addr [8]
 Destination address. More...
 
uint8_t frame802154_fcf_t::dest_addr_mode
 < 3 bit. More...
 
uint16_t frame802154_t::dest_pid
 Destination PAN ID. More...
 
frame802154_fcf_t frame802154_t::fcf
 Frame control field. More...
 
uint32_t frame802154_aux_hdr_t::frame_counter
 Frame counter, used for security. More...
 
uint8_t frame802154_fcf_t::frame_pending
 1 bit. More...
 
uint8_t frame802154_fcf_t::frame_type
 3 bit. More...
 
uint8_t frame802154_fcf_t::frame_version
 2 bit. More...
 
uint8_t frame802154_aux_hdr_t::key [9]
 The key itself, or an index to the key. More...
 
uint8_t frame802154_scf_t::key_id_mode
 2 bit. More...
 
uint8_t frame802154_fcf_t::panid_compression
 1 bit. More...
 
uint8_t * frame802154_t::payload
 Pointer to 802.15.4 frame payload. More...
 
int frame802154_t::payload_len
 Length of payload field. More...
 
uint8_t frame802154_scf_t::reserved
 3 bit. More...
 
frame802154_scf_t frame802154_aux_hdr_t::security_control
 Security control bitfield. More...
 
uint8_t frame802154_fcf_t::security_enabled
 1 bit. More...
 
uint8_t frame802154_scf_t::security_level
 3 bit. More...
 
uint8_t frame802154_t::seq
 Sequence number. More...
 
uint8_t frame802154_t::src_addr [8]
 Source address. More...
 
uint8_t frame802154_fcf_t::src_addr_mode
 2 bit. More...
 
uint16_t frame802154_t::src_pid
 Source PAN ID. More...
 

FCF element values definitions

These are some definitions of values used in the FCF.

See the 802.15.4 spec for details.

int frame802154_hdrlen (frame802154_t *p)
 Calculates the length of the frame header. More...
 
int frame802154_create (frame802154_t *p, uint8_t *buf, int buf_len)
 Creates a frame for transmission over the air. More...
 
int frame802154_parse (uint8_t *data, int len, frame802154_t *pf)
 Parses an input frame. More...
 
#define FRAME802154_BEACONFRAME   (0x00)
 
#define FRAME802154_DATAFRAME   (0x01)
 
#define FRAME802154_ACKFRAME   (0x02)
 
#define FRAME802154_CMDFRAME   (0x03)
 
#define FRAME802154_BEACONREQ   (0x07)
 
#define FRAME802154_IEEERESERVED   (0x00)
 
#define FRAME802154_NOADDR   (0x00)
 Only valid for ACK or Beacon frames. More...
 
#define FRAME802154_SHORTADDRMODE   (0x02)
 
#define FRAME802154_LONGADDRMODE   (0x03)
 
#define FRAME802154_NOBEACONS   (0x0F)
 
#define FRAME802154_BROADCASTADDR   (0xFFFF)
 
#define FRAME802154_BROADCASTPANDID   (0xFFFF)
 
#define FRAME802154_IEEE802154_2003   (0x00)
 
#define FRAME802154_IEEE802154_2006   (0x01)
 
#define FRAME802154_SECURITY_LEVEL_NONE   (0)
 
#define FRAME802154_SECURITY_LEVEL_128   (3)
 

#define FRAME802154_ACKFRAME   (0x02)

Referenced by packet_input().

#define FRAME802154_BEACONFRAME   (0x00)
#define FRAME802154_BEACONREQ   (0x07)
#define FRAME802154_BROADCASTADDR   (0xFFFF)
#define FRAME802154_BROADCASTPANDID   (0xFFFF)

Referenced by parse().

#define FRAME802154_CMDFRAME   (0x03)
#define FRAME802154_DATAFRAME   (0x01)

Referenced by create(), and packet_input().

#define FRAME802154_IEEE802154_2003   (0x00)

Referenced by create().

#define FRAME802154_IEEE802154_2006   (0x01)
#define FRAME802154_IEEERESERVED   (0x00)
#define FRAME802154_LONGADDRMODE   (0x03)

Referenced by addr_len(), create(), and frame802154_parse().

#define FRAME802154_NOADDR   (0x00)

Only valid for ACK or Beacon frames.

#define FRAME802154_NOBEACONS   (0x0F)
#define FRAME802154_SECURITY_LEVEL_128   (3)
#define FRAME802154_SECURITY_LEVEL_NONE   (0)
#define FRAME802154_SHORTADDRMODE   (0x02)
#define IEEE802154_PANID   IEEE802154_CONF_PANID

static CC_INLINE uint8_t addr_len ( uint8_t  mode)
static
int frame802154_create ( frame802154_t p,
uint8_t *  buf,
int  buf_len 
)

Creates a frame for transmission over the air.

This function is meant to be called by a higher level function, that interfaces to a MAC.

Parameters
pPointer to frame802154_t struct, which specifies the frame to send.
bufPointer to the buffer to use for the frame.
buf_lenThe length of the buffer to use for the frame.
Returns
The length of the frame header or 0 if there was insufficient space in the buffer for the frame headers.

References frame802154_fcf_t::ack_required, field_length_t::aux_sec_len, buf, c, frame802154_t::dest_addr, field_length_t::dest_addr_len, frame802154_fcf_t::dest_addr_mode, frame802154_t::dest_pid, field_length_t::dest_pid_len, frame802154_t::fcf, field_len(), frame802154_fcf_t::frame_pending, frame802154_fcf_t::frame_type, frame802154_fcf_t::frame_version, frame802154_fcf_t::panid_compression, frame802154_fcf_t::security_enabled, frame802154_t::seq, frame802154_t::src_addr, field_length_t::src_addr_len, frame802154_fcf_t::src_addr_mode, frame802154_t::src_pid, and field_length_t::src_pid_len.

Referenced by create().

int frame802154_hdrlen ( frame802154_t p)

Calculates the length of the frame header.

This function is meant to be called by a higher level function, that interfaces to a MAC.

Parameters
pPointer to frame802154_t_t struct, which specifies the frame to send.
Returns
The length of the frame header.

References field_length_t::aux_sec_len, field_length_t::dest_addr_len, field_length_t::dest_pid_len, field_len(), field_length_t::src_addr_len, and field_length_t::src_pid_len.

Referenced by create().

int frame802154_parse ( uint8_t *  data,
int  len,
frame802154_t pf 
)

uint8_t frame802154_fcf_t::ack_required

1 bit.

Is an ack frame required?

Referenced by create(), frame802154_create(), frame802154_parse(), and packet_input().

frame802154_aux_hdr_t frame802154_t::aux_hdr

Aux security header.

Referenced by field_len().

uint8_t frame802154_t::dest_addr[8]

Destination address.

Referenced by create(), frame802154_create(), frame802154_parse(), packet_input(), and parse().

uint8_t frame802154_fcf_t::dest_addr_mode

< 3 bit.

Unused bits 2 bit. Destination address mode, see 802.15.4

Referenced by create(), field_len(), frame802154_create(), frame802154_parse(), and parse().

uint16_t frame802154_t::dest_pid

Destination PAN ID.

Referenced by create(), field_len(), frame802154_create(), frame802154_parse(), and parse().

frame802154_fcf_t frame802154_t::fcf
uint32_t frame802154_aux_hdr_t::frame_counter

Frame counter, used for security.

uint8_t frame802154_fcf_t::frame_pending

1 bit.

True if sender has more data to send

Referenced by create(), frame802154_create(), frame802154_parse(), and parse().

uint8_t frame802154_fcf_t::frame_type

3 bit.

Frame type field, see 802.15.4

Referenced by create(), frame802154_create(), frame802154_parse(), packet_input(), and parse().

uint8_t frame802154_fcf_t::frame_version

2 bit.

802.15.4 frame version

Referenced by create(), frame802154_create(), and frame802154_parse().

uint8_t frame802154_aux_hdr_t::key[9]

The key itself, or an index to the key.

uint8_t frame802154_scf_t::key_id_mode

2 bit.

Key identifier mode

Referenced by field_len().

uint8_t frame802154_fcf_t::panid_compression

1 bit.

Is this a compressed header?

Referenced by create(), field_len(), frame802154_create(), and frame802154_parse().

uint8_t* frame802154_t::payload

Pointer to 802.15.4 frame payload.

Referenced by create(), and frame802154_parse().

int frame802154_t::payload_len

Length of payload field.

Referenced by create(), frame802154_parse(), and parse().

uint8_t frame802154_scf_t::reserved

3 bit.

Reserved bits

frame802154_scf_t frame802154_aux_hdr_t::security_control

Security control bitfield.

Referenced by field_len().

uint8_t frame802154_fcf_t::security_enabled

1 bit.

True if security is used in this frame

Referenced by create(), field_len(), frame802154_create(), and frame802154_parse().

uint8_t frame802154_scf_t::security_level

3 bit.

security level

uint8_t frame802154_t::seq

Sequence number.

Referenced by create(), frame802154_create(), frame802154_parse(), packet_input(), and parse().

uint8_t frame802154_t::src_addr[8]

Source address.

Referenced by create(), frame802154_create(), frame802154_parse(), and parse().

uint8_t frame802154_fcf_t::src_addr_mode

2 bit.

Source address mode, see 802.15.4

Referenced by create(), field_len(), frame802154_create(), and frame802154_parse().

uint16_t frame802154_t::src_pid

Source PAN ID.

Referenced by create(), field_len(), frame802154_create(), and frame802154_parse().