#include "conf_usb.h"
#include <avr32/io.h>
#include "preprocessor.h"
#include "usb_drv.h"
#include "usb_task.h"
#include "usb_host_enum.h"
#include "usb_host_task.h"
Macros | |
#define | DEVICE_DEFAULT_MAX_ERROR_COUNT 2 |
Functions | |
Status_t | host_get_data (uint8_t pipe, uint16_t *nb_data, void *ptr_buf) |
This function receives nb_data bytes pointed to by ptr_buf on the specified pipe. More... | |
bool | host_get_data_interrupt (uint8_t pipe, uint16_t nb_data, void *ptr_buf, Pipe_handler *handler) |
This function receives nb_data bytes pointed to by ptr_buf on the specified pipe. More... | |
Status_t | host_send_data (uint8_t pipe, uint16_t nb_data, const void *ptr_buf) |
This function sends nb_data bytes pointed to by ptr_buf on the specified pipe. More... | |
bool | host_send_data_interrupt (uint8_t pipe, uint16_t nb_data, const void *ptr_buf, Pipe_handler *handler) |
This function sends nb_data bytes pointed to by ptr_buf on the specified pipe. More... | |
bool | is_any_interrupt_pipe_active (void) |
void | reset_it_pipe_str (void) |
void | usb_host_task (void) |
Entry point of the USB host management. More... | |
void | usb_host_task_init (void) |
This function initializes the USB host controller. More... | |
void | usb_pipe_interrupt (uint8_t pipe) |
USB pipe interrupt subroutine. More... | |
Variables | |
uint8_t | data_stage [SIZEOF_DATA_STAGE] |
Public: uint8_t data_stage[SIZEOF_DATA_STAGE] Internal RAM buffer for USB data stage content This buffer is required to setup host enumeration process It contains the device descriptors received. More... | |
volatile uint8_t | device_state |
Public: uint8_t device_state Its value represents the current state of the device connected to the USB host controller Value can be: More... | |
volatile bool | g_sav_int_sof_enable |
volatile S_pipe_int | it_pipe_str [MAX_PEP_NB] |
static const char | log_device_connected [] = "Device connected\r\n" |
static const char | log_device_enumerated [] = "Device enumerated\r\n" |
static const char | log_unsupported_device [] = "Unsupported device\r\n" |
static const char | log_usb_resumed [] = "USB resumed\r\n" |
static const char | log_usb_suspended [] = "USB suspended\r\n" |
volatile bool | request_resume |
static uint16_t | sof_cnt |
As internal host Start-of-Frame counter. More... | |
volatile uint8_t | usb_host_device_status |
volatile S_usb_setup_data | usb_request |
For control requests management over control pipe. More... | |
#define DEVICE_DEFAULT_MAX_ERROR_COUNT 2 |
Referenced by usb_host_task().
volatile bool g_sav_int_sof_enable |
Referenced by host_get_data_interrupt(), host_send_data_interrupt(), usb_general_interrupt(), and usb_pipe_interrupt().
volatile S_pipe_int it_pipe_str[MAX_PEP_NB] |
|
static |
Referenced by usb_host_task().
|
static |
Referenced by usb_host_task().
|
static |
Referenced by usb_host_task().
|
static |
Referenced by usb_host_task().
|
static |
Referenced by usb_host_task().
|
static |
As internal host Start-of-Frame counter.
Referenced by usb_host_task(), and usb_host_task_init().