#include <string.h>
#include "compiler.h"
#include "conf_audio_interface.h"
#include "audio_interface.h"
Macros | |
#define | AI_CALL(fct_set, macro) AI_CALL_##fct_set(macro); |
#define | AI_CALL_AI_HID_CLASS(macro) |
#define | AI_CALL_AI_SD_MMC(macro) |
#define | AI_CALL_AI_USB_MS(macro) |
#define | AI_CMD_RETRY_RELOAD 3 |
#define | AI_GET_DEVICE_STATUS(fct_set) |
#define | AI_HID_CLASS 2 |
#define | AI_NONE 0 |
#define | AI_PRIORITY0(macro) |
#define | AI_PRIORITY1(macro) AI_PRIORITY0(macro) AI_CALL(AI_USB_MS, macro) |
#define | AI_PRIORITY2(macro) AI_PRIORITY1(macro) AI_CALL(AI_HID_CLASS, macro) |
#define | AI_PRIORITY3(macro) AI_PRIORITY2(macro) AI_CALL(AI_SD_MMC, macro) |
#define | AI_PRIORITY_CALL(macro) AI_PRIORITY3(macro) |
#define | AI_SD_MMC 3 |
#define | AI_SYNC_FUNC_MALLOC(ret_type, func_name, pp_arg, err_ret) |
#define | AI_SYNC_FUNC_RET_STRUCT(ret_type, func_name, arg_type, arg_val, err_ret) |
-----— SYNCHRONOUS routines -----— More... | |
#define | AI_SYNC_FUNC_RET_VALUE(ret_type, func_name, arg_type, arg_val, err_ret) |
#define | AI_SYNC_FUNC_RET_VOID(func_name, arg_type, arg_val) |
#define | AI_SYNC_TASK_CALL_BACK() |
#define | AI_TASK_SELECT_FCT_SET(cur_fct_set) |
#define | AI_USB_MS 1 |
Functions | |
void | ai_async_cmd_out_free_ArrayU8 (void) |
Free the allocated buffer which holds the extra-result. More... | |
char * | ai_async_cmd_out_PtrArrayU8 (void) |
Returns the pointer on extra result of the last asynchronous command executed. More... | |
uint16_t | ai_async_cmd_out_SizeArrayU8 (void) |
Returns the size of the extra result (no size limit) of the last asynchronous executed command. More... | |
uint8_t | ai_async_cmd_out_status (void) |
Returns the status of the last asynchronous command executed. More... | |
uint32_t | ai_async_cmd_out_u32 (void) |
Return the result (max 32bits) of the last asynchronous command executed. More... | |
uint64_t | ai_async_cmd_out_u64 (void) |
Return the result (max 64 bits) of the last asynchronous command executed. More... | |
bool | ai_async_cmd_put (cmd_ai_id_t cmd_id, uint32_t u32_in, uint16_t u16_arg_size, char *u8_arg_in, bool need_extra_buffer) |
This routine may be used to send directly a command values from a communication port to audio interface. More... | |
void | ai_async_cmd_task (void) |
-----— ASYNCHRONOUS routines -----— note: to use these routines, you must call specific routine to know the end of execution and take the result More... | |
bool | ai_async_context_pop (ai_async_context_t *ctx) |
Pop a context from the stack. More... | |
bool | ai_async_context_push (ai_async_context_t *ctx) |
Push a new context into the stack. More... | |
void | ai_async_update_cmd_status (ai_async_status_t *cmd_ai_status) |
Update the current command status. More... | |
void * | ai_audio_context_save (uint8_t *status, uint16_t *size) |
Give complete audio context (player state, play time, repeat, shuffle, file played, explorer mode ) More... | |
void * | ai_audio_nav_file_info_image (ai_image_size_t *size) |
Returns a pointer and image information of the embedded image of the selected track. More... | |
void | ai_command_abort (void) |
Aborts the current command. More... | |
ai_device_status_t | ai_get_device_status (void) |
Here is the list of the SYNCHRONOUS functions. More... | |
void | ai_init (void) |
Initialize the audio interface. More... | |
bool | ai_is_hid_class (void) |
Returns true if the application is using hid class; false otherwise. More... | |
bool | ai_is_none (void) |
Returns true if no devices are connected. More... | |
bool | ai_is_sd_mmc (void) |
Returns true if the application is using sd/mmc card support; false otherwise. More... | |
bool | ai_is_usb_ms (void) |
Returns true if the current device is a USB mass storage device; false otherwise. More... | |
void * | ai_nav_file_info_image (ai_image_size_t *size) |
Returns a pointer and image information of the embedded image of the selected track. More... | |
bool | ai_read_string (bool(*fcnt_read_string)(char *, uint8_t), char **string, uint16_t *size_string) |
uint16_t | ai_song_read_info (uint16_t(*fcnt_song_read_info)(char **), char **string) |
static bool | ai_specific_async_cmd_task (cmd_ai_id_t cmd_id, uint32_t u32_in, uint16_t *u16_arg_size, char **u8_arg_in, uint32_t *u32_out, uint64_t *u64_out) |
AI_SYNC_FUNC_MALLOC (uint16_t, get_serial_number, pp_sz_sn, 0) | |
AI_SYNC_FUNC_MALLOC (uint16_t, nav_dir_name, ppstring, 0) | |
AI_SYNC_FUNC_MALLOC (uint16_t, nav_file_name, ppstring, 0) | |
AI_SYNC_FUNC_MALLOC (uint16_t, nav_file_info_title, ppsz_title, 0) | |
AI_SYNC_FUNC_MALLOC (uint16_t, nav_file_info_artist, ppsz_artist, 0) | |
AI_SYNC_FUNC_MALLOC (uint16_t, nav_file_info_album, ppsz_album, 0) | |
AI_SYNC_FUNC_MALLOC (uint16_t, nav_file_info_genre, ppsz_genre, 0) | |
AI_SYNC_FUNC_MALLOC (uint16_t, audio_nav_getname, ppstring, 0) | |
AI_SYNC_FUNC_MALLOC (uint16_t, audio_nav_file_info_title, ppsz_title, 0) | |
AI_SYNC_FUNC_MALLOC (uint16_t, audio_nav_file_info_artist, ppsz_artist, 0) | |
AI_SYNC_FUNC_MALLOC (uint16_t, audio_nav_file_info_album, ppsz_album, 0) | |
AI_SYNC_FUNC_MALLOC (uint16_t, audio_nav_file_info_genre, ppsz_genre, 0) | |
AI_SYNC_FUNC_RET_STRUCT (St_ai_info_version, nav_file_info_version, void,, 0) | |
AI_SYNC_FUNC_RET_STRUCT (St_ai_info_version, audio_nav_file_info_version, void,, 0) | |
AI_SYNC_FUNC_RET_STRUCT (Ai_player_flag_t, audio_ctrl_status, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (uint16_t, get_product_id, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (uint16_t, get_vendor_id, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (uint8_t, nav_drive_nb, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (bool, nav_drive_set, uint8_t, u8_number, 0) | |
AI_SYNC_FUNC_RET_VALUE (uint8_t, nav_drive_get, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (bool, nav_drive_mount, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (uint64_t, nav_drive_total_space, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (uint64_t, nav_drive_free_space, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (bool, nav_dir_root, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (bool, nav_dir_cd, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (bool, nav_dir_gotoparent, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (bool, nav_file_isdir, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (bool, nav_file_next, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (bool, nav_file_previous, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (bool, nav_file_goto, uint32_t, u32_newpos, 0) | |
AI_SYNC_FUNC_RET_VALUE (uint16_t, nav_file_pos, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (uint16_t, nav_file_nb, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (uint16_t, nav_dir_nb, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (uint16_t, nav_playlist_nb, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (uint32_t, nav_file_info_type, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (uint16_t, nav_file_info_year, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (uint32_t, nav_file_info_track, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (uint32_t, nav_file_info_duration, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (bool, nav_getplayfile, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (bool, audio_nav_playfile, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (bool, audio_context_restore, void *, ctx, 0) | |
AI_SYNC_FUNC_RET_VALUE (bool, audio_nav_next, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (bool, audio_nav_previous, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (bool, audio_nav_eof_occur, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (uint16_t, audio_nav_nb, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (uint16_t, audio_nav_getpos, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (bool, audio_nav_setpos, uint16_t, u16_pos, 0) | |
AI_SYNC_FUNC_RET_VALUE (Ai_repeat_mode, audio_nav_repeat_get, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (Ai_shuffle_mode, audio_nav_shuffle_get, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (Ai_explorer_mode, audio_nav_expmode_get, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (uint32_t, audio_nav_file_info_type, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (uint16_t, audio_nav_file_info_year, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (uint32_t, audio_nav_file_info_track, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (uint32_t, audio_nav_file_info_duration, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (bool, audio_ctrl_stop, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (bool, audio_ctrl_resume, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (bool, audio_ctrl_pause, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (uint32_t, audio_ctrl_time, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (bool, audio_ctrl_ffw, uint32_t, u32_duration, 0) | |
AI_SYNC_FUNC_RET_VALUE (bool, audio_ctrl_frw, uint32_t, u32_duration, 0) | |
AI_SYNC_FUNC_RET_VALUE (bool, audio_ctrl_start_ffw, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (bool, audio_ctrl_start_frw, void,, 0) | |
AI_SYNC_FUNC_RET_VALUE (bool, audio_ctrl_stop_ffw_frw, void,, 0) | |
AI_SYNC_FUNC_RET_VOID (audio_nav_repeat_set, Ai_repeat_mode, repeat_mode) | |
AI_SYNC_FUNC_RET_VOID (audio_nav_shuffle_set, Ai_shuffle_mode, shuffle) | |
AI_SYNC_FUNC_RET_VOID (audio_nav_expmode_set, Ai_explorer_mode, exp_mode) | |
void | ai_task (void) |
Task for the internal behaviors of the Audio Interface. More... | |
bool | is_ai_async_cmd_finished (void) |
Tests if the current asynchronous routine is finished. More... | |
Variables | |
const ai_fct_set | ai_default_fct_set |
const ai_fct_set * | ai_fct_set_tab [4] |
uint8_t | current_ai_fct_set = AI_NONE |
static char * | g_ai_char_arg |
ai_async_status_t | g_ai_cmd_execution_status |
static cmd_ai_id_t | g_ai_cmdid |
static uint8_t | g_ai_status |
static uint16_t | g_ai_u16_arg_size |
static uint32_t | g_ai_u32_in |
static uint32_t | g_ai_u32_out |
static uint64_t | g_ai_u64_out |
volatile bool | g_b_ai_cmd_received |
uint8_t | g_retry_cnt |
Number of retries before aborting the command. More... | |
#define AI_CALL | ( | fct_set, | |
macro | |||
) | AI_CALL_##fct_set(macro); |
#define AI_CALL_AI_HID_CLASS | ( | macro | ) |
#define AI_CALL_AI_SD_MMC | ( | macro | ) |
#define AI_CALL_AI_USB_MS | ( | macro | ) |
#define AI_CMD_RETRY_RELOAD 3 |
Referenced by ai_async_cmd_put().
#define AI_GET_DEVICE_STATUS | ( | fct_set | ) |
Referenced by ai_get_device_status().
#define AI_HID_CLASS 2 |
Referenced by ai_init(), and ai_is_hid_class().
#define AI_NONE 0 |
Referenced by ai_init(), ai_is_none(), and ai_task().
#define AI_PRIORITY0 | ( | macro | ) |
#define AI_PRIORITY1 | ( | macro | ) | AI_PRIORITY0(macro) AI_CALL(AI_USB_MS, macro) |
#define AI_PRIORITY2 | ( | macro | ) | AI_PRIORITY1(macro) AI_CALL(AI_HID_CLASS, macro) |
#define AI_PRIORITY3 | ( | macro | ) | AI_PRIORITY2(macro) AI_CALL(AI_SD_MMC, macro) |
#define AI_PRIORITY_CALL | ( | macro | ) | AI_PRIORITY3(macro) |
Referenced by ai_get_device_status(), and ai_task().
#define AI_SD_MMC 3 |
Referenced by ai_init(), and ai_is_sd_mmc().
#define AI_SYNC_FUNC_MALLOC | ( | ret_type, | |
func_name, | |||
pp_arg, | |||
err_ret | |||
) |
#define AI_SYNC_FUNC_RET_STRUCT | ( | ret_type, | |
func_name, | |||
arg_type, | |||
arg_val, | |||
err_ret | |||
) |
-----— SYNCHRONOUS routines -----—
#define AI_SYNC_FUNC_RET_VALUE | ( | ret_type, | |
func_name, | |||
arg_type, | |||
arg_val, | |||
err_ret | |||
) |
#define AI_SYNC_FUNC_RET_VOID | ( | func_name, | |
arg_type, | |||
arg_val | |||
) |
#define AI_SYNC_TASK_CALL_BACK | ( | ) |
#define AI_TASK_SELECT_FCT_SET | ( | cur_fct_set | ) |
Referenced by ai_task().
#define AI_USB_MS 1 |
Referenced by ai_init(), and ai_is_usb_ms().
void ai_async_cmd_out_free_ArrayU8 | ( | void | ) |
Free the allocated buffer which holds the extra-result.
This shall be done when the "extra results" are no more needed by the application.
References g_ai_char_arg, g_ai_u16_arg_size, and NULL.
Referenced by ai_async_cmd_put().
char* ai_async_cmd_out_PtrArrayU8 | ( | void | ) |
Returns the pointer on extra result of the last asynchronous command executed.
References g_ai_char_arg.
Referenced by ai_audio_context_save(), navigation_task(), and track_changed_task().
uint16_t ai_async_cmd_out_SizeArrayU8 | ( | void | ) |
Returns the size of the extra result (no size limit) of the last asynchronous executed command.
References g_ai_u16_arg_size.
Referenced by ai_audio_context_save(), navigation_task(), and track_changed_task().
uint8_t ai_async_cmd_out_status | ( | void | ) |
Returns the status of the last asynchronous command executed.
References CMD_ERROR, g_ai_cmd_execution_status, and g_ai_status.
Referenced by ai_audio_context_save(), and com_task().
uint32_t ai_async_cmd_out_u32 | ( | void | ) |
Return the result (max 32bits) of the last asynchronous command executed.
References g_ai_u32_out.
Referenced by ai_audio_nav_file_info_image(), ai_nav_file_info_image(), check_device_task(), config_task(), navigation_task(), playback_task(), and track_changed_task().
uint64_t ai_async_cmd_out_u64 | ( | void | ) |
Return the result (max 64 bits) of the last asynchronous command executed.
References g_ai_u64_out.
bool ai_async_cmd_put | ( | cmd_ai_id_t | cmd_id, |
uint32_t | u32_in, | ||
uint16_t | u16_arg_size, | ||
char * | u8_arg_in, | ||
bool | need_extra_buffer | ||
) |
This routine may be used to send directly a command values from a communication port to audio interface.
This routine may be use to send directly a command values from a communication port to audio interface.
References ai_async_cmd_out_free_ArrayU8(), AI_CMD_RETRY_RELOAD, g_ai_char_arg, g_ai_cmdid, g_ai_u16_arg_size, g_ai_u32_in, g_b_ai_cmd_received, and g_retry_cnt.
Referenced by ai_async_audio_context_restore(), ai_async_audio_context_save(), ai_async_audio_ctrl_ffw(), ai_async_audio_ctrl_frw(), ai_async_audio_ctrl_pause(), ai_async_audio_ctrl_resume(), ai_async_audio_ctrl_start_ffw(), ai_async_audio_ctrl_start_frw(), ai_async_audio_ctrl_status(), ai_async_audio_ctrl_stop(), ai_async_audio_ctrl_stop_ffw_frw(), ai_async_audio_ctrl_time(), ai_async_audio_nav_eof_occur(), ai_async_audio_nav_expmode_get(), ai_async_audio_nav_expmode_set(), ai_async_audio_nav_file_info_album(), ai_async_audio_nav_file_info_artist(), ai_async_audio_nav_file_info_duration(), ai_async_audio_nav_file_info_genre(), ai_async_audio_nav_file_info_image(), ai_async_audio_nav_file_info_title(), ai_async_audio_nav_file_info_track(), ai_async_audio_nav_file_info_type(), ai_async_audio_nav_file_info_version(), ai_async_audio_nav_file_info_year(), ai_async_audio_nav_getname(), ai_async_audio_nav_getpos(), ai_async_audio_nav_nb(), ai_async_audio_nav_next(), ai_async_audio_nav_playfile(), ai_async_audio_nav_previous(), ai_async_audio_nav_repeat_get(), ai_async_audio_nav_repeat_set(), ai_async_audio_nav_setpos(), ai_async_audio_nav_shuffle_get(), ai_async_audio_nav_shuffle_set(), ai_async_get_product_id(), ai_async_get_serial_number(), ai_async_get_vendor_id(), ai_async_is_device_connected(), ai_async_nav_dir_cd(), ai_async_nav_dir_gotoparent(), ai_async_nav_dir_name(), ai_async_nav_dir_nb(), ai_async_nav_dir_root(), ai_async_nav_drive_free_space(), ai_async_nav_drive_get(), ai_async_nav_drive_mount(), ai_async_nav_drive_nb(), ai_async_nav_drive_set(), ai_async_nav_drive_total_space(), ai_async_nav_file_goto(), ai_async_nav_file_info_album(), ai_async_nav_file_info_artist(), ai_async_nav_file_info_duration(), ai_async_nav_file_info_genre(), ai_async_nav_file_info_image(), ai_async_nav_file_info_title(), ai_async_nav_file_info_track(), ai_async_nav_file_info_type(), ai_async_nav_file_info_version(), ai_async_nav_file_info_year(), ai_async_nav_file_isdir(), ai_async_nav_file_name(), ai_async_nav_file_nb(), ai_async_nav_file_next(), ai_async_nav_file_pos(), ai_async_nav_file_previous(), ai_async_nav_getplayfile(), ai_async_nav_playlist_nb(), ai_async_usb_ms_specific_audio_nav_get_folder_name(), ai_async_usb_ms_specific_audio_nav_playlist_play_link(), ai_async_usb_ms_specific_audio_nav_restore(), ai_async_usb_ms_specific_audio_nav_save(), ai_async_usb_ms_specific_nav_get_next_playlist_pos(), ai_async_usb_ms_specific_nav_getplaylistfile(), ai_async_usb_ms_specific_nav_playlist_link_name(), ai_async_usb_ms_specific_nav_playlist_link_nb(), ai_async_usb_ms_specific_nav_restore(), ai_async_usb_ms_specific_nav_save(), ai_async_usb_ms_specific_playlist_nav_restore(), and ai_async_usb_ms_specific_playlist_nav_save().
void ai_async_cmd_task | ( | void | ) |
-----— ASYNCHRONOUS routines -----— note: to use these routines, you must call specific routine to know the end of execution and take the result
Launch the execution (it can be a part of the job or its full execution) of the current asynchronous command.
References AI_ASYNC_STACK_NB_ELEMENTS, ai_specific_async_cmd_task(), ai_fct_set::audio_context_restore, ai_fct_set::audio_ctrl_ffw, ai_fct_set::audio_ctrl_frw, ai_fct_set::audio_ctrl_pause, ai_fct_set::audio_ctrl_resume, ai_fct_set::audio_ctrl_start_ffw, ai_fct_set::audio_ctrl_start_frw, ai_fct_set::audio_ctrl_stop, ai_fct_set::audio_ctrl_stop_ffw_frw, ai_fct_set::audio_ctrl_time, ai_fct_set::audio_nav_eof_occur, ai_fct_set::audio_nav_expmode_get, ai_fct_set::audio_nav_expmode_set, ai_fct_set::audio_nav_file_info_album, ai_fct_set::audio_nav_file_info_artist, ai_fct_set::audio_nav_file_info_duration, ai_fct_set::audio_nav_file_info_genre, ai_fct_set::audio_nav_file_info_title, ai_fct_set::audio_nav_file_info_track, ai_fct_set::audio_nav_file_info_type, ai_fct_set::audio_nav_file_info_version, ai_fct_set::audio_nav_file_info_year, ai_fct_set::audio_nav_getname, ai_fct_set::audio_nav_getpos, ai_fct_set::audio_nav_nb, ai_fct_set::audio_nav_next, ai_fct_set::audio_nav_playfile, ai_fct_set::audio_nav_previous, ai_fct_set::audio_nav_repeat_get, ai_fct_set::audio_nav_repeat_set, ai_fct_set::audio_nav_setpos, ai_fct_set::audio_nav_shuffle_get, ai_fct_set::audio_nav_shuffle_set, CMD_AI_AUDIO_CONTEXT_RESTORE, CMD_AI_AUDIO_CONTEXT_SAVE, CMD_AI_AUDIO_CTRL_FFW, CMD_AI_AUDIO_CTRL_FRW, CMD_AI_AUDIO_CTRL_PAUSE, CMD_AI_AUDIO_CTRL_RESUME, CMD_AI_AUDIO_CTRL_START_FFW, CMD_AI_AUDIO_CTRL_START_FRW, CMD_AI_AUDIO_CTRL_STATUS, CMD_AI_AUDIO_CTRL_STOP, CMD_AI_AUDIO_CTRL_STOP_FFW_FRW, CMD_AI_AUDIO_CTRL_TIME, CMD_AI_AUDIO_NAV_EOF_OCCUR, CMD_AI_AUDIO_NAV_EXPMODE_GET, CMD_AI_AUDIO_NAV_EXPMODE_SET, CMD_AI_AUDIO_NAV_GETNAME, CMD_AI_AUDIO_NAV_GETPOS, CMD_AI_AUDIO_NAV_INFO_ALBUM, CMD_AI_AUDIO_NAV_INFO_ARTIST, CMD_AI_AUDIO_NAV_INFO_DURATION, CMD_AI_AUDIO_NAV_INFO_GENRE, CMD_AI_AUDIO_NAV_INFO_IMAGE, CMD_AI_AUDIO_NAV_INFO_TITLE, CMD_AI_AUDIO_NAV_INFO_TRACK, CMD_AI_AUDIO_NAV_INFO_TYPE, CMD_AI_AUDIO_NAV_INFO_VERSION, CMD_AI_AUDIO_NAV_INFO_YEAR, CMD_AI_AUDIO_NAV_NB, CMD_AI_AUDIO_NAV_NEXT, CMD_AI_AUDIO_NAV_PLAYFILE, CMD_AI_AUDIO_NAV_PREV, CMD_AI_AUDIO_NAV_REPEAT_GET, CMD_AI_AUDIO_NAV_REPEAT_SET, CMD_AI_AUDIO_NAV_SETPOS, CMD_AI_AUDIO_NAV_SHUFFLE_GET, CMD_AI_AUDIO_NAV_SHUFFLE_SET, CMD_AI_GET_DEVICE_STATUS, CMD_AI_GET_PRODUCT_ID, CMD_AI_GET_SERIAL_NUMBER, CMD_AI_GET_VENDOR_ID, CMD_AI_NAV_DIR_CD, CMD_AI_NAV_DIR_GOTOPARENT, CMD_AI_NAV_DIR_NAME, CMD_AI_NAV_DIR_NB, CMD_AI_NAV_DIR_ROOT, CMD_AI_NAV_DRIVE_FREE_SPACE, CMD_AI_NAV_DRIVE_GET, CMD_AI_NAV_DRIVE_MOUNT, CMD_AI_NAV_DRIVE_NB, CMD_AI_NAV_DRIVE_SET, CMD_AI_NAV_DRIVE_TOTAL_SPACE, CMD_AI_NAV_FILE_GOTO, CMD_AI_NAV_FILE_ISDIR, CMD_AI_NAV_FILE_NAME, CMD_AI_NAV_FILE_NB, CMD_AI_NAV_FILE_NEXT, CMD_AI_NAV_FILE_POS, CMD_AI_NAV_FILE_PREVIOUS, CMD_AI_NAV_GETPLAYFILE, CMD_AI_NAV_INFO_ALBUM, CMD_AI_NAV_INFO_ARTIST, CMD_AI_NAV_INFO_DURATION, CMD_AI_NAV_INFO_GENRE, CMD_AI_NAV_INFO_IMAGE, CMD_AI_NAV_INFO_TITLE, CMD_AI_NAV_INFO_TRACK, CMD_AI_NAV_INFO_TYPE, CMD_AI_NAV_INFO_VERSION, CMD_AI_NAV_INFO_YEAR, CMD_AI_NAV_PLAYLIST_NB, CMD_ERROR, CMD_EXECUTING, current_ai_fct_set, St_ai_info_version::digit, g_ai_char_arg, g_ai_cmd_execution_status, g_ai_cmdid, g_ai_status, g_ai_u16_arg_size, g_ai_u32_in, g_ai_u32_out, g_ai_u64_out, g_b_ai_cmd_received, ai_fct_set::get_product_id, ai_fct_set::get_serial_number, ai_fct_set::get_vendor_id, St_ai_info_version::major, St_ai_info_version::minor, ai_fct_set::nav_dir_cd, ai_fct_set::nav_dir_gotoparent, ai_fct_set::nav_dir_name, ai_fct_set::nav_dir_nb, ai_fct_set::nav_dir_root, ai_fct_set::nav_drive_free_space, ai_fct_set::nav_drive_get, ai_fct_set::nav_drive_mount, ai_fct_set::nav_drive_nb, ai_fct_set::nav_drive_set, ai_fct_set::nav_drive_total_space, ai_fct_set::nav_file_goto, ai_fct_set::nav_file_info_album, ai_fct_set::nav_file_info_artist, ai_fct_set::nav_file_info_duration, ai_fct_set::nav_file_info_genre, ai_fct_set::nav_file_info_title, ai_fct_set::nav_file_info_track, ai_fct_set::nav_file_info_type, ai_fct_set::nav_file_info_version, ai_fct_set::nav_file_info_year, ai_fct_set::nav_file_isdir, ai_fct_set::nav_file_name, ai_fct_set::nav_file_nb, ai_fct_set::nav_file_next, ai_fct_set::nav_file_pos, ai_fct_set::nav_file_previous, ai_fct_set::nav_getplayfile, ai_fct_set::nav_playlist_nb, NULL, and St_ai_info_version::revision.
Referenced by ai_audio_context_save(), ai_audio_nav_file_info_image(), ai_nav_file_info_image(), codec_mp3_task(), codec_wav_task(), and com_task().
bool ai_async_context_pop | ( | ai_async_context_t * | ctx | ) |
Pop a context from the stack.
ctx | A pointer on an empty context structure to store the new context. |
References AI_ASYNC_STACK_NB_ELEMENTS.
Referenced by ai_usb_ms_audio_nav_mov().
bool ai_async_context_push | ( | ai_async_context_t * | ctx | ) |
Push a new context into the stack.
ctx | The new context to push. |
Referenced by ai_usb_ms_audio_nav_mov().
void ai_async_update_cmd_status | ( | ai_async_status_t * | cmd_ai_status | ) |
Update the current command status.
cmd_ai_status | The current command status to update |
References AI_ASYNC_STACK_NB_ELEMENTS, CMD_DONE, CMD_ERROR, ctx, and ai_async_context_t::status.
Referenced by ai_usb_ms_audio_nav_mov().
void* ai_audio_context_save | ( | uint8_t * | status, |
uint16_t * | size | ||
) |
Give complete audio context (player state, play time, repeat, shuffle, file played, explorer mode )
References ai_async_audio_context_save(), ai_async_cmd_out_PtrArrayU8(), ai_async_cmd_out_SizeArrayU8(), ai_async_cmd_out_status(), ai_async_cmd_task(), AI_SYNC_TASK_CALL_BACK, is_ai_async_cmd_finished(), and NULL.
void* ai_audio_nav_file_info_image | ( | ai_image_size_t * | size | ) |
Returns a pointer and image information of the embedded image of the selected track.
size | The desire width and height of the decoded image. |
size | The actual width and height of the decoded image. |
References ai_async_audio_nav_file_info_image(), ai_async_cmd_out_u32(), ai_async_cmd_task(), AI_SYNC_TASK_CALL_BACK, is_ai_async_cmd_finished(), and NULL.
void ai_command_abort | ( | void | ) |
Aborts the current command.
References CMD_ERROR, g_ai_cmd_execution_status, g_ai_status, and g_b_ai_cmd_received.
Referenced by com_task().
ai_device_status_t ai_get_device_status | ( | void | ) |
Here is the list of the SYNCHRONOUS functions.
Tells the status of the device connected.
Tells if a device is connected or not
References AI_DEVICE_STATUS_NOT_PRESENT, AI_GET_DEVICE_STATUS, and AI_PRIORITY_CALL.
Referenced by usb_device_get_state().
void ai_init | ( | void | ) |
Initialize the audio interface.
Initialize the Audio Interface.
References AI_ASYNC_STACK_NB_ELEMENTS, ai_default_fct_set, AI_HID_CLASS, ai_hid_class_fct_set, AI_NONE, AI_SD_MMC, ai_sd_mmc_fct_set, AI_USB_MS, ai_usb_ms_fct_set, g_ai_status, g_b_ai_cmd_received, and ai_fct_set::init.
Referenced by main().
bool ai_is_hid_class | ( | void | ) |
Returns true if the application is using hid class; false otherwise.
References AI_HID_CLASS.
bool ai_is_none | ( | void | ) |
bool ai_is_sd_mmc | ( | void | ) |
Returns true if the application is using sd/mmc card support; false otherwise.
References AI_SD_MMC.
bool ai_is_usb_ms | ( | void | ) |
Returns true if the current device is a USB mass storage device; false otherwise.
References AI_USB_MS.
void* ai_nav_file_info_image | ( | ai_image_size_t * | size | ) |
Returns a pointer and image information of the embedded image of the selected track.
size | The desire width and height of the decoded image. |
size | The actual width and height of the decoded image. |
References ai_async_cmd_out_u32(), ai_async_cmd_task(), ai_async_nav_file_info_image(), AI_SYNC_TASK_CALL_BACK, is_ai_async_cmd_finished(), and NULL.
bool ai_read_string | ( | bool(*)(char *, uint8_t) | fcnt_read_string, |
char ** | string, | ||
uint16_t * | size_string | ||
) |
uint16_t ai_song_read_info | ( | uint16_t(*)(char **) | fcnt_song_read_info, |
char ** | string | ||
) |
|
static |
References current_ai_fct_set, g_ai_cmd_execution_status, and ai_fct_set::specific_async_cmd_task.
Referenced by ai_async_cmd_task().
AI_SYNC_FUNC_MALLOC | ( | uint16_t | , |
get_serial_number | , | ||
pp_sz_sn | , | ||
0 | |||
) |
AI_SYNC_FUNC_MALLOC | ( | uint16_t | , |
nav_dir_name | , | ||
ppstring | , | ||
0 | |||
) |
AI_SYNC_FUNC_MALLOC | ( | uint16_t | , |
nav_file_name | , | ||
ppstring | , | ||
0 | |||
) |
AI_SYNC_FUNC_MALLOC | ( | uint16_t | , |
nav_file_info_title | , | ||
ppsz_title | , | ||
0 | |||
) |
AI_SYNC_FUNC_MALLOC | ( | uint16_t | , |
nav_file_info_artist | , | ||
ppsz_artist | , | ||
0 | |||
) |
AI_SYNC_FUNC_MALLOC | ( | uint16_t | , |
nav_file_info_album | , | ||
ppsz_album | , | ||
0 | |||
) |
AI_SYNC_FUNC_MALLOC | ( | uint16_t | , |
nav_file_info_genre | , | ||
ppsz_genre | , | ||
0 | |||
) |
AI_SYNC_FUNC_MALLOC | ( | uint16_t | , |
audio_nav_getname | , | ||
ppstring | , | ||
0 | |||
) |
AI_SYNC_FUNC_MALLOC | ( | uint16_t | , |
audio_nav_file_info_title | , | ||
ppsz_title | , | ||
0 | |||
) |
AI_SYNC_FUNC_MALLOC | ( | uint16_t | , |
audio_nav_file_info_artist | , | ||
ppsz_artist | , | ||
0 | |||
) |
AI_SYNC_FUNC_MALLOC | ( | uint16_t | , |
audio_nav_file_info_album | , | ||
ppsz_album | , | ||
0 | |||
) |
AI_SYNC_FUNC_MALLOC | ( | uint16_t | , |
audio_nav_file_info_genre | , | ||
ppsz_genre | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_STRUCT | ( | St_ai_info_version | , |
nav_file_info_version | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_STRUCT | ( | St_ai_info_version | , |
audio_nav_file_info_version | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_STRUCT | ( | Ai_player_flag_t | , |
audio_ctrl_status | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | uint16_t | , |
get_product_id | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | uint16_t | , |
get_vendor_id | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | uint8_t | , |
nav_drive_nb | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | bool | , |
nav_drive_set | , | ||
uint8_t | , | ||
u8_number | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | uint8_t | , |
nav_drive_get | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | bool | , |
nav_drive_mount | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | uint64_t | , |
nav_drive_total_space | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | uint64_t | , |
nav_drive_free_space | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | bool | , |
nav_dir_root | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | bool | , |
nav_dir_cd | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | bool | , |
nav_dir_gotoparent | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | bool | , |
nav_file_isdir | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | bool | , |
nav_file_next | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | bool | , |
nav_file_previous | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | bool | , |
nav_file_goto | , | ||
uint32_t | , | ||
u32_newpos | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | uint16_t | , |
nav_file_pos | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | uint16_t | , |
nav_file_nb | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | uint16_t | , |
nav_dir_nb | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | uint16_t | , |
nav_playlist_nb | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | uint32_t | , |
nav_file_info_type | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | uint16_t | , |
nav_file_info_year | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | uint32_t | , |
nav_file_info_track | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | uint32_t | , |
nav_file_info_duration | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | bool | , |
nav_getplayfile | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | bool | , |
audio_nav_playfile | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | bool | , |
audio_nav_next | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | bool | , |
audio_nav_previous | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | bool | , |
audio_nav_eof_occur | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | uint16_t | , |
audio_nav_nb | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | uint16_t | , |
audio_nav_getpos | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | bool | , |
audio_nav_setpos | , | ||
uint16_t | , | ||
u16_pos | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | Ai_repeat_mode | , |
audio_nav_repeat_get | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | Ai_shuffle_mode | , |
audio_nav_shuffle_get | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | Ai_explorer_mode | , |
audio_nav_expmode_get | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | uint32_t | , |
audio_nav_file_info_type | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | uint16_t | , |
audio_nav_file_info_year | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | uint32_t | , |
audio_nav_file_info_track | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | uint32_t | , |
audio_nav_file_info_duration | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | bool | , |
audio_ctrl_stop | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | bool | , |
audio_ctrl_resume | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | bool | , |
audio_ctrl_pause | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | uint32_t | , |
audio_ctrl_time | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | bool | , |
audio_ctrl_ffw | , | ||
uint32_t | , | ||
u32_duration | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | bool | , |
audio_ctrl_frw | , | ||
uint32_t | , | ||
u32_duration | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | bool | , |
audio_ctrl_start_ffw | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | bool | , |
audio_ctrl_start_frw | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VALUE | ( | bool | , |
audio_ctrl_stop_ffw_frw | , | ||
void | , | ||
0 | |||
) |
AI_SYNC_FUNC_RET_VOID | ( | audio_nav_repeat_set | , |
Ai_repeat_mode | , | ||
repeat_mode | |||
) |
AI_SYNC_FUNC_RET_VOID | ( | audio_nav_shuffle_set | , |
Ai_shuffle_mode | , | ||
shuffle | |||
) |
AI_SYNC_FUNC_RET_VOID | ( | audio_nav_expmode_set | , |
Ai_explorer_mode | , | ||
exp_mode | |||
) |
void ai_task | ( | void | ) |
Task for the internal behaviors of the Audio Interface.
References AI_NONE, AI_PRIORITY_CALL, AI_TASK_SELECT_FCT_SET, and status.
Referenced by main().
bool is_ai_async_cmd_finished | ( | void | ) |
Tests if the current asynchronous routine is finished.
References g_b_ai_cmd_received.
Referenced by ai_audio_context_save(), ai_audio_nav_file_info_image(), ai_nav_file_info_image(), codec_mp3_task(), codec_wav_task(), and com_task().
const ai_fct_set ai_default_fct_set |
Referenced by ai_init().
const ai_fct_set* ai_fct_set_tab[4] |
uint8_t current_ai_fct_set = AI_NONE |
Referenced by ai_async_cmd_task(), and ai_specific_async_cmd_task().
|
static |
Referenced by ai_async_cmd_out_free_ArrayU8(), ai_async_cmd_out_PtrArrayU8(), ai_async_cmd_put(), and ai_async_cmd_task().
ai_async_status_t g_ai_cmd_execution_status |
Referenced by ai_async_cmd_out_status(), ai_async_cmd_task(), ai_command_abort(), and ai_specific_async_cmd_task().
|
static |
Referenced by ai_async_cmd_put(), and ai_async_cmd_task().
|
static |
Referenced by ai_async_cmd_out_status(), ai_async_cmd_task(), ai_command_abort(), and ai_init().
|
static |
Referenced by ai_async_cmd_out_free_ArrayU8(), ai_async_cmd_out_SizeArrayU8(), ai_async_cmd_put(), and ai_async_cmd_task().
|
static |
Referenced by ai_async_cmd_put(), and ai_async_cmd_task().
|
static |
Referenced by ai_async_cmd_out_u32(), and ai_async_cmd_task().
|
static |
Referenced by ai_async_cmd_out_u64(), and ai_async_cmd_task().
volatile bool g_b_ai_cmd_received |
Referenced by ai_async_cmd_put(), ai_async_cmd_task(), ai_command_abort(), ai_init(), and is_ai_async_cmd_finished().
uint8_t g_retry_cnt |
Number of retries before aborting the command.
Referenced by ai_async_cmd_put().