Copyright (C) 2006-2010, Brainspark B.V.
This file is part of PolarSSL (http://www.polarssl.org) Lead Maintainer: Paul Bakker <polarssl_maintainer at polarssl.org>
All rights reserved.
This program is free software; you can redistribute it and/or modify it under the terms of the GNU General Public License as published by the Free Software Foundation; either version 2 of the License, or (at your option) any later version.
This program is distributed in the hope that it will be useful, but WITHOUT ANY WARRANTY; without even the implied warranty of MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU General Public License for more details.
You should have received a copy of the GNU General Public License along with this program; if not, write to the Free Software Foundation, Inc., 51 Franklin Street, Fifth Floor, Boston, MA 02110-1301 USA.
Macros | |
#define | POLARSSL_ERR_BASE64_BUFFER_TOO_SMALL 0x0010 |
#define | POLARSSL_ERR_BASE64_INVALID_CHARACTER 0x0012 |
Functions | |
int | base64_decode (unsigned char *dst, int *dlen, const unsigned char *src, int slen) |
Decode a base64-formatted buffer. More... | |
int | base64_encode (unsigned char *dst, int *dlen, const unsigned char *src, int slen) |
Encode a buffer into base64 format. More... | |
int | base64_self_test (int verbose) |
Checkup routine. More... | |
#define POLARSSL_ERR_BASE64_BUFFER_TOO_SMALL 0x0010 |
#define POLARSSL_ERR_BASE64_INVALID_CHARACTER 0x0012 |
int base64_decode | ( | unsigned char * | dst, |
int * | dlen, | ||
const unsigned char * | src, | ||
int | slen | ||
) |
Decode a base64-formatted buffer.
dst | destination buffer |
dlen | size of the buffer |
src | source buffer |
slen | amount of data to be decoded |
int base64_encode | ( | unsigned char * | dst, |
int * | dlen, | ||
const unsigned char * | src, | ||
int | slen | ||
) |
Encode a buffer into base64 format.
dst | destination buffer |
dlen | size of the buffer |
src | source buffer |
slen | amount of data to be encoded |
int base64_self_test | ( | int | verbose | ) |