USB host configuration file.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | USB_HOST_UHI UHI_AOA |
USB Host Configuration. More... | |
#define | USB_HOST_POWER_MAX 500 |
Maximum current allowed on Vbus (mA) More... | |
#define | UHC_MODE_CHANGE(b_host_mode) ui_usb_mode_change(b_host_mode) |
Authorize the USB HUB support. More... | |
#define | UHC_VBUS_CHANGE(b_present) ui_usb_vbus_change(b_present) |
To notify that the Vbus level has changed. More... | |
#define | UHC_VBUS_ERROR() ui_usb_vbus_error() |
To notify that a Vbus error has occurred. More... | |
#define | UHC_CONNECTION_EVENT(dev, b_present) ui_usb_connection_event(dev, b_present) |
To notify that a device has been connected or disconnected. More... | |
#define | UHC_WAKEUP_EVENT() ui_usb_wakeup_event() |
Called when a USB device or the host have wake up the USB line. More... | |
#define | UHC_SOF_EVENT() ui_usb_sof_event() |
Called for each received SOF each 1 ms. More... | |
#define | UHC_ENUM_EVENT(dev, b_status) ui_usb_enum_event(dev, b_status) |
Called when a USB device configuration must be chosen Thus, the application can choose either a configuration number for this device or a configuration number 0 to reject it. More... | |
#define | UHI_AOA_CHANGE(dev, b_plug) ui_uhi_aoa_change(dev, b_plug) |
USB Interface Configuration. More... | |
#define UHC_CONNECTION_EVENT | ( | dev, | |
b_present | |||
) | ui_usb_connection_event(dev, b_present) |
To notify that a device has been connected or disconnected.
#define UHC_ENUM_EVENT | ( | dev, | |
b_status | |||
) | ui_usb_enum_event(dev, b_status) |
Called when a USB device configuration must be chosen Thus, the application can choose either a configuration number for this device or a configuration number 0 to reject it.
If callback not defined the configuration 1 is chosen Called when a USB device enumeration is completed
#define UHC_MODE_CHANGE | ( | b_host_mode | ) | ui_usb_mode_change(b_host_mode) |
Authorize the USB HUB support.
USB Host callbacksTo notify that the USB mode are switched automatically This is possible only when ID pin is available
#define UHC_SOF_EVENT | ( | ) | ui_usb_sof_event() |
Called for each received SOF each 1 ms.
Note: Available in High and Full speed mode
#define UHC_VBUS_CHANGE | ( | b_present | ) | ui_usb_vbus_change(b_present) |
To notify that the Vbus level has changed.
Available only in USB hardware with Vbus monitoring
#define UHC_VBUS_ERROR | ( | ) | ui_usb_vbus_error() |
To notify that a Vbus error has occurred.
Available only in USB hardware with Vbus monitoring
#define UHC_WAKEUP_EVENT | ( | ) | ui_usb_wakeup_event() |
Called when a USB device or the host have wake up the USB line.
#define UHI_AOA_CHANGE | ( | dev, | |
b_plug | |||
) | ui_uhi_aoa_change(dev, b_plug) |
USB Interface Configuration.
Configuration of AOA Interface
Referenced by uhi_aoa_enable_success(), and uhi_aoa_uninstall().
#define USB_HOST_POWER_MAX 500 |
Maximum current allowed on Vbus (mA)
#define USB_HOST_UHI UHI_AOA |
USB Host Configuration.
Array of UHI APIs Define the list of UHI supported by USB host