Microchip® Advanced Software Framework

common/services/usb/class/phdc/device/example/main.c File Reference

Main functions.

Copyright (c) 2012-2018 Microchip Technology Inc. and its subsidiaries.

#include <asf.h>
#include "conf_usb.h"
#include "ui.h"
#include "ieee11073_skeleton.h"

Functions

int main (void)
 Main function. Execution starts here. More...
 
void main_phdc_disable (void)
 Called by PHDC interface Callback running when USB Host disable PHDC interface. More...
 
bool main_phdc_enable (void)
 Called by PHDC interface Callback running when USB Host enable PHDC interface. More...
 
void main_resume_action (void)
 Called by UDD when the USB line exit of suspend state. More...
 
void main_sof_action (void)
 Called when a start of frame is received on USB line. More...
 
void main_suspend_action (void)
 Enters the application in low power mode Callback called when USB host sets USB line in suspend state. More...
 

Variables

static volatile bool main_b_phdc_enable = false
 

void main_phdc_disable ( void  )

Called by PHDC interface Callback running when USB Host disable PHDC interface.

References ieee11073_skeleton_disable(), and main_b_phdc_enable.

bool main_phdc_enable ( void  )

Called by PHDC interface Callback running when USB Host enable PHDC interface.

Return values
trueif phdc startup is ok

References ieee11073_skeleton_enable(), and main_b_phdc_enable.

void main_resume_action ( void  )

Called by UDD when the USB line exit of suspend state.

Turn on a led to notify active mode Called when the USB line is resumed from the suspend state.

References ui_wakeup().

void main_sof_action ( void  )

Called when a start of frame is received on USB line.

Manages the leds behaviors Called when a start of frame is received on USB line each 1ms.

References main_b_phdc_enable, udd_get_frame_number(), and ui_process().

void main_suspend_action ( void  )

Enters the application in low power mode Callback called when USB host sets USB line in suspend state.

Turn off all leds Callback running when USB Host set USB line in suspend state.

Called by UDD when a suspend is received Callback running when USB Host set USB line in suspend state.

References ui_powerdown().

volatile bool main_b_phdc_enable = false
static