Macros | |
#define | _32_BITS_RATIO(frequency, fosc) ((int)(((float)frequency/(fosc))*(1<<20))) |
Build the 32-bits ratio constant to be loaded in the CS2200 to make the desired frequency. More... | |
#define | PPM(value, ppm) ( ((int)( (long long)value*(ppm)/1000000) ) ) |
Compute the PPM of a number. More... | |
#define | PPM_ADD(value, ppm) ( ((int)(value + (long long)value*(ppm)/1000000)) ) |
Add x PPM to a value. More... | |
#define | PPM_SUB(value, ppm) ( ((int)(value - (long long)value*(ppm)/1000000)) ) |
Remove x PPM to a value. More... | |
Communication Interfaces | |
#define | CS2200_INTERFACE_SPI 1 |
#define | CS2200_INTERFACE_TWI 2 |
Macro Constructors | |
These macros create inline functions to access the cs2200 registers. | |
#define | CS2200_READ(name) |
#define | CS2200_READ1(name) |
#define | CS2200_READ2(name) |
#define | CS2200_READ4(name) |
#define | CS2200_WRITE(name) |
#define | CS2200_WRITE1(name) |
#define | CS2200_WRITE2(name) |
#define | CS2200_WRITE4(name) |
Register Addresses | |
#define | CS2200_REG_TEST_MODE_1_ADDR 0x00 |
#define | CS2200_REG_DEVICE_ID_ADDR 0x01 |
#define | CS2200_REG_DEVICE_CTRL_ADDR 0x02 |
#define | CS2200_REG_DEVICE_CFG_1_ADDR 0x03 |
#define | CS2200_REG_GLOBAL_CFG_ADDR 0x05 |
#define | CS2200_REG_32_BITS_RATIO_ADDR 0x06 |
#define | CS2200_REG_LSW_RATIO_ADDR 0x08 |
#define | CS2200_REG_LSB_RATIO_ADDR 0x09 |
#define | CS2200_REG_FUNCT_CFG_1_ADDR 0x16 |
#define | CS2200_REG_FUNCT_CFG_2_ADDR 0x17 |
#define | CS2200_REG_TEST_MODE_2_ADDR 0x77 |
Functions | |
void | cs2200_enter_power_down_mode (void) |
Enter power down mode and stop twi comms. More... | |
void | cs2200_enter_test_mode (void) |
Enter into the test mode. More... | |
void | cs2200_freq_clk_adjust (uint16_t lsw_ratio) |
Function used to adjust the CLK_OUT frequency (LSW only). More... | |
void | cs2200_freq_clk_out (uint32_t ratio) |
Function used to program the CLK_OUT frequency. More... | |
void | cs2200_leave_power_down_mode (void) |
Leave power down mode and twi comms can be restarted. More... | |
void | cs2200_leave_test_mode (void) |
Leave the test mode. More... | |
void | cs2200_read (uint8_t address, void *buffer, uint8_t len) |
Reads data from the CS2200 chip. More... | |
CS2200_READ1 (DEVICE_ID) | |
CS2200_READ1 (DEVICE_CTRL) | |
CS2200_READ1 (DEVICE_CFG_1) | |
CS2200_READ1 (GLOBAL_CFG) | |
CS2200_READ1 (FUNCT_CFG_1) | |
CS2200_READ1 (FUNCT_CFG_2) | |
CS2200_READ4 (32_BITS_RATIO) | |
void | cs2200_set_new_freq_clk_out (uint32_t ratio) |
Function used to program the CLK_OUT frequency and wait that the PLL is locked. More... | |
bool | cs2200_setup (uint32_t out_freq, uint32_t fosc) |
Function used to initialize the chip and communication interface. More... | |
void | cs2200_switch_off (void) |
void | cs2200_switch_on (void) |
void | cs2200_write (uint8_t address, const void *buffer, uint8_t len) |
Writes data into the CS2200 chip. More... | |
CS2200_WRITE1 (DEVICE_CTRL) | |
CS2200_WRITE1 (DEVICE_CFG_1) | |
CS2200_WRITE1 (GLOBAL_CFG) | |
CS2200_WRITE1 (LSB_RATIO) | |
CS2200_WRITE1 (FUNCT_CFG_1) | |
CS2200_WRITE1 (FUNCT_CFG_2) | |
CS2200_WRITE1 (TEST_MODE_1) | |
CS2200_WRITE1 (TEST_MODE_2) | |
CS2200_WRITE4 (32_BITS_RATIO) | |
int | cs2200_write_ex (uint8_t address, const void *buffer, uint8_t len) |
Writes data into the CS2200 chip using the non blocking release of the TWI driver. More... | |
#define _32_BITS_RATIO | ( | frequency, | |
fosc | |||
) | ((int)(((float)frequency/(fosc))*(1<<20))) |
Build the 32-bits ratio constant to be loaded in the CS2200 to make the desired frequency.
Referenced by aic23b_dac_setup(), cs2200_setup(), ms3_dac_setup(), usb_stream_input(), and usb_stream_resync().
#define CS2200_INTERFACE_SPI 1 |
#define CS2200_INTERFACE_TWI 2 |
#define CS2200_READ | ( | name | ) |
#define CS2200_READ1 | ( | name | ) |
#define CS2200_READ2 | ( | name | ) |
#define CS2200_READ4 | ( | name | ) |
#define CS2200_REG_32_BITS_RATIO_ADDR 0x06 |
#define CS2200_REG_DEVICE_CFG_1_ADDR 0x03 |
#define CS2200_REG_DEVICE_CTRL_ADDR 0x02 |
#define CS2200_REG_DEVICE_ID_ADDR 0x01 |
#define CS2200_REG_FUNCT_CFG_1_ADDR 0x16 |
#define CS2200_REG_FUNCT_CFG_2_ADDR 0x17 |
#define CS2200_REG_GLOBAL_CFG_ADDR 0x05 |
#define CS2200_REG_LSB_RATIO_ADDR 0x09 |
#define CS2200_REG_LSW_RATIO_ADDR 0x08 |
Referenced by cs2200_freq_clk_adjust().
#define CS2200_REG_TEST_MODE_1_ADDR 0x00 |
#define CS2200_REG_TEST_MODE_2_ADDR 0x77 |
#define CS2200_WRITE | ( | name | ) |
#define CS2200_WRITE1 | ( | name | ) |
#define CS2200_WRITE2 | ( | name | ) |
#define CS2200_WRITE4 | ( | name | ) |
#define PPM | ( | value, | |
ppm | |||
) | ( ((int)( (long long)value*(ppm)/1000000) ) ) |
Compute the PPM of a number.
#define PPM_ADD | ( | value, | |
ppm | |||
) | ( ((int)(value + (long long)value*(ppm)/1000000)) ) |
Add x PPM to a value.
#define PPM_SUB | ( | value, | |
ppm | |||
) | ( ((int)(value - (long long)value*(ppm)/1000000)) ) |
Remove x PPM to a value.
void cs2200_enter_power_down_mode | ( | void | ) |
Enter power down mode and stop twi comms.
void cs2200_enter_test_mode | ( | void | ) |
Enter into the test mode.
Referenced by cs2200_setup().
void cs2200_freq_clk_adjust | ( | uint16_t | lsw_ratio | ) |
Function used to adjust the CLK_OUT frequency (LSW only).
References CS2200_REG_LSW_RATIO_ADDR, and cs2200_write_ex().
Referenced by usb_stream_resync().
void cs2200_freq_clk_out | ( | uint32_t | ratio | ) |
Function used to program the CLK_OUT frequency.
Referenced by aic23b_dac_setup(), ms3_dac_setup(), and usb_stream_input().
void cs2200_leave_power_down_mode | ( | void | ) |
Leave power down mode and twi comms can be restarted.
void cs2200_leave_test_mode | ( | void | ) |
Leave the test mode.
void cs2200_read | ( | uint8_t | address, |
void * | buffer, | ||
uint8_t | len | ||
) |
Reads data from the CS2200 chip.
CS2200_READ1 | ( | DEVICE_ID | ) |
CS2200_READ1 | ( | DEVICE_CTRL | ) |
CS2200_READ1 | ( | DEVICE_CFG_1 | ) |
CS2200_READ1 | ( | GLOBAL_CFG | ) |
CS2200_READ1 | ( | FUNCT_CFG_1 | ) |
CS2200_READ1 | ( | FUNCT_CFG_2 | ) |
CS2200_READ4 | ( | 32_BITS_RATIO | ) |
void cs2200_set_new_freq_clk_out | ( | uint32_t | ratio | ) |
Function used to program the CLK_OUT frequency and wait that the PLL is locked.
bool cs2200_setup | ( | uint32_t | out_freq, |
uint32_t | fosc | ||
) |
Function used to initialize the chip and communication interface.
References _32_BITS_RATIO, CS2200_DEVICE_ID_REG_MASK, CS2200_DEVICE_ID_REG_OFFSET, cs2200_enter_test_mode(), CS2200_EXPECTED_DEVICE_ID, and CS2200_NB_TRIES.
Referenced by main().
void cs2200_switch_off | ( | void | ) |
void cs2200_switch_on | ( | void | ) |
void cs2200_write | ( | uint8_t | address, |
const void * | buffer, | ||
uint8_t | len | ||
) |
Writes data into the CS2200 chip.
CS2200_WRITE1 | ( | DEVICE_CTRL | ) |
CS2200_WRITE1 | ( | DEVICE_CFG_1 | ) |
CS2200_WRITE1 | ( | GLOBAL_CFG | ) |
CS2200_WRITE1 | ( | LSB_RATIO | ) |
CS2200_WRITE1 | ( | FUNCT_CFG_1 | ) |
CS2200_WRITE1 | ( | FUNCT_CFG_2 | ) |
CS2200_WRITE1 | ( | TEST_MODE_1 | ) |
CS2200_WRITE1 | ( | TEST_MODE_2 | ) |
CS2200_WRITE4 | ( | 32_BITS_RATIO | ) |
int cs2200_write_ex | ( | uint8_t | address, |
const void * | buffer, | ||
uint8_t | len | ||
) |
Writes data into the CS2200 chip using the non blocking release of the TWI driver.
Referenced by cs2200_freq_clk_adjust().