Microchip® Advanced Software Framework

fixed_t.h File Reference

ASF Sensor API fixed point math operations.

This header defines types and operations that support basic fixed-point arithmetic operations. The fixed_t type is a signed 32-bit value that is stored and operated on using integer operations. The number of fractional bits operated on will be context-specific.

The conversion functions and some of the arithmetic functions require a Q parameter specifying the number of fractional bits in the operands. Arithmetic functions that do not require the Q parameter assume that both operands have the same Q format (the same number of fractional bits).

Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.

#include <assert.h>
#include <stdint.h>
#include <stdbool.h>
#include <math.h>

Typedefs

typedef int32_t fixed_t
 Signed fixed-point format storage type. More...
 

Functions

static fixed_t fixed_conv (fixed_t a, int q1, int q2)
 fixed point Q format conversion More...
 
Type Conversion Primitives
static fixed_t long_to_fixed (long n, int Q)
 
static fixed_t float_to_fixed (float x, int Q)
 
static fixed_t double_to_fixed (double x, int Q)
 
static long fixed_to_long (fixed_t f, int Q)
 
static float fixed_to_float (fixed_t f, int Q)
 
static double fixed_to_double (fixed_t f, int Q)
 
Addition and Subtraction Primitives
static fixed_t fixed_add (fixed_t a, fixed_t b)
 
static fixed_t fixed_addl (fixed_t a, long b, int Q)
 
static fixed_t fixed_sub (fixed_t a, fixed_t b)
 
static fixed_t fixed_subl (fixed_t a, long b, int Q)
 
Multiplication and Division Primitives
static fixed_t fixed_mul (fixed_t a, fixed_t b, int Q)
 
static fixed_t fixed_mull (fixed_t a, long b)
 
static fixed_t fixed_mul_rounded (fixed_t a, fixed_t b, int Q)
 
static fixed_t fixed_div (fixed_t a, fixed_t b, int Q)
 
static fixed_t fixed_divl (fixed_t a, long b)
 
static fixed_t fixed_div_rounded (fixed_t a, fixed_t b, int Q)
 
Algebraic and Transcendental Functions
fixed_t fixed_sqrt (fixed_t f, int Q)
 Calculate the square root of an integer. More...
 
fixed-point resolution and range utilities

The fixed_range() and fixed_resolution() utilities can be used to define, verify, test, and characterize fixed-point formats for applications that are being converted from floating-point or implemented in fixed-point.

int fixed_range (double x_min, double x_max)
 signed fixed-point range More...
 
int fixed_resolution (double epsilon)
 signed fixed-point resolution More...
 

typedef int32_t fixed_t

Signed fixed-point format storage type.

static fixed_t double_to_fixed ( double  x,
int  Q 
)
inlinestatic
static fixed_t fixed_add ( fixed_t  a,
fixed_t  b 
)
inlinestatic
static fixed_t fixed_addl ( fixed_t  a,
long  b,
int  Q 
)
inlinestatic

References long_to_fixed().

static fixed_t fixed_conv ( fixed_t  a,
int  q1,
int  q2 
)
inlinestatic

fixed point Q format conversion

This routine performs a change of exponent operation where fixed-point value a in q1 format is converted to q2 format. The change of binary exponent is derived from the following relation:

\[ n2^{-p} = k2^{-r} \Longrightarrow k = n2^{r - p} \]

Thus, the converted value k is obtained by dividing n by \( 2^{p - r} \) when \( (p > r) \) or by multiplying by \( 2^{r - p} \) when \( (r \ge p) \).

static fixed_t fixed_div ( fixed_t  a,
fixed_t  b,
int  Q 
)
inlinestatic
static fixed_t fixed_div_rounded ( fixed_t  a,
fixed_t  b,
int  Q 
)
inlinestatic
static fixed_t fixed_divl ( fixed_t  a,
long  b 
)
inlinestatic
static fixed_t fixed_mul ( fixed_t  a,
fixed_t  b,
int  Q 
)
inlinestatic
static fixed_t fixed_mul_rounded ( fixed_t  a,
fixed_t  b,
int  Q 
)
inlinestatic
static fixed_t fixed_mull ( fixed_t  a,
long  b 
)
inlinestatic
int fixed_range ( double  x_min,
double  x_max 
)

signed fixed-point range

Given a signed fixed-point format Qm.f, where f represents the number of fractional bits and m the number of integer bits, this routine calculates the the number of integer bits m required to represent real data types in the interval [x_min, x_max].

The x_min and x_max interval endpoints are the smallest and largest integer portions, respectively, of the numbers that must be represented in fixed-point.

Parameters
x_minThe smallest signed integer portion of a real type.
x_maxThe largest signed integer portion of a real type.
Returns
The required number of integer bits required for a fixed-point implementation.

References a().

int fixed_resolution ( double  epsilon)

signed fixed-point resolution

Given a signed fixed-point format Qm.f, where f represents the number of fractional bits and m the number of integer bits, this routine calculates the the number of fractional bits f required to represent real data types with resolution \( \epsilon = \frac{1}{2^{f}} \). For example, a signed variable A = 3.141 requires <= 0.001.

Parameters
epsilonThe required resolution of the fixed-point number.
Returns
The required number of fractional bits required for a fixed-point implementation.

Given a signed fixed-point format Qm.f, where f represents the number of fractional bits and m the number of integer bits, this routine calculates the the number of fractional bits f required to represent real data types with resolution

\[ \epsilon = \frac{1}{2^{f}} \]

. For example, a signed variable A = 3.141 requires <= 0.001.

Parameters
epsilonThe required resolution of the fixed-point number.
Returns
The required number of fractional bits required for a fixed-point implementation.
fixed_t fixed_sqrt ( fixed_t  f,
int  Q 
)

Calculate the square root of an integer.

This routine calculates the integer square root, isqrt(), of a positive integer argument n:

\[ isqrt(n) = \lfloor n^{1/2} \rfloor \]

The computed value is the largest positive integer m with a square that is less than or equal to the given integer n such that \( m^{2} \le n \).

Parameters
fA fixed-point value. Negative values will be computed using the unsigned magnitude without reporting a domain error.
QThe number of fractional bits in parameter f.
Returns
The integer square root.

References b, clzll, n, and temp.

static fixed_t fixed_sub ( fixed_t  a,
fixed_t  b 
)
inlinestatic
static fixed_t fixed_subl ( fixed_t  a,
long  b,
int  Q 
)
inlinestatic

References long_to_fixed().

static double fixed_to_double ( fixed_t  f,
int  Q 
)
inlinestatic
static float fixed_to_float ( fixed_t  f,
int  Q 
)
inlinestatic
static long fixed_to_long ( fixed_t  f,
int  Q 
)
inlinestatic
static fixed_t float_to_fixed ( float  x,
int  Q 
)
inlinestatic
static fixed_t long_to_fixed ( long  n,
int  Q 
)
inlinestatic

Referenced by fixed_addl(), and fixed_subl().