Copyright (C) 2006-2010, Brainspark B.V.
This file is part of PolarSSL (http://www.polarssl.org) Lead Maintainer: Paul Bakker <polarssl_maintainer at polarssl.org>
All rights reserved.
This program is free software; you can redistribute it and/or modify it under the terms of the GNU General Public License as published by the Free Software Foundation; either version 2 of the License, or (at your option) any later version.
This program is distributed in the hope that it will be useful, but WITHOUT ANY WARRANTY; without even the implied warranty of MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU General Public License for more details.
You should have received a copy of the GNU General Public License along with this program; if not, write to the Free Software Foundation, Inc., 51 Franklin Street, Fifth Floor, Boston, MA 02110-1301 USA.
Data Structures | |
struct | havege_state |
HAVEGE state structure. More... | |
Macros | |
#define | COLLECT_SIZE 1024 |
Functions | |
void | havege_init (havege_state *hs) |
HAVEGE initialization. More... | |
int | havege_rand (void *p_rng) |
HAVEGE rand function. More... | |
#define COLLECT_SIZE 1024 |
void havege_init | ( | havege_state * | hs | ) |
HAVEGE initialization.
hs | HAVEGE state to be initialized |
int havege_rand | ( | void * | p_rng | ) |
HAVEGE rand function.
p_rng | A HAVEGE state |