Microchip® Advanced Software Framework

lwip-1.4.1/src/include/lwip/mem.h File Reference
#include "lwip/opt.h"

Macros

#define LWIP_MEM_ALIGN(addr)   ((void *)(((mem_ptr_t)(addr) + MEM_ALIGNMENT - 1) & ~(mem_ptr_t)(MEM_ALIGNMENT-1)))
 Align a memory pointer to the alignment defined by MEM_ALIGNMENT so that ADDR % MEM_ALIGNMENT == 0. More...
 
#define LWIP_MEM_ALIGN_BUFFER(size)   (((size) + MEM_ALIGNMENT - 1))
 Calculate safe memory size for an aligned buffer when using an unaligned type as storage. More...
 
#define LWIP_MEM_ALIGN_SIZE(size)   (((size) + MEM_ALIGNMENT - 1) & ~(MEM_ALIGNMENT-1))
 Calculate memory size for an aligned buffer - returns the next highest multiple of MEM_ALIGNMENT (e.g. More...
 
#define MEM_SIZE_F   U16_F
 

Typedefs

typedef u16_t mem_size_t
 

Functions

void * mem_calloc (mem_size_t count, mem_size_t size)
 Contiguously allocates enough space for count objects that are size bytes of memory each and returns a pointer to the allocated memory. More...
 
void mem_free (void *mem)
 Put a struct mem back on the heap. More...
 
void mem_init (void)
 Zero the heap and initialize start, end and lowest-free. More...
 
void * mem_malloc (mem_size_t size)
 Adam's mem_malloc() plus solution for bug #17922 Allocate a block of memory with a minimum of 'size' bytes. More...
 
void * mem_trim (void *mem, mem_size_t size)
 Shrink memory returned by mem_malloc(). More...
 

#define LWIP_MEM_ALIGN (   addr)    ((void *)(((mem_ptr_t)(addr) + MEM_ALIGNMENT - 1) & ~(mem_ptr_t)(MEM_ALIGNMENT-1)))

Align a memory pointer to the alignment defined by MEM_ALIGNMENT so that ADDR % MEM_ALIGNMENT == 0.

Referenced by mem_init(), memp_init(), and pbuf_alloc().

#define LWIP_MEM_ALIGN_BUFFER (   size)    (((size) + MEM_ALIGNMENT - 1))

Calculate safe memory size for an aligned buffer when using an unaligned type as storage.

This includes a safety-margin on (MEM_ALIGNMENT - 1) at the start (e.g. if buffer is u8_t[] and actual data will be u32_t*)

#define LWIP_MEM_ALIGN_SIZE (   size)    (((size) + MEM_ALIGNMENT - 1) & ~(MEM_ALIGNMENT-1))

Calculate memory size for an aligned buffer - returns the next highest multiple of MEM_ALIGNMENT (e.g.

LWIP_MEM_ALIGN_SIZE(3) and LWIP_MEM_ALIGN_SIZE(4) will both yield 4 for MEM_ALIGNMENT == 4).

Referenced by mem_malloc(), mem_realloc(), mem_trim(), and pbuf_alloc().

#define MEM_SIZE_F   U16_F

typedef u16_t mem_size_t

void* mem_calloc ( mem_size_t  count,
mem_size_t  size 
)

Contiguously allocates enough space for count objects that are size bytes of memory each and returns a pointer to the allocated memory.

The allocated memory is filled with bytes of value zero.

Parameters
countnumber of objects to allocate
sizesize of the objects to allocate
Returns
pointer to allocated memory / NULL pointer if there is an error
void mem_free ( void *  rmem)

Put a struct mem back on the heap.

Parameters
rmemis the data portion of a struct mem as returned by a previous call to mem_malloc()
void mem_init ( void  )

Zero the heap and initialize start, end and lowest-free.

void* mem_malloc ( mem_size_t  size)

Adam's mem_malloc() plus solution for bug #17922 Allocate a block of memory with a minimum of 'size' bytes.

Parameters
sizeis the minimum size of the requested block in bytes.
Returns
pointer to allocated memory or NULL if no free memory was found.

Note that the returned value will always be aligned (as defined by MEM_ALIGNMENT).

void* mem_trim ( void *  rmem,
mem_size_t  newsize 
)

Shrink memory returned by mem_malloc().

Parameters
rmempointer to memory allocated by mem_malloc the is to be shrinked
newsizerequired size after shrinking (needs to be smaller than or equal to the previous size)
Returns
for compatibility reasons: is always == rmem, at the moment or NULL if newsize is > old size, in which case rmem is NOT touched or freed!