Functions | |
void | ethernetif_input (void *pvParameters) |
This function should be called when a packet is ready to be read from the interface. More... | |
void ethernetif_input | ( | void * | pvParameters | ) |
This function should be called when a packet is ready to be read from the interface.
It uses the function low_level_input() that should handle the actual reception of bytes from the network interface. Then the type of the received packet is determined and the appropriate input function is called.
netif | the lwip network interface structure for this ethernetif |
References ERR_OK, netif::input, low_level_input(), NULL, pbuf_free(), and vMACBWaitForInput().
Referenced by low_level_init().