Microchip® Advanced Software Framework

lwip-port-1.4.0/hd/if/include/lwipopts_example.h File Reference

lwIP Options Configuration

This is a default configuration that is usually overridden by a configuration file tuned for a specific application.

#include <wl_api.h>

Macros

#define ETH_PAD_SIZE   WL_HEADER_SIZE /* size of wifiengine header */
 
#define ICMP_TTL   (IP_DEFAULT_TTL)
 ICMP_TTL: Default value for Time-To-Live used by ICMP packets. More...
 
#define IP_DEFAULT_TTL   255
 IP_DEFAULT_TTL: Default value for Time-To-Live used by transport layers. More...
 
#define IP_FORWARD   0
 IP_FORWARD==1: Enables the ability to forward IP packets across network interfaces. More...
 
#define IP_FRAG   1
 IP_FRAG==1: Fragment outgoing IP packets if their size exceeds MTU. More...
 
#define IP_FRAG_USES_STATIC_BUF   0
 IP_FRAG_USES_STATIC_BUF==1: Use a static MTU-sized buffer for IP fragmentation. More...
 
#define IP_OPTIONS_ALLOWED   1
 IP_OPTIONS: Defines the behavior for IP options. More...
 
#define IP_REASS_MAX_PBUFS   10
 IP_REASS_MAX_PBUFS: Total maximum amount of pbufs waiting to be reassembled. More...
 
#define IP_REASS_MAXAGE   3
 IP_REASS_MAXAGE: Maximum time (in multiples of IP_TMR_INTERVAL - so seconds, normally) a fragmented IP packet waits for all fragments to arrive. More...
 
#define IP_REASSEMBLY   1
 IP_REASSEMBLY==1: Reassemble incoming fragmented IP packets. More...
 
#define LINK_STATS   1
 
#define LWIP_ARP   1
 LWIP_ARP==1: Enable ARP functionality. More...
 
#define LWIP_AUTOIP   0
 LWIP_AUTOIP==1: Enable AUTOIP module. More...
 
#define LWIP_DHCP   1
 LWIP_DHCP==1: Enable DHCP module. More...
 
#define LWIP_DNS   1
 LWIP_DNS==1: Turn on DNS module. More...
 
#define LWIP_HAVE_LOOPIF   1
 LWIP_HAVE_LOOPIF==1: Support loop interface (127.0.0.1) and loopif.c. More...
 
#define LWIP_ICMP   1
 LWIP_ICMP==1: Enable ICMP module inside the IP stack. More...
 
#define LWIP_IGMP   1
 LWIP_IGMP==1: Turn on IGMP module. More...
 
#define LWIP_LOOPIF_MULTITHREADING   0
 
#define LWIP_NETCONN   0
 LWIP_NETCONN==1: Enable Netconn API (require to use api_lib.c) More...
 
#define LWIP_NETIF_LINK_CALLBACK   1
 
#define LWIP_NETIF_STATUS_CALLBACK   1
 
#define LWIP_RAW   1
 LWIP_RAW==1: Enable application layer to hook into the IP layer itself. More...
 
#define LWIP_SNMP   0
 LWIP_SNMP==1: Turn on SNMP module. More...
 
#define LWIP_SOCKET   0
 LWIP_SOCKET==1: Enable Socket API (require to use sockets.c) More...
 
#define LWIP_STATS   1
 LWIP_STATS==1: Enable statistics collection in lwip_stats. More...
 
#define LWIP_TCP   1
 LWIP_TCP==1: Turn on TCP. More...
 
#define LWIP_TIMEVAL_PRIVATE   0
 
#define LWIP_UDP   1
 LWIP_UDP==1: Turn on UDP. More...
 
#define LWIP_UDPLITE   0
 LWIP_UDPLITE==1: Turn on UDP-Lite. More...
 
#define MEM_ALIGNMENT   4
 MEM_ALIGNMENT: should be set to the alignment of the CPU 4 byte alignment -> #define MEM_ALIGNMENT 4 2 byte alignment -> #define MEM_ALIGNMENT 2. More...
 
#define MEM_LIBC_MALLOC   1
 
#define MEM_SIZE   16000
 MEM_SIZE: the size of the heap memory. More...
 
#define MEMP_NUM_ARP_QUEUE   2
 MEMP_NUM_ARP_QUEUE: the number of simulateously queued outgoing packets (pbufs) that are waiting for an ARP request (to resolve their destination address) to finish. More...
 
#define MEMP_NUM_NETBUF   0
 MEMP_NUM_NETBUF: the number of struct netbufs. More...
 
#define MEMP_NUM_NETCONN   0
 MEMP_NUM_NETCONN: the number of struct netconns. More...
 
#define MEMP_NUM_PBUF   30
 MEMP_NUM_PBUF: the number of memp struct pbufs (used for PBUF_ROM and PBUF_REF). More...
 
#define MEMP_NUM_RAW_PCB   4
 MEMP_NUM_RAW_PCB: Number of raw connection PCBs (requires the LWIP_RAW option) More...
 
#define MEMP_NUM_SYS_TIMEOUT   0
 MEMP_NUM_SYS_TIMEOUT: the number of simulateously active timeouts. More...
 
#define MEMP_NUM_TCP_PCB   2
 MEMP_NUM_TCP_PCB: the number of simulatenously active TCP connections. More...
 
#define MEMP_NUM_TCP_PCB_LISTEN   2
 MEMP_NUM_TCP_PCB_LISTEN: the number of listening TCP connections. More...
 
#define MEMP_NUM_TCP_SEG   32
 MEMP_NUM_TCP_SEG: the number of simultaneously queued TCP segments. More...
 
#define MEMP_NUM_TCPIP_MSG_API   0
 MEMP_NUM_TCPIP_MSG_API: the number of struct tcpip_msg, which are used for callback/timeout API communication. More...
 
#define MEMP_NUM_TCPIP_MSG_INPKT   0
 MEMP_NUM_TCPIP_MSG_INPKT: the number of struct tcpip_msg, which are used for incoming packets. More...
 
#define MEMP_NUM_UDP_PCB   4
 MEMP_NUM_UDP_PCB: the number of UDP protocol control blocks. More...
 
#define NO_SYS   1
 NO_SYS==1: Provides VERY minimal functionality. More...
 
#define PBUF_LINK_HLEN   (14 + ETH_PAD_SIZE)
 PBUF_LINK_HLEN: the number of bytes that should be allocated for a link level header. More...
 
#define PBUF_POOL_SIZE   32
 PBUF_POOL_SIZE: the number of buffers in the pbuf pool. More...
 
#define SNMP_PRIVATE_MIB   0
 
#define TCP_MSS   512
 
#define TCP_SND_BUF   4096
 
#define UDP_TTL   (IP_DEFAULT_TTL)
 UDP_TTL: Default Time-To-Live value. More...
 

#define ETH_PAD_SIZE   WL_HEADER_SIZE /* size of wifiengine header */
#define ICMP_TTL   (IP_DEFAULT_TTL)

ICMP_TTL: Default value for Time-To-Live used by ICMP packets.

#define IP_DEFAULT_TTL   255

IP_DEFAULT_TTL: Default value for Time-To-Live used by transport layers.

#define IP_FORWARD   0

IP_FORWARD==1: Enables the ability to forward IP packets across network interfaces.

If you are going to run lwIP on a device with only one network interface, define this to 0.

#define IP_FRAG   1

IP_FRAG==1: Fragment outgoing IP packets if their size exceeds MTU.

Note that this option does not affect incoming packet sizes, which can be controlled via IP_REASSEMBLY.

#define IP_FRAG_USES_STATIC_BUF   0

IP_FRAG_USES_STATIC_BUF==1: Use a static MTU-sized buffer for IP fragmentation.

Otherwise pbufs are allocated and reference the original packet data to be fragmented.

#define IP_OPTIONS_ALLOWED   1

IP_OPTIONS: Defines the behavior for IP options.

IP_OPTIONS==0_ALLOWED: All packets with IP options are dropped. IP_OPTIONS==1_ALLOWED: IP options are allowed (but not parsed).

#define IP_REASS_MAX_PBUFS   10

IP_REASS_MAX_PBUFS: Total maximum amount of pbufs waiting to be reassembled.

Since the received pbufs are enqueued, be sure to configure PBUF_POOL_SIZE > IP_REASS_MAX_PBUFS so that the stack is still able to receive packets even if the maximum amount of fragments is enqueued for reassembly!

#define IP_REASS_MAXAGE   3

IP_REASS_MAXAGE: Maximum time (in multiples of IP_TMR_INTERVAL - so seconds, normally) a fragmented IP packet waits for all fragments to arrive.

If not all fragments arrived in this time, the whole packet is discarded.

#define IP_REASSEMBLY   1

IP_REASSEMBLY==1: Reassemble incoming fragmented IP packets.

Note that this option does not affect outgoing packet sizes, which can be controlled via IP_FRAG.

#define LINK_STATS   1
#define LWIP_ARP   1

LWIP_ARP==1: Enable ARP functionality.

#define LWIP_AUTOIP   0

LWIP_AUTOIP==1: Enable AUTOIP module.

#define LWIP_DHCP   1

LWIP_DHCP==1: Enable DHCP module.

#define LWIP_DNS   1

LWIP_DNS==1: Turn on DNS module.

UDP must be available for DNS transport.

#define LWIP_HAVE_LOOPIF   1

LWIP_HAVE_LOOPIF==1: Support loop interface (127.0.0.1) and loopif.c.

#define LWIP_ICMP   1

LWIP_ICMP==1: Enable ICMP module inside the IP stack.

Be careful, disable that make your product non-compliant to RFC1122

#define LWIP_IGMP   1

LWIP_IGMP==1: Turn on IGMP module.

#define LWIP_LOOPIF_MULTITHREADING   0
#define LWIP_NETCONN   0

LWIP_NETCONN==1: Enable Netconn API (require to use api_lib.c)

#define LWIP_NETIF_LINK_CALLBACK   1
#define LWIP_NETIF_STATUS_CALLBACK   1
#define LWIP_RAW   1

LWIP_RAW==1: Enable application layer to hook into the IP layer itself.

#define LWIP_SNMP   0

LWIP_SNMP==1: Turn on SNMP module.

UDP must be available for SNMP transport.

#define LWIP_SOCKET   0

LWIP_SOCKET==1: Enable Socket API (require to use sockets.c)

#define LWIP_STATS   1

LWIP_STATS==1: Enable statistics collection in lwip_stats.

#define LWIP_TCP   1

LWIP_TCP==1: Turn on TCP.

#define LWIP_TIMEVAL_PRIVATE   0
#define LWIP_UDP   1

LWIP_UDP==1: Turn on UDP.

#define LWIP_UDPLITE   0

LWIP_UDPLITE==1: Turn on UDP-Lite.

(Requires LWIP_UDP)

#define MEM_ALIGNMENT   4

MEM_ALIGNMENT: should be set to the alignment of the CPU 4 byte alignment -> #define MEM_ALIGNMENT 4 2 byte alignment -> #define MEM_ALIGNMENT 2.

#define MEM_LIBC_MALLOC   1
#define MEM_SIZE   16000

MEM_SIZE: the size of the heap memory.

If the application will send a lot of data that needs to be copied, this should be set high.

#define MEMP_NUM_ARP_QUEUE   2

MEMP_NUM_ARP_QUEUE: the number of simulateously queued outgoing packets (pbufs) that are waiting for an ARP request (to resolve their destination address) to finish.

(requires the ARP_QUEUEING option)

#define MEMP_NUM_NETBUF   0

MEMP_NUM_NETBUF: the number of struct netbufs.

(only needed if you use the sequential API, like api_lib.c)

#define MEMP_NUM_NETCONN   0

MEMP_NUM_NETCONN: the number of struct netconns.

(only needed if you use the sequential API, like api_lib.c)

#define MEMP_NUM_PBUF   30

MEMP_NUM_PBUF: the number of memp struct pbufs (used for PBUF_ROM and PBUF_REF).

If the application sends a lot of data out of ROM (or other static memory), this should be set high.

#define MEMP_NUM_RAW_PCB   4

MEMP_NUM_RAW_PCB: Number of raw connection PCBs (requires the LWIP_RAW option)

#define MEMP_NUM_SYS_TIMEOUT   0

MEMP_NUM_SYS_TIMEOUT: the number of simulateously active timeouts.

(requires NO_SYS==0)

#define MEMP_NUM_TCP_PCB   2

MEMP_NUM_TCP_PCB: the number of simulatenously active TCP connections.

(requires the LWIP_TCP option)

#define MEMP_NUM_TCP_PCB_LISTEN   2

MEMP_NUM_TCP_PCB_LISTEN: the number of listening TCP connections.

(requires the LWIP_TCP option)

#define MEMP_NUM_TCP_SEG   32

MEMP_NUM_TCP_SEG: the number of simultaneously queued TCP segments.

(requires the LWIP_TCP option)

#define MEMP_NUM_TCPIP_MSG_API   0

MEMP_NUM_TCPIP_MSG_API: the number of struct tcpip_msg, which are used for callback/timeout API communication.

(only needed if you use tcpip.c)

#define MEMP_NUM_TCPIP_MSG_INPKT   0

MEMP_NUM_TCPIP_MSG_INPKT: the number of struct tcpip_msg, which are used for incoming packets.

(only needed if you use tcpip.c)

#define MEMP_NUM_UDP_PCB   4

MEMP_NUM_UDP_PCB: the number of UDP protocol control blocks.

One per active UDP "connection". (requires the LWIP_UDP option)

#define NO_SYS   1

NO_SYS==1: Provides VERY minimal functionality.

Otherwise, use lwIP facilities.

#define PBUF_LINK_HLEN   (14 + ETH_PAD_SIZE)

PBUF_LINK_HLEN: the number of bytes that should be allocated for a link level header.

The default is 14, the standard value for Ethernet.

#define PBUF_POOL_SIZE   32

PBUF_POOL_SIZE: the number of buffers in the pbuf pool.

#define SNMP_PRIVATE_MIB   0
#define TCP_MSS   512
#define TCP_SND_BUF   4096
#define UDP_TTL   (IP_DEFAULT_TTL)

UDP_TTL: Default Time-To-Live value.