#include "fs_com.h"
Functions | |
bool | nav_flat_cd (void) |
This function enters in the selected directory in file list FLAT. More... | |
bool | nav_flat_fileisnotopen (void) |
This function checks if no file is opened. More... | |
bool | nav_flat_findname (const FS_STRING sz_name, bool b_match_case) |
This function searches a file name in file list FLAT. More... | |
uint16_t | nav_flat_get (void) |
This function returns the position of selected file in file list FLAT. More... | |
bool | nav_flat_goto (uint16_t u16_newpos) |
This function goes to a position in file list FLAT. More... | |
bool | nav_flat_gotoparent (void) |
This function goes to the parent directory. More... | |
bool | nav_flat_mount (void) |
This function mounts the selected partition. More... | |
uint16_t | nav_flat_nb (void) |
This function computes the number of files and directories present in the file list FLAT. More... | |
bool | nav_flat_next (void) |
Go to next file or directory in file list FLAT. More... | |
bool | nav_flat_previous (void) |
Go to previous file or directory in file list FLAT. More... | |
bool | nav_flat_reset (void) |
This function resets the selection pointer, so "no file is selected" in file list FLAT. More... | |
bool | nav_flat_root (void) |
This function initializes the file list on the root directory. More... | |
bool | nav_flat_validpos (void) |
This function checks if a file is selected. More... | |
bool nav_flat_cd | ( | void | ) |
This function enters in the selected directory in file list FLAT.
References fs_g_nav, nav_dir_cd(), Fs_management::u16_flat_pos_offset, and Fs_management::u8_flat_dir_level.
bool nav_flat_fileisnotopen | ( | void | ) |
This function checks if no file is opened.
References nav_filelist_fileisnotopen().
This function searches a file name in file list FLAT.
@param sz_name name to search (UNICODE or ASCII) <br> It must be terminated by NULL or '*' value @param b_match_case false to ignore the case @return false in case of error, see global value "fs_g_status" for more detail @return true otherwise
//! This function starts a search at the next position of the current in file list //!
References FS_NAME_CHECK, nav_file_name(), and nav_flat_next().
uint16_t nav_flat_get | ( | void | ) |
This function returns the position of selected file in file list FLAT.
References fs_g_nav, nav_filelist_get(), and Fs_management::u16_flat_pos_offset.
Referenced by nav_flat_goto(), and nav_flat_nb().
bool nav_flat_goto | ( | uint16_t | u16_newpos | ) |
This function goes to a position in file list FLAT.
u16_newpos | new position to select (0 is the first position) |
References nav_flat_get(), nav_flat_next(), nav_flat_previous(), nav_flat_reset(), and nav_flat_validpos().
Referenced by nav_flat_nb().
bool nav_flat_gotoparent | ( | void | ) |
This function goes to the parent directory.
@return false in case of error, see global value "fs_g_status" for more detail @return true otherwise
//! After the selected file is the first entry of the new file list FLAT //!
References _MEM_TYPE_SLOW_, fs_g_nav, index, nav_dir_gotoparent(), nav_filelist_reset(), nav_flat_next(), nav_getindex(), nav_gotoindex(), Fs_management::u16_flat_pos_offset, and Fs_management::u8_flat_dir_level.
bool nav_flat_mount | ( | void | ) |
This function mounts the selected partition.
@return false in case of error, see global value "fs_g_status" for more detail @return true otherwise
//! If the FS_MULTI_PARTITION option is disabled //! then the mount routine selects the first partition supported by file system. <br> //! After mount, the file list contains files and directories of ROOT directory //!
References fs_g_nav, nav_partition_mount(), Fs_management::u16_flat_pos_offset, and Fs_management::u8_flat_dir_level.
uint16_t nav_flat_nb | ( | void | ) |
This function computes the number of files and directories present in the file list FLAT.
References nav_flat_get(), nav_flat_goto(), nav_flat_next(), and nav_flat_reset().
bool nav_flat_next | ( | void | ) |
Go to next file or directory in file list FLAT.
References FS_FIND_NEXT, fs_g_nav, nav_dir_cd(), nav_dir_gotoparent(), nav_file_isdir(), nav_filelist_get(), nav_filelist_set(), Fs_management::u16_flat_pos_offset, and Fs_management::u8_flat_dir_level.
Referenced by nav_flat_findname(), nav_flat_goto(), nav_flat_gotoparent(), and nav_flat_nb().
bool nav_flat_previous | ( | void | ) |
Go to previous file or directory in file list FLAT.
References FS_FIND_NEXT, FS_FIND_PREV, fs_g_nav, nav_dir_cd(), nav_dir_gotoparent(), nav_file_isdir(), nav_filelist_get(), nav_filelist_set(), Fs_management::u16_flat_pos_offset, and Fs_management::u8_flat_dir_level.
Referenced by nav_flat_goto().
bool nav_flat_reset | ( | void | ) |
This function resets the selection pointer, so "no file is selected" in file list FLAT.
References fs_g_nav, nav_dir_gotoparent(), nav_filelist_reset(), Fs_management::u16_flat_pos_offset, and Fs_management::u8_flat_dir_level.
Referenced by nav_flat_goto(), and nav_flat_nb().
bool nav_flat_root | ( | void | ) |
This function initializes the file list on the root directory.
This function initializes the file list on the root directory.
References fs_g_nav, nav_dir_root(), Fs_management::u16_flat_pos_offset, and Fs_management::u8_flat_dir_level.
bool nav_flat_validpos | ( | void | ) |
This function checks if a file is selected.
References nav_filelist_validpos().
Referenced by nav_flat_goto().