Microchip® Advanced Software Framework

S_usb_as_interface_descriptor Struct Reference

Class-Specific AS Interface Descriptor.

#include <usb_descriptors.h>

Data Fields

uint8_t bDelay
 
uint8_t bDescriptorSubType
 
uint8_t bDescriptorType
 
uint8_t bLenght
 
uint8_t bTerminalLink
 
uint16_t wFormatTag
 

uint8_t S_usb_as_interface_descriptor::bDelay
uint8_t S_usb_as_interface_descriptor::bDescriptorSubType
uint8_t S_usb_as_interface_descriptor::bDescriptorType
uint8_t S_usb_as_interface_descriptor::bLenght
uint8_t S_usb_as_interface_descriptor::bTerminalLink
uint16_t S_usb_as_interface_descriptor::wFormatTag