Options to attribute to the resampling algorithm.
#include <dsp_resampling.h>
Public Types | |
enum | { DSP16_RESAMPLING_OPTIONS_USE_DYNAMIC = 0, DSP16_RESAMPLING_OPTIONS_USE_FIXED } |
Method used to generate the filter coefficients. More... | |
Data Fields | |
union { | |
struct { | |
bool coefficients_normalization | |
If set to true, normalize the filter coefficients to ensure the output won't be too reduced. More... | |
int custom_fc_hz | |
Use a custom cut-off frequency for this filter. By default it will choose min(fsin, fsmax) / 2. More... | |
void(* dsp16_custom_filter )(dsp16_t *coefficients, int fc_hz, int fs_hz, int order) | |
Custom filter function. If set to NULL, the algorithm will use the dsp16_filt_lpfirdesign function. More... | |
void(* dsp16_custom_window )(dsp16_t *window, dsp16_t *input, int size) | |
Custom window function. If set to NULL, the algorithm will use a rectangular window. More... | |
} dynamic | |
If using the dynamic method to generate the filter coefficients. More... | |
struct { | |
dsp16_t * dsp16_coefficients | |
Pointer on the fixed coefficient table. More... | |
} fixed | |
If using the static method to generate the filter coefficients. More... | |
}; | |
enum dsp16_resampling_options_t:: { ... } | coefficients_generation |
Method used to generate the filter coefficients. More... | |
anonymous enum |
union { ... } |
enum { ... } dsp16_resampling_options_t::coefficients_generation |
Method used to generate the filter coefficients.
Referenced by dsp16_resampling_setup(), main(), and usb_stream_init().
bool dsp16_resampling_options_t::coefficients_normalization |
If set to true, normalize the filter coefficients to ensure the output won't be too reduced.
int dsp16_resampling_options_t::custom_fc_hz |
Use a custom cut-off frequency for this filter. By default it will choose min(fsin, fsmax) / 2.
dsp16_t* dsp16_resampling_options_t::dsp16_coefficients |
Pointer on the fixed coefficient table.
void(* dsp16_resampling_options_t::dsp16_custom_filter)(dsp16_t *coefficients, int fc_hz, int fs_hz, int order) |
Custom filter function. If set to NULL, the algorithm will use the dsp16_filt_lpfirdesign function.
Custom window function. If set to NULL, the algorithm will use a rectangular window.
struct { ... } dsp16_resampling_options_t::dynamic |
If using the dynamic method to generate the filter coefficients.
Referenced by dsp16_resampling_setup(), main(), and usb_stream_init().
struct { ... } dsp16_resampling_options_t::fixed |
If using the static method to generate the filter coefficients.
Referenced by dsp16_resampling_setup().