Macros | |
#define | _STATIC_PORT_PIN_CONF_ 1 |
#define | INTRABURST_1 0 |
#define | INTRABURST_2 0 |
#define | QTOUCH_SNS_PORT_COUNT 1 |
QTOUCH LIBRARY CONFIGURATION | |
#define | QT_NUM_CHANNELS 32 |
Number of QTouch Channels to be used 8 or 16 or 32 - Defined in the Symbols in Project Properties. More... | |
#define | QT_DELAY_CYCLES 5 |
Delay cycles that determine the capacitance charge transfer time. More... | |
#define | _ROTOR_SLIDER_ |
Rotor/slider can be added to the design, if this macro is enabled. More... | |
#define | SNS A |
Port to be used for SNS Defined in the Symbols in Project Properties. More... | |
#define | SNSK B |
Port to be used for SNSK Defined in the Symbols in Project Properties. More... | |
#define _ROTOR_SLIDER_ |
Rotor/slider can be added to the design, if this macro is enabled.
Defined in the Symbols in Project Properties
#define _STATIC_PORT_PIN_CONF_ 1 |
#define INTRABURST_1 0 |
#define INTRABURST_2 0 |
#define QT_DELAY_CYCLES 5 |
Delay cycles that determine the capacitance charge transfer time.
1 to 255 - Defined in the Symbols in Project Properties
#define QT_NUM_CHANNELS 32 |
Number of QTouch Channels to be used 8 or 16 or 32 - Defined in the Symbols in Project Properties.
#define QTOUCH_SNS_PORT_COUNT 1 |
#define SNS A |
Port to be used for SNS Defined in the Symbols in Project Properties.
#define SNSK B |
Port to be used for SNSK Defined in the Symbols in Project Properties.