#include "dsp.h"
Macros | |
Twiddle factors table | |
#define | DSP16_N_TWIDDLE_FACTORS 1024 |
This constant defines the size of the twiddle factors table we want to store in memory. i.e.: if we want to compute a 1024-point (or less) complex FFT, we will define this constant as follow: More... | |
#define | TWIDDLE_FACTORS_PREFIX_TAB |
This constant permits you to add attributes to the twiddle factors table. It is useful if you want to store the table into another memory for example. i.e.: More... | |
Variables | |
TWIDDLE_FACTORS_PREFIX_TAB dsp16_t | dsp16_twiddle_factors [] |
This table has been generated using the following algorithm: More... | |
TWIDDLE_FACTORS_PREFIX_TAB dsp16_t | dsp16_twiddle_factors2 [] |
This table has been generated using the following algorithm: More... | |
TWIDDLE_FACTORS_PREFIX_TAB dsp16_t dsp16_twiddle_factors[] |
This table has been generated using the following algorithm:
It is a one dimensional array containing the real parts (even parts) and imaginary parts (odd parts) of the w value.
Referenced by dsp16_trans_complexfft(), dsp16_trans_complexifft(), and dsp16_trans_realcomplexfft().
TWIDDLE_FACTORS_PREFIX_TAB dsp16_t dsp16_twiddle_factors2[] |
This table has been generated using the following algorithm:
It is a one dimensional array containing the real parts (4*i parts) and imaginary parts (4*i+1 parts) of the w2 value and the real parts (4*i+2 parts) and imaginary parts (4*i+3 parts) of the w3 value.
Referenced by dsp16_trans_complexfft(), dsp16_trans_complexifft(), and dsp16_trans_realcomplexfft().