#include <avr32/io.h>
#include "compiler.h"
#include "gpio.h"
#include "board.h"
#include "eic.h"
#include "intc.h"
Macros | |
Keypad scan index configuration | |
Choose the scan index for each scan column in the [0,7] range.
| |
#define | SCAN_COL1_IDX 0 |
#define | SCAN_COL1_MUX _0 |
#define | SCAN_COL2_IDX 1 |
#define | SCAN_COL2_MUX _0 |
External Interrupt pin Mappings | |
#define | EXT_INT_EXAMPLE_PIN_LINE1 AVR32_EIC_EXTINT_6_PIN |
#define | EXT_INT_EXAMPLE_FUNCTION_LINE1 AVR32_EIC_EXTINT_6_FUNCTION |
#define | EXT_INT_EXAMPLE_LINE1 EXT_INT6 |
#define | EXT_INT_EXAMPLE_IRQ_LINE1 AVR32_EIC_IRQ_6 |
#define | EXT_INT_EXAMPLE_PIN_LINE2 AVR32_EIC_EXTINT_7_PIN |
#define | EXT_INT_EXAMPLE_FUNCTION_LINE2 AVR32_EIC_EXTINT_7_FUNCTION |
#define | EXT_INT_EXAMPLE_LINE2 EXT_INT7 |
#define | EXT_INT_EXAMPLE_IRQ_LINE2 AVR32_EIC_IRQ_7 |
#define | EXT_SCAN_EXAMPLE_PIN_LINE1 ATPASTE4(AVR32_EIC_SCAN_,SCAN_COL1_IDX,SCAN_COL1_MUX,_PIN) |
#define | EXT_SCAN_EXAMPLE_FUNCTION_LINE1 ATPASTE4(AVR32_EIC_SCAN_,SCAN_COL1_IDX,SCAN_COL1_MUX,_FUNCTION) |
#define | EXT_SCAN_EXAMPLE_PIN_LINE2 ATPASTE4(AVR32_EIC_SCAN_,SCAN_COL2_IDX,SCAN_COL2_MUX,_PIN) |
#define | EXT_SCAN_EXAMPLE_FUNCTION_LINE2 ATPASTE4(AVR32_EIC_SCAN_,SCAN_COL2_IDX,SCAN_COL2_MUX,_FUNCTION) |
Functions | |
static void | eic_int_handler1 (void) |
Interrupt handler of the External interrupt line "1". More... | |
static void | eic_int_handler2 (void) |
Interrupt handler of the External interrupt line "2". More... | |
int | main (void) |
static void | software_delay (void) |
Variables | |
static volatile bool | bCancelSwDelay = false |
Global var used to cancel the software delay if an External Interrupt occurs. More... | |
eic_options_t | eic_options [2] |
Structure holding the configuration parameters of the EIC module. More... | |
unsigned char | key_number = 0 |
Global var used to switch between different LED patterns. More... | |
#define EXT_INT_EXAMPLE_FUNCTION_LINE1 AVR32_EIC_EXTINT_6_FUNCTION |
Referenced by main().
#define EXT_INT_EXAMPLE_FUNCTION_LINE2 AVR32_EIC_EXTINT_7_FUNCTION |
Referenced by main().
#define EXT_INT_EXAMPLE_IRQ_LINE1 AVR32_EIC_IRQ_6 |
Referenced by main().
#define EXT_INT_EXAMPLE_IRQ_LINE2 AVR32_EIC_IRQ_7 |
Referenced by main().
#define EXT_INT_EXAMPLE_LINE1 EXT_INT6 |
Referenced by eic_int_handler1(), eic_nmi_handler(), and main().
#define EXT_INT_EXAMPLE_LINE2 EXT_INT7 |
Referenced by eic_int_handler2(), and main().
#define EXT_INT_EXAMPLE_PIN_LINE1 AVR32_EIC_EXTINT_6_PIN |
Referenced by main().
#define EXT_INT_EXAMPLE_PIN_LINE2 AVR32_EIC_EXTINT_7_PIN |
Referenced by main().
#define EXT_SCAN_EXAMPLE_FUNCTION_LINE1 ATPASTE4(AVR32_EIC_SCAN_,SCAN_COL1_IDX,SCAN_COL1_MUX,_FUNCTION) |
Referenced by main().
#define EXT_SCAN_EXAMPLE_FUNCTION_LINE2 ATPASTE4(AVR32_EIC_SCAN_,SCAN_COL2_IDX,SCAN_COL2_MUX,_FUNCTION) |
Referenced by main().
#define EXT_SCAN_EXAMPLE_PIN_LINE1 ATPASTE4(AVR32_EIC_SCAN_,SCAN_COL1_IDX,SCAN_COL1_MUX,_PIN) |
Referenced by main().
#define EXT_SCAN_EXAMPLE_PIN_LINE2 ATPASTE4(AVR32_EIC_SCAN_,SCAN_COL2_IDX,SCAN_COL2_MUX,_PIN) |
Referenced by main().
#define SCAN_COL1_IDX 0 |
Referenced by eic_int_handler1(), and eic_int_handler2().
#define SCAN_COL1_MUX _0 |
#define SCAN_COL2_IDX 1 |
Referenced by eic_int_handler1(), and eic_int_handler2().
#define SCAN_COL2_MUX _0 |
|
static |
Interrupt handler of the External interrupt line "1".
References bCancelSwDelay, eic_clear_interrupt_line(), eic_get_interrupt_pad_scan(), EXT_INT_EXAMPLE_LINE1, key_number, SCAN_COL1_IDX, and SCAN_COL2_IDX.
Referenced by main().
|
static |
Interrupt handler of the External interrupt line "2".
References bCancelSwDelay, eic_clear_interrupt_line(), eic_get_interrupt_pad_scan(), EXT_INT_EXAMPLE_LINE2, key_number, SCAN_COL1_IDX, and SCAN_COL2_IDX.
Referenced by main().
int main | ( | void | ) |
References Disable_global_interrupt, eic_options_t::eic_async, eic_options_t::eic_edge, EIC_EDGE_FALLING_EDGE, eic_enable_interrupt_lines(), eic_enable_interrupt_scan(), eic_enable_lines(), eic_init(), eic_int_handler1(), eic_int_handler2(), eic_options_t::eic_line, eic_options_t::eic_mode, EIC_MODE_EDGE_TRIGGERED, EIC_SYNCH_MODE, Enable_global_interrupt, EXT_INT_EXAMPLE_FUNCTION_LINE1, EXT_INT_EXAMPLE_FUNCTION_LINE2, EXT_INT_EXAMPLE_IRQ_LINE1, EXT_INT_EXAMPLE_IRQ_LINE2, EXT_INT_EXAMPLE_LINE1, EXT_INT_EXAMPLE_LINE2, EXT_INT_EXAMPLE_PIN_LINE1, EXT_INT_EXAMPLE_PIN_LINE2, EXT_SCAN_EXAMPLE_FUNCTION_LINE1, EXT_SCAN_EXAMPLE_FUNCTION_LINE2, EXT_SCAN_EXAMPLE_PIN_LINE1, EXT_SCAN_EXAMPLE_PIN_LINE2, gpio_clr_gpio_pin(), gpio_enable_module(), gpio_enable_pin_pull_up(), gpio_set_gpio_pin(), INTC_init_interrupts(), INTC_register_interrupt(), key_number, LED1_GPIO, LED2_GPIO, LED3_GPIO, and software_delay().
|
static |
References bCancelSwDelay, and i.
Referenced by main().
Global var used to cancel the software delay if an External Interrupt occurs.
Referenced by eic_int_handler1(), eic_int_handler2(), and software_delay().
eic_options_t eic_options[2] |
Structure holding the configuration parameters of the EIC module.
unsigned char key_number = 0 |
Global var used to switch between different LED patterns.
Referenced by eic_int_handler1(), eic_int_handler2(), eic_nmi_handler(), and main().