Microchip® Advanced Software Framework

 All Data Structures Namespaces Files Functions Variables Typedefs Enumerations Enumerator Friends Macros Groups Pages
MultiMedia Card Interface (MCI)

implementation

Macros

#define AVR32_MCI_MR_FBYTE_MASK   AVR32_MCI_MR_PDCFBYTE_MASK
 
static uint32_t mci_transfert_pos
 
static uint16_t mci_block_size
 
static uint16_t mci_nb_block
 
static void mci_reset (void)
 Reset the MCI interface. More...
 
static void mci_set_speed (uint32_t speed, uint32_t pbb_hz)
 Set speed of the MCI clock. More...
 
static bool mci_wait_busy (void)
 Wait the end of busy signal on data line. More...
 
static bool mci_wait_busy_on_line (void)
 Wait the end of busy signal on data line through GPIO. More...
 
static bool mci_send_cmd_execute (uint32_t cmdr, sdmmc_cmd_def_t cmd, uint32_t arg)
 Send a command. More...
 
void mci_init (void)
 Initialize the low level driver. More...
 
uint8_t mci_get_bus_width (uint8_t slot)
 Return the maximum bus width of a slot. More...
 
bool mci_is_high_speed_capable (void)
 Return the high speed capability of the driver. More...
 
void mci_select_device (uint8_t slot, uint32_t clock, uint8_t bus_width, bool high_speed)
 Select a slot and initialize it. More...
 
void mci_deselect_device (uint8_t slot)
 Deselect a slot. More...
 
void mci_send_clock (void)
 Send 74 clock cycles on the line of selected slot Note: It is required after card plug and before card install. More...
 
bool mci_send_cmd (sdmmc_cmd_def_t cmd, uint32_t arg)
 Send a command on the selected slot. More...
 
uint32_t mci_get_response (void)
 Return the 32 bits response of the last command. More...
 
void mci_get_response_128 (uint8_t *response)
 Return the 128-bits response of the last command. More...
 
bool mci_adtc_start (sdmmc_cmd_def_t cmd, uint32_t arg, uint16_t block_size, uint16_t nb_block, bool access_block)
 Send an ADTC command on the selected slot An ADTC (Addressed Data Transfer Commands) command is used for read/write access. More...
 
bool mci_adtc_stop (sdmmc_cmd_def_t cmd, uint32_t arg)
 Send a command to stop an ADTC command on the selected slot. More...
 
bool mci_read_word (uint32_t *value)
 Read a word on the line. More...
 
bool mci_write_word (uint32_t value)
 Write a word on the line. More...
 
bool mci_start_read_blocks (void *dest, uint16_t nb_block)
 Start a read blocks transfer on the line Note: The driver will use the DMA available to speed up the transfer. More...
 
bool mci_wait_end_of_read_blocks (void)
 Wait the end of transfer started by mci_start_read_blocks() More...
 
bool mci_start_write_blocks (const void *src, uint16_t nb_block)
 Start a write blocks transfer on the line Note: The driver will use the DMA available to speed up the transfer. More...
 
bool mci_wait_end_of_write_blocks (void)
 Wait the end of transfer started by mci_start_write_blocks() More...
 
#define AVR32_MCI_DTOR_DTOMUL_1048576_MASK   (AVR32_MCI_DTOR_DTOMUL_1048576 << AVR32_MCI_DTOR_DTOMUL_OFFSET)
 Registers masks definitions. More...
 
#define AVR32_MCI_CSTOR_CSTOMUL_1048576_MASK   (AVR32_MCI_CSTOR_CSTOMUL_1048576 << AVR32_MCI_CSTOR_CSTOMUL_OFFSET)
 
#define AVR32_MCI_CSTOR_CSTOCYC_2_MASK   ( 2 << AVR32_MCI_CSTOR_CSTOCYC_OFFSET)
 
#define AVR32_MCI_DTOR_DTOCYC_2_MASK   ( 2 << AVR32_MCI_DTOR_DTOCYC_OFFSET)
 
#define AVR32_MCI_SDCR_SDCBUS_1_BIT_MASK   ( AVR32_MCI_SDCR_SDCBUS_1_BIT << AVR32_MCI_SDCR_SDCBUS_OFFSET)
 
#define AVR32_MCI_SDCR_SDCBUS_4_BIT_MASK   ( AVR32_MCI_SDCR_SDCBUS_4_BIT << AVR32_MCI_SDCR_SDCBUS_OFFSET)
 
#define AVR32_MCI_SDCR_SDCBUS_8_BIT_MASK   ( AVR32_MCI_SDCR_SDCBUS_8_BIT << AVR32_MCI_SDCR_SDCBUS_OFFSET)
 
#define AVR32_MCI_SDCR_SDCSEL_0_MASK   ( 0 << AVR32_MCI_SDCR_SDCSEL_OFFSET)
 
#define AVR32_MCI_SDCR_SDCSEL_1_MASK   ( 1 << AVR32_MCI_SDCR_SDCSEL_OFFSET)
 
#define AVR32_MCI_CMDR_TRCMD_START_TRANS_MASK   ( AVR32_MCI_CMDR_TRCMD_START_TRANS << AVR32_MCI_CMDR_TRCMD_OFFSET)
 
#define AVR32_MCI_CMDR_TRDIR_READ_MASK   ( AVR32_MCI_CMDR_TRDIR_READ << AVR32_MCI_CMDR_TRDIR_OFFSET)
 
#define AVR32_MCI_CMDR_TRTYP_SDIO_BYTE_MASK   ( AVR32_MCI_CMDR_TRTYP_SDIO_BYTE << AVR32_MCI_CMDR_TRTYP_OFFSET)
 
#define AVR32_MCI_CMDR_TRTYP_SDIO_BLOCK_MASK   ( AVR32_MCI_CMDR_TRTYP_SDIO_BLOCK << AVR32_MCI_CMDR_TRTYP_OFFSET)
 
#define AVR32_MCI_CMDR_TRTYP_STREAM_MASK   ( AVR32_MCI_CMDR_TRTYP_STREAM << AVR32_MCI_CMDR_TRTYP_OFFSET)
 
#define AVR32_MCI_CMDR_TRTYP_BLOCK_MASK   ( AVR32_MCI_CMDR_TRTYP_BLOCK << AVR32_MCI_CMDR_TRTYP_OFFSET)
 
#define AVR32_MCI_CMDR_TRTYP_MULTI_BLOCK_MASK   ( AVR32_MCI_CMDR_TRTYP_MULTI_BLOCK << AVR32_MCI_CMDR_TRTYP_OFFSET)
 
#define SD_MMC_MCI_MEM_CNT   1
 
#define SD_MMC_MCI_SLOT_0_SIZE   1
 
#define SD_MMC_MCI_SLOT_0_DATA0_PIN   0
 
#define SD_MMC_MCI_SLOT_0_DATA3_PIN   0
 
#define mci_debug(...)
 
#define CONF_MCI_DMACA_CHANNEL   1
 

#define AVR32_MCI_CMDR_TRCMD_START_TRANS_MASK   ( AVR32_MCI_CMDR_TRCMD_START_TRANS << AVR32_MCI_CMDR_TRCMD_OFFSET)

Referenced by mci_adtc_start().

#define AVR32_MCI_CMDR_TRDIR_READ_MASK   ( AVR32_MCI_CMDR_TRDIR_READ << AVR32_MCI_CMDR_TRDIR_OFFSET)

Referenced by mci_adtc_start().

#define AVR32_MCI_CMDR_TRTYP_BLOCK_MASK   ( AVR32_MCI_CMDR_TRTYP_BLOCK << AVR32_MCI_CMDR_TRTYP_OFFSET)

Referenced by mci_adtc_start().

#define AVR32_MCI_CMDR_TRTYP_MULTI_BLOCK_MASK   ( AVR32_MCI_CMDR_TRTYP_MULTI_BLOCK << AVR32_MCI_CMDR_TRTYP_OFFSET)

Referenced by mci_adtc_start().

#define AVR32_MCI_CMDR_TRTYP_SDIO_BLOCK_MASK   ( AVR32_MCI_CMDR_TRTYP_SDIO_BLOCK << AVR32_MCI_CMDR_TRTYP_OFFSET)

Referenced by mci_adtc_start().

#define AVR32_MCI_CMDR_TRTYP_SDIO_BYTE_MASK   ( AVR32_MCI_CMDR_TRTYP_SDIO_BYTE << AVR32_MCI_CMDR_TRTYP_OFFSET)

Referenced by mci_adtc_start().

#define AVR32_MCI_CMDR_TRTYP_STREAM_MASK   ( AVR32_MCI_CMDR_TRTYP_STREAM << AVR32_MCI_CMDR_TRTYP_OFFSET)

Referenced by mci_adtc_start().

#define AVR32_MCI_CSTOR_CSTOCYC_2_MASK   ( 2 << AVR32_MCI_CSTOR_CSTOCYC_OFFSET)

Referenced by mci_init().

#define AVR32_MCI_CSTOR_CSTOMUL_1048576_MASK   (AVR32_MCI_CSTOR_CSTOMUL_1048576 << AVR32_MCI_CSTOR_CSTOMUL_OFFSET)

Referenced by mci_init().

#define AVR32_MCI_DTOR_DTOCYC_2_MASK   ( 2 << AVR32_MCI_DTOR_DTOCYC_OFFSET)

Referenced by mci_init().

#define AVR32_MCI_DTOR_DTOMUL_1048576_MASK   (AVR32_MCI_DTOR_DTOMUL_1048576 << AVR32_MCI_DTOR_DTOMUL_OFFSET)

Registers masks definitions.

Referenced by mci_init().

#define AVR32_MCI_MR_FBYTE_MASK   AVR32_MCI_MR_PDCFBYTE_MASK
#define AVR32_MCI_SDCR_SDCBUS_1_BIT_MASK   ( AVR32_MCI_SDCR_SDCBUS_1_BIT << AVR32_MCI_SDCR_SDCBUS_OFFSET)
#define AVR32_MCI_SDCR_SDCBUS_4_BIT_MASK   ( AVR32_MCI_SDCR_SDCBUS_4_BIT << AVR32_MCI_SDCR_SDCBUS_OFFSET)

Referenced by mci_select_device().

#define AVR32_MCI_SDCR_SDCBUS_8_BIT_MASK   ( AVR32_MCI_SDCR_SDCBUS_8_BIT << AVR32_MCI_SDCR_SDCBUS_OFFSET)

Referenced by mci_select_device().

#define AVR32_MCI_SDCR_SDCSEL_0_MASK   ( 0 << AVR32_MCI_SDCR_SDCSEL_OFFSET)

Referenced by mci_select_device().

#define AVR32_MCI_SDCR_SDCSEL_1_MASK   ( 1 << AVR32_MCI_SDCR_SDCSEL_OFFSET)

Referenced by mci_select_device().

#define CONF_MCI_DMACA_CHANNEL   1
#define SD_MMC_MCI_MEM_CNT   1
#define SD_MMC_MCI_SLOT_0_DATA0_PIN   0

Referenced by mci_wait_busy_on_line().

#define SD_MMC_MCI_SLOT_0_DATA3_PIN   0

Referenced by mci_send_cmd_execute().

#define SD_MMC_MCI_SLOT_0_SIZE   1

Referenced by mci_get_bus_width().

bool mci_adtc_start ( sdmmc_cmd_def_t  cmd,
uint32_t  arg,
uint16_t  block_size,
uint16_t  nb_block,
bool  access_block 
)

Send an ADTC command on the selected slot An ADTC (Addressed Data Transfer Commands) command is used for read/write access.

Parameters
cmdCommand definition
argArgument of the command
block_sizeBlock size used for the transfer
nb_blockTotal number of block for this transfer
access_blockif true, the x_read_blocks() and x_write_blocks() functions must be used after this function. If false, the mci_read_word() and mci_write_word() functions must be used after this function.
Returns
true if success, otherwise false

References Assert, AVR32_MCI_CMDR_TRCMD_START_TRANS_MASK, AVR32_MCI_CMDR_TRDIR_READ_MASK, AVR32_MCI_CMDR_TRTYP_BLOCK_MASK, AVR32_MCI_CMDR_TRTYP_MULTI_BLOCK_MASK, AVR32_MCI_CMDR_TRTYP_SDIO_BLOCK_MASK, AVR32_MCI_CMDR_TRTYP_SDIO_BYTE_MASK, AVR32_MCI_CMDR_TRTYP_STREAM_MASK, AVR32_MCI_MR_FBYTE_MASK, mci_block_size, mci_nb_block, mci_send_cmd_execute(), mci_transfert_pos, SDMMC_CMD_MULTI_BLOCK, SDMMC_CMD_SDIO_BLOCK, SDMMC_CMD_SDIO_BYTE, SDMMC_CMD_SINGLE_BLOCK, SDMMC_CMD_STREAM, and SDMMC_CMD_WRITE.

bool mci_adtc_stop ( sdmmc_cmd_def_t  cmd,
uint32_t  arg 
)

Send a command to stop an ADTC command on the selected slot.

Parameters
cmdCommand definition
argArgument of the command
Returns
true if success, otherwise false

References mci_send_cmd_execute(), and mci_wait_busy_on_line().

void mci_deselect_device ( uint8_t  slot)

Deselect a slot.

Parameters
slotSelected slot

References AVR32_MCI_SDCR_SDCBUS_1_BIT_MASK, and UNUSED().

uint8_t mci_get_bus_width ( uint8_t  slot)

Return the maximum bus width of a slot.

Parameters
slotSelected slot
Returns
1, 4 or 8 lines.

References SD_MMC_MCI_SLOT_0_SIZE.

uint32_t mci_get_response ( void  )

Return the 32 bits response of the last command.

Returns
32 bits response
void mci_get_response_128 ( uint8_t *  response)

Return the 128-bits response of the last command.

Parameters
responsePointer on the array to fill with the 128-bits response

References i.

bool mci_is_high_speed_capable ( void  )

Return the high speed capability of the driver.

Returns
true, if the high speed mode is supported
bool mci_read_word ( uint32_t *  value)

Read a word on the line.

Parameters
valuePointer on a word to fill
Returns
true if success, otherwise false

References Assert, le32_to_cpu, mci_block_size, mci_debug, mci_nb_block, mci_reset(), and mci_transfert_pos.

void mci_select_device ( uint8_t  slot,
uint32_t  clock,
uint8_t  bus_width,
bool  high_speed 
)

Select a slot and initialize it.

Parameters
slotSelected slot
clockMaximum clock to use (Hz)
bus_widthBus width to use (1, 4 or 8)
high_speedtrue, to enable high speed mode

References Assert, AVR32_MCI_SDCR_SDCBUS_1_BIT_MASK, AVR32_MCI_SDCR_SDCBUS_4_BIT_MASK, AVR32_MCI_SDCR_SDCBUS_8_BIT_MASK, AVR32_MCI_SDCR_SDCSEL_0_MASK, AVR32_MCI_SDCR_SDCSEL_1_MASK, mci_set_speed(), and sysclk_get_pbb_hz().

void mci_send_clock ( void  )

Send 74 clock cycles on the line of selected slot Note: It is required after card plug and before card install.

References AVR32_MCI_MR_FBYTE_MASK.

bool mci_send_cmd ( sdmmc_cmd_def_t  cmd,
uint32_t  arg 
)
static bool mci_send_cmd_execute ( uint32_t  cmdr,
sdmmc_cmd_def_t  cmd,
uint32_t  arg 
)
static

Send a command.

Parameters
cmdrCMDR register bit mask to use for this command
cmdCommand definition
argArgument of the command
Returns
true if success, otherwise false

References arg, gpio_configure_pin(), GPIO_DIR_INPUT, gpio_enable_gpio_pin(), GPIO_PULL_UP, mci_debug, mci_reset(), mci_wait_busy(), SD_MMC_MCI_SLOT_0_DATA3_PIN, SDMMC_CMD_OPENDRAIN, SDMMC_MCI_CMD0_GO_IDLE_STATE, SDMMC_RESP_136, SDMMC_RESP_BUSY, SDMMC_RESP_CRC, and SDMMC_RESP_PRESENT.

Referenced by mci_adtc_start(), mci_adtc_stop(), and mci_send_cmd().

static void mci_set_speed ( uint32_t  speed,
uint32_t  pbb_hz 
)
static

Set speed of the MCI clock.

Parameters
speedMCI clock speed in Hz.
pbb_hzPBB clock speed in Hz.

References speed.

Referenced by mci_init(), mci_select_device(), and sd_mmc_mci_card_init().

bool mci_start_read_blocks ( void *  dest,
uint16_t  nb_block 
)

Start a read blocks transfer on the line Note: The driver will use the DMA available to speed up the transfer.

Parameters
destPointer on the buffer to fill
nb_blockNumber of block to transfer
Returns
true if started, otherwise false

References Assert, AVR32_MCI_MR_FBYTE_MASK, mci_block_size, mci_nb_block, and mci_transfert_pos.

bool mci_start_write_blocks ( const void *  src,
uint16_t  nb_block 
)

Start a write blocks transfer on the line Note: The driver will use the DMA available to speed up the transfer.

Parameters
srcPointer on the buffer to send
nb_blockNumber of block to transfer
Returns
true if started, otherwise false

References Assert, AVR32_MCI_MR_FBYTE_MASK, mci_block_size, mci_nb_block, and mci_transfert_pos.

static bool mci_wait_busy ( void  )
static

Wait the end of busy signal on data line.

Returns
true if success, otherwise false

References mci_debug, and mci_reset().

Referenced by mci_send_cmd_execute().

static bool mci_wait_busy_on_line ( void  )
static

Wait the end of busy signal on data line through GPIO.

Returns
true if success, otherwise false

References gpio_get_pin_value(), mci_debug, mci_reset(), and SD_MMC_MCI_SLOT_0_DATA0_PIN.

Referenced by mci_adtc_stop().

bool mci_wait_end_of_read_blocks ( void  )

Wait the end of transfer started by mci_start_read_blocks()

Returns
true if success, otherwise false

References mci_block_size, mci_debug, mci_nb_block, mci_reset(), and mci_transfert_pos.

bool mci_wait_end_of_write_blocks ( void  )

Wait the end of transfer started by mci_start_write_blocks()

Returns
true if success, otherwise false

References Assert, mci_block_size, mci_debug, mci_nb_block, mci_reset(), and mci_transfert_pos.

bool mci_write_word ( uint32_t  value)

Write a word on the line.

Parameters
valueWord to send
Returns
true if success, otherwise false

References Assert, cpu_to_le32, mci_block_size, mci_debug, mci_nb_block, mci_reset(), and mci_transfert_pos.